RIoTboard
  • Products
  • Dev Tools
  • Single-Board Computers
  • RIoTboard
  • More
  • Cancel
RIoTboard
Forum How to add module usbserial
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join RIoTboard to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 4 replies
  • Subscribers 24 subscribers
  • Views 1150 views
  • Users 0 members are here
Related

How to add module usbserial

e14 Contributor
e14 Contributor over 12 years ago

I want to attach the mobile-modem Huawei E-169 and an USB-RS485 adapter.

Both devices are listed in lsusb.

but no one will be mounted correctly

The Huawei Modem should be mounted at /dev/ttyUSB*.

dmesg delivers output only mounted as storage.

 

usb 2-1.2: new high speed USB device number 8 using fsl-ehci

scsi7 : usb-storage 2-1.2:1.2

scsi8 : usb-storage 2-1.2:1.3

scsi 7:0:0:0: CD-ROM            HUAWEI   Mass Storage     2.31 PQ: 0 ANSI: 2

scsi 8:0:0:0: Direct-Access     HUAWEI   MMC Storage      2.31 PQ: 0 ANSI: 2

sd 8:0:0:0: [sda] Attached SCSI removable disk

linaro@linaro-ubuntu-desktop:~$

 

I tried to modeswitch the device with modeprobe usbserial with following error.

FATAL: Module usb_serial not found.

 

How can i load module usb_serial?

 

linaro@linaro-ubuntu-desktop:~$ modprobe -l | grep serial

kernel/drivers/usb/gadget/g_serial.ko

already tried to /boot/linux.config

CONFIG_USB_SERIAL=y and

CONFIG_USB_SERIAL=m

 

Working on Ubuntu 12.11

Linux linaro-ubuntu-desktop 3.0.35-03023-ga0660f4 #1 SMP PREEMPT Tue Mar 25 21:17:12 CET 2014 armv7l armv7l armv7l GNU/Linux

  • Sign in to reply
  • Cancel
Parents
  • tusharp
    0 tusharp over 12 years ago

    as mentioned by agrahambell  you can recompile the kernel, however you can give the below just-a-try to check if it works.

    i have got a number of usb devices working on X86 (not arm) by just changing modeswitch .

     

    goto module build directory "lib/modules/<kernel version>"

    execute below comands with your PID VID & check if its has a supported module.

    cat modules.alias | grep [PID]

    cat modules.alias | grep [VID]

     

    try this also

    in "/etc/usb_modeswitch.conf"

    change DisableSwitching from "0" to "1",

    this ensures the USB default mode is not activated.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to tusharp

    fairly sure the entry won't be in modules.alias if the module was never built, but sure it's worth a try.

     

    I downloaded the e14 Ubuntu image and there appears to be so few modules included that lots of people are going to have problems.. Only a single wifi module included sticks out as being a really strange choice image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to tusharp

    fairly sure the entry won't be in modules.alias if the module was never built, but sure it's worth a try.

     

    I downloaded the e14 Ubuntu image and there appears to be so few modules included that lots of people are going to have problems.. Only a single wifi module included sticks out as being a really strange choice image