RIoTboard
  • Products
  • Dev Tools
  • Single-Board Computers
  • RIoTboard
  • More
  • Cancel
RIoTboard
Forum Open SDA
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join RIoTboard to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 12 replies
  • Subscribers 24 subscribers
  • Views 1571 views
  • Users 0 members are here
Related

Open SDA

tjmerics
tjmerics over 12 years ago

ANy info on getting the Open SDA interface working on the riot board ? Given the builtin usb-serial bridge this could be quite useful.

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    I tried getting some response using the instructions in the OpenSDA users guide from http://www.pemicro.com/opensda/ but no luck.

     

    I've heard that there will be support for it at some point, but nothing more than that.

     

    I'm not really sure how useful that usb-serial connection will be, given that most of the usefull stuff will be directed towards the debug connector at J18 by default.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • tjmerics
    0 tjmerics over 12 years ago in reply to e14 Contributor

    THe device is a composite usb device. It will support a serial port and debug port at the same time. It's not hard to redirect the console. Will only need a USB cable to get serial. Seems to me they would want at least the serial running to make things easy.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to tjmerics

    You'd think.

     

    On the couple of boards I have, I get no usb devices enumerated when I connect to that port, which would appear to suggest there's either no firmware on the device, or that what's on it doesn't do the OpenSDA features.

    Is yours any different? Do you see anything enumerated if you connect it to a PC?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • tjmerics
    0 tjmerics over 12 years ago in reply to e14 Contributor

    Mine doesn't enumerate either. Hope one doesn't need a jtag programmer to install the software. SHould have been setup to use the USB boot loader. Thought this was really going to be a great board. It's very disappointing.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to tjmerics

    I still think it's a good board, but I don't understand what the point is in loading the OpenSDA parts without the firmware.  If jtag is needed then I suspect that very few people will bother, especially as J17 isn't installed.

    Only other way I can see from the schematics is if it can somehow detect a specially formatted SD card in J6 and read OpenSDA firmware from there.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • tusharp
    0 tusharp over 12 years ago in reply to e14 Contributor

    if it can somehow detect a specially formatted SD card in J6 and read OpenSDA firmware from there

    but its connected to SPI flash.

    Once the burn SDA_BURN_EN is active, it will interface with SPI flash rather than  SDCARD, i guess.

    sry , i misread a bit,

    the SD is supported SDA_SD2_DATA3.

     

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • tjmerics
    0 tjmerics over 12 years ago in reply to tusharp

    except I haven't seen a board with a spi flash installed.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • tjmerics
    0 tjmerics over 12 years ago in reply to tusharp

    except I haven't seen a board with a spi flash installed.