RIoTboard
  • Products
  • Dev Tools
  • Single-Board Computers
  • RIoTboard
  • More
  • Cancel
RIoTboard
Forum Serial connection (j18) is definitely dead...
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join RIoTboard to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 4 replies
  • Answers 1 answer
  • Subscribers 24 subscribers
  • Views 734 views
  • Users 0 members are here
  • problem
  • j18
  • riotboard
Related

Serial connection (j18) is definitely dead...

mubase
mubase over 12 years ago

Hi all. I have been having immense fun with my Riotboard, getting a debian distribution working and figuring out how to program audio and the GPIOs using python and C++. This was up till about a 2 weeks ago when the serial port (j18) decided to stop working. It simply stopped being able to send or recieve anything.. I checked the connections about 5 times and even bought a new CP2102 USB to TTL converter and the result was the same.. No response either way when the ground wire is connected, and no working carriage return or display when it isn't....I have contacted Elemnt 14 technical about it but they are being very slow with their response..Has anyone else had a serial port blow out on them?

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    I've never had the misfortune to kill a serial port.

    All I would say is that if you look at the schematic these pins go directly to the SoC, there's no buffering or protection.  It's likely to be easier to overload these than you'd think and the only fix is to replace the SoC.  Realistically that's going to mean a new board..

     

    If there's nothing else wrong, then it may be possible to use one of the other uart ports instead.  How easy that would be depends a lot on whether you're using android or linux and just how good you are at tracking down all of the places you need to configure the new port.

     

    Further debugging may be possible if you have access to a scope and other appropriate equipment..  A starting point for this is to connect the TX & RX on your USB cable together - having done that what you type in the terminal program should get sent back to the screen - simple way to check the cable is functional to some degree..

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • mubase
    0 mubase over 12 years ago in reply to e14 Contributor

    Hi Selsinor,.

    Well. The situation has got worse. My board has DIED. :...(    image

    I had it plugged in to the usual 5V 1A PSU. I was looking into rebuilding the ubuntu linux and adding support for UARTs and the LED suddenly went out. All contact lost. I unplugged and replugged the power back in. Nothing happened and the imx chip started to get hot..

    I can only assume the board is now dead.

    I've contacted Farnell about returns and hope to get a reply sometime soon. (hope..)

    Now I am RIoTboardless.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • mubase
    0 mubase over 12 years ago in reply to e14 Contributor

    Hi Selsinor,.

    Well. The situation has got worse. My board has DIED. :...(    image

    I had it plugged in to the usual 5V 1A PSU. I was looking into rebuilding the ubuntu linux and adding support for UARTs and the LED suddenly went out. All contact lost. I unplugged and replugged the power back in. Nothing happened and the imx chip started to get hot..

    I can only assume the board is now dead.

    I've contacted Farnell about returns and hope to get a reply sometime soon. (hope..)

    Now I am RIoTboardless.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • tusharp
    0 tusharp over 12 years ago in reply to mubase

    Well. The situation has got worse. My board has DIED

    Now I am RIoTboardless.

    sry image to know that, but the Riot journey shouldn't stop.

     

    I have talked to support team and its been understood the board is at fault and requested to give a new replacement board.

    the procedure will take a few days.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • mubase
    0 mubase over 12 years ago in reply to tusharp

    Happy to announce that a UPS delivery arrived today with a replacement board!

    The faulty one has been sent back as per insructions that were sent to me by the lovely people at Element14.

    Thanks to everyone and especially Tushar for their support. image

    As a token of my appreciation, here's a picture of one of our local smooberries (i mean squirrels...)

    image

    The RIoT continues!!