RIoTboard
  • Products
  • Dev Tools
  • Single-Board Computers
  • RIoTboard
  • More
  • Cancel
RIoTboard
Forum Board questions
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join RIoTboard to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 1 reply
  • Subscribers 23 subscribers
  • Views 418 views
  • Users 0 members are here
Related

Board questions

e14 Contributor
e14 Contributor over 12 years ago

I have just a few questions about the RIoT Board design. I'm trying to figure what the intention was behind the decisions.

 

Schematic '08 IMX6Q_SOC_B' has the PCIE_REXT (A2) pin to ground. The spec sheet (http://cache.freescale.com/files/32bit/doc/data_sheet/IMX6SDLCEC.pdf) says to connect it to ground through an external 200R precision resistor, but not what to do if the circuit is not used. Was this done because PCIe isn't used and thus doesn't need to do impedance calibration? Shouldn't it still be terminated?

 

Schematics '07 IMX6Q_SOC_A' and '18 Boot_UART2' has a push button connected to POR (C11) instead of On/Off (D12) on the processor. I assume it is forcing a reset in hardware by pulling the line low. However the On/Off pin can be used for software reseting (long pressing forces hardware reset). The On/Off pin has an offsheet connector that doesn't connect anywhere. I'm not going to lie, but this baffles me. I don't need a software reset on my design, but I am curious as to what the reasoning was.

  • Sign in to reply
  • Cancel
  • tusharp
    0 tusharp over 12 years ago

    ON/OFF signal is used for power management

    External programmable PMIC is used on Riot..