RIoTboard
  • Products
  • Dev Tools
  • Single-Board Computers
  • RIoTboard
  • More
  • Cancel
RIoTboard
Forum Yacto build error
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join RIoTboard to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 6 replies
  • Subscribers 25 subscribers
  • Views 981 views
  • Users 0 members are here
  • yacto
  • riotboard
  • embedded
  • bsp
  • linux
Related

Yacto build error

e14 Contributor
e14 Contributor over 12 years ago

  i have downloaded the latest image its working but not getting riot board login .i am getting only sh my display also working up to getting logo after that its not working .i am preparing image by using Yacto when i gave bitbake  build is failed because of two packages i double check SRC_URI and did but getting same error.Yacto error is below
 

  WARNING: Failed to fetch URL
http://www.freescale.com/lgfiles/NMG/MAD/YOCTO/fsl-gpu-sdk-1.1.bin/libfslcodec-3.0.11.bin;fsl-eula=true, attempting MIRRORS if available
  ERROR: Fetcher failure: Fetch command failed with exit code 8, output:

  http://www.freescale.com/lgfiles/NMG/MAD/YOCTO/fsl-gpu-sdk-1.1.bin/libfslcodec-3.0.11.bin:

  2014-08-05 15:18:07 ERROR 404: Not Found.

   ERROR: Function failed: Fetcher failure for URL: '
http://www.freescale.com/lgfiles/NMG/MAD/YOCTO/fsl-gpu-sdk-1.1.bin/libfslcodec-3.0.11.bin;fsl-eula=true'. Unable to fetch URL from any source.
  ERROR:

   Logfile of failure stored in:

  /home/teju/fsl-arm-yocto-bsp/build/tmp/work/riotboard-poky-linux-gnueabi/libfslcodec/3.0.11-r0/temp/log.do_fetch.18930

  ERROR:

   Task 1615

  (/home/teju/fsl-arm-yocto-bsp/sources/meta-fsl-bsp-release/imx/meta-fsl-arm/recipes-multimedia/libfslcodec/libfslcodec_3.0.11.bb,

   do_fetch) failed with exit code '1'

  NOTE: Tasks Summary: Attempted 1944 tasks of which 1935 didn't need to be rerun and 1 failed.

  Waiting for 0 running tasks to finish:

   Summary: 1 task failed:

 

 

  /home/teju/fsl-arm-yocto-bsp/sources/meta-fsl-bsp-release/imx/meta-fsl-arm/recipes-multimedia/libfslcodec/libfslcodec_3.0.11.bb,

   do_fetch

  Summary: There was 1 WARNING message shown.

  Summary: There were 2 ERROR messages shown, returning a non-zero exit code.

 

 

  • Sign in to reply
  • Cancel
  • tusharp
    0 tusharp over 12 years ago
    not getting riot board login

    use root as login name.

    i am getting only sh my display

    gui support is not enabled in the image

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • tusharp
    0 tusharp over 12 years ago
    build is failed because of two packages

       plz share your host environment .

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • tusharp
    0 tusharp over 12 years ago

    any warnings like below, then your host OS is not supported

    WARNING: Host distribution "Fedora" has not been validated with this version of the build system; you may possibly experience unexpected failures. It is recommended that you use a tested distribution.

     

    what host OS are you using ??

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to tusharp

    I am using linux Os ubuntu 12.04

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • bwelsby
    0 bwelsby over 12 years ago

    the URL with error is http://www.freescale.com/lgfiles/NMG/MAD/YOCTO/fsl-gpu-sdk-1.1.bin/libfslcodec-3.0.11.bin;fsl-eula=true,

    This looks like two files are in one URL,  I checked and found I can download each of the files  with the following


    http://www.freescale.com/lgfiles/NMG/MAD/YOCTO/fsl-gpu-sdk-1.1.bin

    and

    http://www.freescale.com/lgfiles/NMG/MAD/YOCTO/libfslcodec-3.0.11.bin


    Brian

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to bwelsby

    Individually  in downloads directory i tried with the same URL its downloading and saved also but when i gave bitbake it was producing the same error . it will work with wget  in bit bake same problem arising again