RIoTboard
  • Products
  • Dev Tools
  • Single-Board Computers
  • RIoTboard
  • More
  • Cancel
RIoTboard
Forum Trouble with ttl to usb interface
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join RIoTboard to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 7 replies
  • Subscribers 28 subscribers
  • Views 2445 views
  • Users 0 members are here
  • interrupt
  • ttl
  • usb
  • riotboard
  • display
  • interface
  • usbttl
  • prompt
  • keypress
  • booting
Related

Trouble with ttl to usb interface

e14 Contributor
e14 Contributor over 11 years ago

Hey guys, riotboard noob here!  A local computer store had a USB to TTL serial cable based on the PL2303 chip and I can see the boot information through screen and minicom as my riotboard is booting up so that's working just fine.  However, when it comes to the prompt where I can press any key to interrupt the boot sequence, nothing works.  Neither keypresses on the host computer (Ubuntu Linux) or an attached usb keyboard will interrupt the 3 second timer.  What am I doing wrong?  I apologize in advance if this is a painfully obvious problem.  I'm really stumped, though!

 

Background: I purchased the 7" LCD display and connector board for my riotboard.  I'm following the documentation where it instructs me to interrupt the boot sequence so I can enter the appropriate parameters to enable the screen.

  • Sign in to reply
  • Cancel

Top Replies

  • johnbeetem
    johnbeetem over 11 years ago +1
    I'm not a RIoTboard user but I've done a lot of UART. Here are a few things I'd try. First, make sure the USB UART dongle is working by itself. Unplug it from the RIoTboard and connect the RX and TX bits…
Parents
  • radiatortwo
    0 radiatortwo over 11 years ago

    To cancel the boot you have to do that over your serial connection.

    With an attached USB Keyboard this won´t work.

     

    What terminal progam are you using to connect on the serial port?

    You have to press a key in this terminal program to cancel the boot.

     

    I´m mainly using putty in Windows. But as far as I know "screen" should be working on the terminal in Ubuntu.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • radiatortwo
    0 radiatortwo over 11 years ago

    To cancel the boot you have to do that over your serial connection.

    With an attached USB Keyboard this won´t work.

     

    What terminal progam are you using to connect on the serial port?

    You have to press a key in this terminal program to cancel the boot.

     

    I´m mainly using putty in Windows. But as far as I know "screen" should be working on the terminal in Ubuntu.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to radiatortwo

    I've used both screen and minicom.  They both allow me to see the output when the board is booting but it's not accepting any keystrokes in return.