RIoTboard
  • Products
  • Dev Tools
  • Single-Board Computers
  • RIoTboard
  • More
  • Cancel
RIoTboard
Forum Trouble with ttl to usb interface
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join RIoTboard to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 7 replies
  • Subscribers 28 subscribers
  • Views 2443 views
  • Users 0 members are here
  • interrupt
  • ttl
  • usb
  • riotboard
  • display
  • interface
  • usbttl
  • prompt
  • keypress
  • booting
Related

Trouble with ttl to usb interface

e14 Contributor
e14 Contributor over 11 years ago

Hey guys, riotboard noob here!  A local computer store had a USB to TTL serial cable based on the PL2303 chip and I can see the boot information through screen and minicom as my riotboard is booting up so that's working just fine.  However, when it comes to the prompt where I can press any key to interrupt the boot sequence, nothing works.  Neither keypresses on the host computer (Ubuntu Linux) or an attached usb keyboard will interrupt the 3 second timer.  What am I doing wrong?  I apologize in advance if this is a painfully obvious problem.  I'm really stumped, though!

 

Background: I purchased the 7" LCD display and connector board for my riotboard.  I'm following the documentation where it instructs me to interrupt the boot sequence so I can enter the appropriate parameters to enable the screen.

  • Sign in to reply
  • Cancel

Top Replies

  • johnbeetem
    johnbeetem over 11 years ago +1
    I'm not a RIoTboard user but I've done a lot of UART. Here are a few things I'd try. First, make sure the USB UART dongle is working by itself. Unplug it from the RIoTboard and connect the RX and TX bits…
Parents
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    Thanks for all of the replies, gentlemen!  I am going to pick up a multimeter after work today and check the voltage and also try the echo test referenced above.

     

    But, yes, you are correct - I can see the output as the machine is booting up.  Could it be a permissions problem maybe?  Or maybe the usb port on the laptop I've been using is bad?

     

    Related question:  if I pick up a dedicated serial port card for my desktop, is it just a 1:1 straight pin mapping between the card's serial port rx/tx pins and the rx/tx pins on the riotboard?

     

    by the way, it's nice to see a vibrant and helpful community for this device!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • tusharp
    0 tusharp over 11 years ago in reply to e14 Contributor

    Could it be a permissions problem maybe?

    IF my detected device is /dev/ttyUSB3 , i use below command.

     

    sudo screen /dev/ttyUSB3 115200 8N1


    i guess sudo (super user) required else not possible to write down the TX, read shouldn't be a problem.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • tusharp
    0 tusharp over 11 years ago in reply to e14 Contributor

    Could it be a permissions problem maybe?

    IF my detected device is /dev/ttyUSB3 , i use below command.

     

    sudo screen /dev/ttyUSB3 115200 8N1


    i guess sudo (super user) required else not possible to write down the TX, read shouldn't be a problem.