RIoTboard
  • Products & Partners
  • Dev Tools
  • Single-Board Computers
  • RIoTboard
  • More
  • Cancel
RIoTboard
Forum Unable to do initial 'make' on Jelly Bean (4.3)
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join RIoTboard to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 8 replies
  • Answers 2 answers
  • Subscribers 24 subscribers
  • Views 2245 views
  • Users 0 members are here
Related

Unable to do initial 'make' on Jelly Bean (4.3)

e14 Contributor
e14 Contributor over 11 years ago

Hi,

 

I'm attempting to work with the RIoTboard for the first time and have run into the issue of creating a flash-able android image. I downloaded the Jelly Bean (Android 4.3) code and got the repo all initialized and synced with no issues. There were no issues with the '. build/envsetup.sh' and choosing the desired lunch item (23 - RIoTboard_6solo-eng), however the 'make -j8' continues to fail regardless of what I try.

 

Please see the attached log from the make command. Note that I had already tried to make the images, thus the reason that the log is so short. However, the issues I am having are fully encompassed in the provided log.

 

As can be seen, there seems to be some issue with the EthernetStateTracker.java includes. There are multiple (22) symbols that are supposed to be included that have not been found. I am also getting Error 41 in regards to a debug .jar file and I'm being told that I'm using deprecated APIs.

 

I am running this with JDK 1.6.0_45 at the moment. I have tried the same process with both the latest JDK 1.5 and JDK 1.8 versions, to no avail.

 

If someone has run across this and knows the solution, I would love to find the answer. My Googling has turned up absolutely nothing helpful enough to solve my problem. Again, I am simply trying to do the first make on the downloaded Android source code. I have not modified it in any way, and yet it will not build.

 

Things I have tried:

  1. Completely commenting out EthernetStateTracker.java. Similar symbol missing errors simply occurred in other .java files
  2. Running 'make clean', 'make clean -j8', 'make update-api', 'make', etc.
  3. Creating a custom classes-full-debug.jar file in the folder where Error 41 popped up (though this might have been wrong?)
  4. Completely deleting, re-downloading, re-initializing, and re-syncing repository.
  5. Multiple versions of Java JDK.
  6. Re-download Jelly Bean code from riotboard.org (as opposed to previous link on the Riotboard Element 14 site).
  7. There are probably more that I can't remember off the top of my head image

 

Thanks,

Caleb

 

P.S. Just noticed that for some reason the log file I attached defaulted to a .zip file, so I'm also pasting the log down below in case you didn't want to have to download and unzip a file just to read the log image

 

riot_source: make -j8

============================================

PLATFORM_VERSION_CODENAME=REL

PLATFORM_VERSION=4.3

TARGET_PRODUCT=RIoTboard_6solo

TARGET_BUILD_VARIANT=eng

TARGET_BUILD_TYPE=release

TARGET_BUILD_APPS=

TARGET_ARCH=arm

TARGET_ARCH_VARIANT=armv7-a-neon

TARGET_CPU_VARIANT=cortex-a9

HOST_ARCH=x86

HOST_OS=linux

HOST_OS_EXTRA=Linux-3.13.0-55-generic-x86_64-with-Ubuntu-12.04-precise

HOST_BUILD_TYPE=release

BUILD_ID=1.0.0-rc2

OUT_DIR=out

============================================

build/core/Makefile:32: warning: overriding commands for target `out/target/product/RIoTboard_6solo/system/etc/wifi/wpa_supplicant.conf'

build/core/base_rules.mk:520: warning: ignoring old commands for target `out/target/product/RIoTboard_6solo/system/etc/wifi/wpa_supplicant.conf'

build/core/Makefile:32: warning: overriding commands for target `out/target/product/RIoTboard_6solo/system/etc/permissions/android.software.live_wallpaper.xml'

build/core/base_rules.mk:520: warning: ignoring old commands for target `out/target/product/RIoTboard_6solo/system/etc/permissions/android.software.live_wallpaper.xml'

No private recovery resources for TARGET_DEVICE RIoTboard_6solo

target Java: voip-common (out/target/common/obj/JAVA_LIBRARIES/voip-common_intermediates/classes)

make -C kernel_imx -j8 uImage ARCH=arm CROSS_COMPILE=`pwd`/prebuilts/gcc/linux-x86/arm/arm-eabi-4.6/bin/arm-eabi-

make[1]: Entering directory `/home/lattice/riot_source/kernel_imx'

make[1]: warning: -jN forced in submake: disabling jobserver mode.

  CHK     include/linux/version.h

target Symbolic: libcutils (out/target/product/RIoTboard_6solo/symbols/system/lib/libcutils.so)

target Strip: libsync (out/target/product/RIoTboard_6solo/obj/lib/libsync.so)

target Strip: libnativehelper (out/target/product/RIoTboard_6solo/obj/lib/libnativehelper.so)

target Symbolic: libicuuc (out/target/product/RIoTboard_6solo/symbols/system/lib/libicuuc.so)

target Symbolic: libcrypto (out/target/product/RIoTboard_6solo/symbols/system/lib/libcrypto.so)

Install: out/target/product/RIoTboard_6solo/system/lib/libsync.so

Copying: out/target/common/obj/APPS/ApplicationsProvider_intermediates/classes-jarjar.jar

Copying: out/target/common/obj/APPS/BasicDreams_intermediates/classes-jarjar.jar

Copying: out/target/common/obj/APPS/BackupRestoreConfirmation_intermediates/classes-jarjar.jar

Copying: out/target/common/obj/JAVA_LIBRARIES/javax.obex_intermediates/classes-jarjar.jar

Copying: out/target/common/obj/JAVA_LIBRARIES/android-support-v4-honeycomb-mr2_intermediates/emma_out/lib/classes-jarjar.jar

Copying: out/target/common/obj/APPS/SoundRecorder_intermediates/classes-jarjar.jar

Note: frameworks/opt/net/voip/src/java/com/android/server/sip/SipService.java uses or overrides a deprecated API.

Note: Recompile with -Xlint:deprecation for details.

Note: frameworks/opt/net/voip/src/java/com/android/server/sip/SipService.java uses unchecked or unsafe operations.

Note: Recompile with -Xlint:unchecked for details.

Copying: out/target/common/obj/APPS/CalendarProvider_intermediates/classes-jarjar.jar

Copying: out/target/common/obj/APPS/CertInstaller_intermediates/classes-jarjar.jar

Copying: out/target/common/obj/JAVA_LIBRARIES/com.android.phone.shared_intermediates/classes-jarjar.jar

Copying: out/target/common/obj/APPS/DefaultContainerService_intermediates/classes-jarjar.jar

Copying: out/target/common/obj/JAVA_LIBRARIES/junit-runner_intermediates/classes-jarjar.jar

Copying: out/target/common/obj/APPS/DownloadProvider_intermediates/classes-jarjar.jar

Copying: out/target/common/obj/APPS/DownloadProviderUi_intermediates/classes-jarjar.jar

target Java: Ethernet (out/target/common/obj/APPS/Ethernet_intermediates/classes)

Copying: out/target/common/obj/JAVA_LIBRARIES/com.android.location.provider_intermediates/classes-jarjar.jar

Copying: out/target/common/obj/JAVA_LIBRARIES/android-support-v8-renderscript_intermediates/classes-jarjar.jar

target Java: HTMLViewer (out/target/common/obj/APPS/HTMLViewer_intermediates/classes)

target Java: InputDevices (out/target/common/obj/APPS/InputDevices_intermediates/classes)

target Java: KeyChain (out/target/common/obj/APPS/KeyChain_intermediates/classes)

target Java: LiveWallpapers (out/target/common/obj/APPS/LiveWallpapers_intermediates/classes)

target Java: LiveWallpapersPicker (out/target/common/obj/APPS/LiveWallpapersPicker_intermediates/classes)

target Java: MagicSmokeWallpapers (out/target/common/obj/APPS/MagicSmokeWallpapers_intermediates/classes)

packages/apps/Ethernet/src/android/net/ethernet/EthernetStateTracker.java:24: cannot find symbol

symbol  : class scanResult

location: class android.net.EthernetDataTracker

import android.net.EthernetDataTracker.scanResult;

                                      ^

packages/apps/Ethernet/src/android/net/ethernet/EthernetStateTracker.java:25: cannot find symbol

symbol  : class connectResult

location: class android.net.EthernetDataTracker

import android.net.EthernetDataTracker.connectResult;

                                      ^

target Java: MediaProvider (out/target/common/obj/APPS/MediaProvider_intermediates/classes)

packages/apps/Ethernet/src/android/net/ethernet/EthernetMonitor.java:57: cannot find symbol

symbol  : method setHandler(android.net.ethernet.EthernetMonitor.NetStateHandler)

location: class android.net.EthernetDataTracker

        mDataTracker.setHandler(sInstance);

                    ^

packages/apps/Ethernet/src/android/net/ethernet/EthernetStateTracker.java:197: cannot find symbol

symbol  : method getEthernetCarrierState(java.lang.String)

location: class android.net.EthernetDataTracker

        return mDataTracker.getEthernetCarrierState(iface);

                           ^

packages/apps/Ethernet/src/android/net/ethernet/EthernetStateTracker.java:238: cannot find symbol

symbol  : method configureIfc(java.lang.String,java.lang.String,java.lang.String,java.lang.String,java.lang.String,java.lang.String,java.lang.String,boolean)

location: class android.net.EthernetDataTracker

        mDataTracker.configureIfc(m.getIfName(),

                    ^

packages/apps/Ethernet/src/android/net/ethernet/EthernetStateTracker.java:255: cannot find symbol

symbol  : method configureIfc(java.lang.String,java.lang.String,java.lang.String,java.lang.String,java.lang.String,java.lang.String,java.lang.String,boolean)

location: class android.net.EthernetDataTracker

            isOK = mDataTracker.configureIfc(m.getIfName(),

                               ^

packages/apps/Ethernet/src/android/net/ethernet/EthernetStateTracker.java:271: cannot find symbol

symbol  : method setUserFlag(boolean)

location: class android.net.EthernetDataTracker

        mDataTracker.setUserFlag(flag);

                    ^

packages/apps/Ethernet/src/android/net/ethernet/EthernetStateTracker.java:346: cannot find symbol

symbol  : class scanResult

location: class android.net.ethernet.EthernetStateTracker

        scanResult sR;

        ^

packages/apps/Ethernet/src/android/net/ethernet/EthernetStateTracker.java:347: cannot find symbol

symbol  : class connectResult

location: class android.net.ethernet.EthernetStateTracker

        connectResult cR;

        ^

packages/apps/Ethernet/src/android/net/ethernet/EthernetStateTracker.java:352: cannot find symbol

symbol  : variable ETHER_MSG_ADD_INTERFACE

location: class android.net.EthernetDataTracker

            case EthernetDataTracker.ETHER_MSG_ADD_INTERFACE:

                                    ^

packages/apps/Ethernet/src/android/net/ethernet/EthernetStateTracker.java:353: cannot find symbol

symbol  : class scanResult

location: class android.net.ethernet.EthernetStateTracker

                sR = (scanResult)msg.obj;

                      ^

packages/apps/Ethernet/src/android/net/ethernet/EthernetStateTracker.java:363: cannot find symbol

symbol  : variable ETHER_MSG_INTERFACE_STATUS_CHANGE

location: class android.net.EthernetDataTracker

            case EthernetDataTracker.ETHER_MSG_INTERFACE_STATUS_CHANGE:

                                    ^

packages/apps/Ethernet/src/android/net/ethernet/EthernetStateTracker.java:364: cannot find symbol

symbol  : class scanResult

location: class android.net.ethernet.EthernetStateTracker

                sR = (scanResult)msg.obj;

                      ^

packages/apps/Ethernet/src/android/net/ethernet/EthernetStateTracker.java:373: cannot find symbol

symbol  : variable ETHER_MSG_INTERFACE_STATUS_CHANGE

location: class android.net.EthernetDataTracker

                    sendMessage(EthernetDataTracker.ETHER_MSG_INTERFACE_STATUS_CHANGE, sR.iFace);

                                                   ^

packages/apps/Ethernet/src/android/net/ethernet/EthernetStateTracker.java:378: cannot find symbol

symbol  : variable ETHER_MSG_CONNECTED_SUCCESS

location: class android.net.EthernetDataTracker

            case EthernetDataTracker.ETHER_MSG_CONNECTED_SUCCESS:

                                    ^

packages/apps/Ethernet/src/android/net/ethernet/EthernetStateTracker.java:379: cannot find symbol

symbol  : class connectResult

location: class android.net.ethernet.EthernetStateTracker

                cR = (connectResult)msg.obj;

                      ^

packages/apps/Ethernet/src/android/net/ethernet/EthernetStateTracker.java:390: cannot find symbol

symbol  : variable ETHER_MSG_CONNECTED_SUCCESS

location: class android.net.EthernetDataTracker

                    sendMessage(EthernetDataTracker.ETHER_MSG_CONNECTED_SUCCESS, cR.iFace);

                                                   ^

packages/apps/Ethernet/src/android/net/ethernet/EthernetStateTracker.java:395: cannot find symbol

symbol  : variable ETHER_MSG_CONNECTED_FAILED

Note: packages/apps/HTMLViewer/src/com/android/htmlviewer/HTMLViewerActivity.java uses or overrides a deprecated API.

Note: Recompile with -Xlint:deprecation for details.

location: class android.net.EthernetDataTracker

            case EthernetDataTracker.ETHER_MSG_CONNECTED_FAILED:

                                    ^

packages/apps/Ethernet/src/android/net/ethernet/EthernetStateTracker.java:396: cannot find symbol

symbol  : class connectResult

location: class android.net.ethernet.EthernetStateTracker

                cR = (connectResult)msg.obj;

                      ^

packages/apps/Ethernet/src/android/net/ethernet/EthernetStateTracker.java:406: cannot find symbol

symbol  : variable ETHER_MSG_CONNECTED_FAILED

location: class android.net.EthernetDataTracker

                    sendMessage(EthernetDataTracker.ETHER_MSG_CONNECTED_FAILED, cR.iFace);

                                                   ^

packages/apps/Ethernet/src/android/net/server/EthernetService.java:63: cannot find symbol

symbol  : method clearConnections()

location: class android.net.EthernetDataTracker

        mDataTracker.clearConnections();

                    ^

packages/apps/Ethernet/src/android/net/server/EthernetService.java:64: cannot find symbol

symbol  : method scanInterface()

location: class android.net.EthernetDataTracker

        mDataTracker.scanInterface();

                    ^

Note: Some input files use or override a deprecated API.

Note: Recompile with -Xlint:deprecation for details.

22 errors

make: *** [out/target/common/obj/APPS/Ethernet_intermediates/classes-full-debug.jar] Error 41

make: *** Waiting for unfinished jobs....

Note: packages/apps/KeyChain/src/com/android/keychain/KeyChainActivity.java uses or overrides a deprecated API.

Note: Recompile with -Xlint:deprecation for details.

Note: Some input files use or override a deprecated API.

Note: Recompile with -Xlint:deprecation for details.

Note: Some input files use or override a deprecated API.

Note: Recompile with -Xlint:deprecation for details.

  CHK     include/generated/utsrelease.h

make[2]: `include/generated/mach-types.h' is up to date.

  CALL    scripts/checksyscalls.sh

Note: Some input files use or override a deprecated API.

Note: Recompile with -Xlint:deprecation for details.

Note: packages/providers/MediaProvider/src/com/android/providers/media/MediaProvider.java uses unchecked or unsafe operations.

Note: Recompile with -Xlint:unchecked for details.

  CHK     include/generated/compile.h

  Kernel: arch/arm/boot/Image is ready

  SHIPPED arch/arm/boot/compressed/lib1funcs.S

  AS      arch/arm/boot/compressed/lib1funcs.o

  LD      arch/arm/boot/compressed/vmlinux

  OBJCOPY arch/arm/boot/zImage

  Kernel: arch/arm/boot/zImage is ready

  UIMAGE  arch/arm/boot/uImage

Image Name:   Linux-3.0.35-06440-g69a9d24

Created:      Tue Jun 23 10:36:38 2015

Image Type:   ARM Linux Kernel Image (uncompressed)

Data Size:    4735296 Bytes = 4624.31 kB = 4.52 MB

Load Address: 10008000

Entry Point:  10008000

  Image arch/arm/boot/uImage is ready

make[1]: Leaving directory `/home/lattice/riot_source/kernel_imx'

install -D kernel_imx/arch/arm/boot/uImage  out/target/product/RIoTboard_6solo/uImage

install -D kernel_imx/arch/arm/boot/zImage  out/target/product/RIoTboard_6solo/kernel

 

Message was edited by: Caleb Timms

Attachments:
make_log.txt.zip
  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    I have exactly the same error, but no solution yet. But actually I'm more interested in compiling kitkat. which also did not work for yet. But this will be discussed in a separate topic.

    If someone finds a solution for jb I would also apprechiate it. I will also go on trying with both.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    I have exactly the same error, but no solution yet. But actually I'm more interested in compiling kitkat. which also did not work for yet. But this will be discussed in a separate topic.

    If someone finds a solution for jb I would also apprechiate it. I will also go on trying with both.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to e14 Contributor

    Hi Tekken Tux,

     

    I've located a solution (though a highly imperfect one, depending on your application) and wanted to make sure you had access to it. The issue appears to be with the Ethernet modules they added in to the most recent commit of the Jelly Bean code, and you can completely disable the inclusion of the Ethernet modules by doing the following:

     

    1. Locate the make file - build/target/product/generic_no_telephony.mk

    2. Open in editor and remove the entry 'Ethernet \' from this file (it occurs within the first 50 or so lines and was the only instance of 'Ethernet' in my file. Might want to run a text search just to be sure for yourself).

     

    Once I removed the Ethernet stuff, I was able to successfully make the solution (and get the resulting .img files in out/target/product/RIoTboard_6solo/. Unfortunately, if you are attempting to make use of the Ethernet modules, then I'm not sure this solution will be of any use to you. I was still unable to find an actual patch or solution to keep the Ethernet functionality and it appears literally impossible to get in contact with anyone at RIoTboard considering their email address bounces back emails (I've also sent a message to Embest Tech with no response).

     

    I just got that at the end of last week and am going to attempt to flash the newly created image onto the RIoTboard this morning. If I have any further issues, I'll comment them below, but no new posts should be a good sign from me. Let me know if these steps solve your problem.

     

    Caleb

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to e14 Contributor

    Thanks for this tip. In the long term I would like to have ethernet support, but it's not important for now. So if this works for now, It may be worth investing some time to fix the ethernet thing later.

    I will try that and let you know. Thanks

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to e14 Contributor

    One annoyance I've found: You can't flash the images from Linux, apparently..? Is this correct? The MfgTool provided on the website runs on Windows, not Linux. So I have to build my images on Linux, then port it over to be able to flash it?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to e14 Contributor

    Ethernet:

    Disabling Ethernet as described above worked for me, so I could compile and boot the system.

     

    MfgTool:

    Edit: did you try this one: http://riotboard.org/download/Mfg_Tool-Linux_Image.zip ?

    I did not use the MfgTool or the eMMC yet, I just dd the images to SD card. This does not answer your question, but it also took me some time to find out, so I post it here, for others:

     

     

    Create SD card:

    http://riotboard.org/download/Android-Users-Guide.pdf

    in "out/target/product/RIoTboard_6solo" run the following:

    1.) create partition table on sd card:

    ./device/fsl/common/tools/fsl-sdcard-partition.sh /dev/sdX

    2.) copy bootloader to sd card:

    dd if=u-boot.bin of=/dev/sdb bs=1K skip=1 seek=1 ; sync

    3.) copy all images to sd card:

    dd if=boot.img of=/dev/sdX1 ; sync

    dd if=recovery.img of=/dev/sdX2 ; sync

    dd if=system.img of=/dev/sdX5 ; sync

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to e14 Contributor

    I'm not using an SD card, I'm just flashing straight to the eMMC. However, I was able to use Fastboot on Windows to successfully get the images flashed to the RIoTboard. Uboot was giving me issues, for whatever reason, so I just scrapped it and went for Fastboot instead and will continue to use that until it gives me some error or doesn't have the functionality I need! image

     

    Caleb

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • stmorgan
    0 stmorgan over 9 years ago in reply to e14 Contributor

    See the MANUALLY APPLY GITHUB REVERSION section of this post for a workaround to this issue:

     

    RIoTboard - Android Jelly Bean Build on openSUSE 13.2 x86_64