RIoTboard
  • Products
  • Dev Tools
  • Single-Board Computers
  • RIoTboard
  • More
  • Cancel
RIoTboard
Forum Riotboard Android - U-Boot 2015
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join RIoTboard to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 2 replies
  • Subscribers 24 subscribers
  • Views 738 views
  • Users 0 members are here
Related

Riotboard Android - U-Boot 2015

phil_94
phil_94 over 11 years ago

Hi guys,

 

I have successfully downloaded, compiled and flashed an Android BSP on the RIotboard following the instructions of RIotBoard user manual (https://www.dropbox.com/s/xap0b9am0bkbi1f/RIoTboard%20User%20Manual_V2.1.pdf?dl=0) . The thing is, it is using an old version of U-Boot (2009) with a custom booti implementation to load the boot.img in RAM, and I need to use last version of U-Boot (2015) for multi boot purposes and flat device tree support of newer kernels.

 

From what I've seen, the newest version of U-Boot has already built-in support for loading Android images if you define CONFIG_ANDROID_IMAGE flag ; so far I have managed to get it to load my boot.img blob, parse header / kernel / ramdisk files, starts the kernel but then nothing happens (it's stuck after Starting kernel... output) . Also I have checked that the  command line is ok so I don't think it's a kernel command line issue.

 

I also tried porting the u-boot 2009 custom booti function to u-boot 2015 ; it compiled ok but i get mmc read driver errors at execution (v7_dcache_inval_range - start address is not aligned - 0x4ffa703)

 

So my question is : has anyone successfully booted Android 4.4 for Riotboard with newest U-boot (2015) ?

 

Thanks for reading me

 

Phil

  • Sign in to reply
  • Cancel
Parents
  • phil_94
    0 phil_94 over 11 years ago

    OK I solved the issue ; seems like the arch number passed when calling the kernel was wrong : by default, when configuring u-boot 2015 with riotboard_defconfig, and running the bootm command on a preloaded android boot.img image, the linux arch number passed is 0, and the kernel expected 4000 (as defined in the freescale custom U-Boot 2009 include/asm-arm/mach-types.h :

     

    #define MACH_TYPE_MX6SOLO_RIoTboard4000


    After that the kernel starts ok. Hope this can be useful for anyone else.

     

    Phil

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to phil_94

    Hey Phil,

     

    I'm trying to switch to the new U-Boot as well but I'm having some trouble.

     

    I've added:

    CONFIG_ANDROID_IMAGE=y

    to:

    u-boot/configs/riotboard_defconfig

     

    How do I set the arch_number?

     

    Also, what would the boot.scr look like?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to phil_94

    Hey Phil,

     

    I'm trying to switch to the new U-Boot as well but I'm having some trouble.

     

    I've added:

    CONFIG_ANDROID_IMAGE=y

    to:

    u-boot/configs/riotboard_defconfig

     

    How do I set the arch_number?

     

    Also, what would the boot.scr look like?