RIoTboard
  • Products
  • Dev Tools
  • Single-Board Computers
  • RIoTboard
  • More
  • Cancel
RIoTboard
Forum Need help adding an SPI device to RIoTBoard device tree
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join RIoTboard to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 1 reply
  • Subscribers 23 subscribers
  • Views 423 views
  • Users 0 members are here
  • yocto
  • riotboard
  • device-tree
  • i.mx6
Related

Need help adding an SPI device to RIoTBoard device tree

jomag
jomag over 10 years ago

Hi

 

I just got a custom Linux dist built using Yocto running on the RIoTboard. Happy days!

 

Now I need to add an SPI-device to the board. I've done this successfully on Raspberry Pi and an Olinuxino (i.MX233) before by modifying the device tree, for example:

 

diff --git a/arch/arm/boot/dts/imx23-olinuxino.dts b/arch/arm/boot/dts/imx23-olinuxino.dts

index fc766ae..a574822 100644

--- a/arch/arm/boot/dts/imx23-olinuxino.dts

+++ b/arch/arm/boot/dts/imx23-olinuxino.dts

@@ -64,7 +64,16 @@

                 compatible = "fsl,imx23-spi";

                 pinctrl-names = "default";

                 pinctrl-0 = <&spi2_pins_a>;

+                clock-frequency = <1000000>;

                 status = "okay";

+

+                mrf24j40@0 {

+                    compatible = "mrf24j40";

+                    spi-max-frequency = <500000>;

+                    reg = <0>;

+                    interrupts = <31 1>;

+                                       interrupt-parent = <&gpio0>;

+                };

             };

         };

 

I'm unsure how to do the same on the RIoTboard/i.MX6 and I have failed to find good examples.

 

The device I need to add requires SPI-connectivity (MOSI, MISO, SCK, CS) and an IRQ. I may have to use a reset-pin as well.

 

Could anyone give me some help/hints? I'm using a 4.1 kernel currently.

  • Sign in to reply
  • Cancel
  • kylemills
    kylemills over 10 years ago

    this my help:

     

    https://community.freescale.com/thread/303513

     

    https://community.freescale.com/thread/322760