Freescale i.MX6 Development Platforms
  • Products & Partners
  • Dev Tools
  • Single-Board Computers
  • Freescale i.MX6 Development Platforms
  • More
  • Cancel
Freescale i.MX6 Development Platforms
Forum SGTL5000
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Freescale i.MX6 Development Platforms to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 6 subscribers
  • Views 642 views
  • Users 0 members are here
Related

SGTL5000

e14 Contributor
e14 Contributor over 13 years ago

HI,Can any one please tell me the I2C slave adress of SGTL5000XNAA3SGTL5000XNAA3 32QFN. As in data sheet "

"For the 32 QFN version of the SGTL5000XNAA3SGTL5000XNAA3, the I2C device

address is 0n01010(R/W) where n is determined by

I2C_ADR0_CS and R/W is the read/write bit from the I2C

protocol."

But I am not understading 'n'

Thanks

jumshed63@gmail.com

  • Sign in to reply
  • Cancel
  • phoenixcomm
    0 phoenixcomm over 13 years ago

    what do you mean by "n"?????????

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • gdstew
    0 gdstew over 13 years ago

    On the 32QFN package pin number 31 is labled I2C_ADR0_CS. The I2C address depends on what logic level this pin is

    connected to. If it is pulled high ( +3.3V) then the I2C address is 0101010 (n = 1), if the pin is low (0V or ground) then the I2C

    address is 0001010 (n = 0).

     

    You could just try both addresses to see which one it is set to.

     

    Hope this helps.