Freescale i.MX6 Development Platforms
  • Products & Partners
  • Dev Tools
  • Single-Board Computers
  • Freescale i.MX6 Development Platforms
  • More
  • Cancel
Freescale i.MX6 Development Platforms
Forum UART Serial connection
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Freescale i.MX6 Development Platforms to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 2 replies
  • Subscribers 6 subscribers
  • Views 1908 views
  • Users 0 members are here
Related

UART Serial connection

rctho
rctho over 7 years ago

Hello everyone. i'm hoping i can get some help with something i have been working off and on for a while. I have a SABRESD i.MX 6Dual/6Quad on a custom board from some OEM manufacturer. A few of them actually. I want to follow this tutorial to put linux on it. Looks pretty straight fwd. The problem i'm having is im unable to connect to the serial port to stop the U-Boot process if there is one at all. Currently there is Android on it so it's probably Fastboot. I'm guessing that the custom board does not allow a serial connection so it's not tampered with. I found what i think is a tx/rx on the board that connects to the chip for development.

image

 

 

Here is the pinout of the connection to the chip. the far left and right are vcc and ground while the two in the center connect to the chip.

image

 

and the headers i soldered onto it

image

 

Sorry for the noob questions. This is all very new to me and this is all i have managed to put together. If there is indeed Fastboot on it, is there a way i can flash U-boot without access to the serial connection that will later have a serial connection for me to connect to?

  • Sign in to reply
  • Cancel
Parents
  • Jan Cumps
    Jan Cumps over 7 years ago

    your pictures don’t show. Can you try to edit your post, make a small change and save it again?

    That usually fixes it.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Jan Cumps
    Jan Cumps over 7 years ago

    your pictures don’t show. Can you try to edit your post, make a small change and save it again?

    That usually fixes it.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • rctho
    rctho over 7 years ago in reply to Jan Cumps

    Updated pics.

     

    on NXP someone suggested using the mfg-tool. I tried that with no luck because of version issues. There are a lot to go through. i'm pretty sure the one i have is the mx6DLL and might be a lil' old. I prefer the buildroot method. I was able to successfully boot to linux through usb, but unfortunately without a display so without the serial connection, i don't really know what's going on. In this time i have come across two more of these boards. If i can fig out one, i can use them all.