Software
  • Products & Partners
  • Dev Tools
  • Software
  • More
  • Cancel
Software
Forum C++ callbacks and templates
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Software to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 17 replies
  • Subscribers 26 subscribers
  • Views 4442 views
  • Users 0 members are here
  • isr
  • interrupt
  • Modern C++
  • stl
  • OO
  • c++
  • callback
Related

C++ callbacks and templates

Jan Cumps
Jan Cumps over 2 years ago

I'm experimenting: can I use a method of a particular object as a callback? This can be used in typical callback situations, e.g.: in a UART driver. But also in interrupt handlers.

  • lightweight: small runtime cost, low firmware hit. Can be used for tiny embedded systems.
  • reusable: don't assume parameters and types for the handler, when writing this little framework -> C++ templates
  • hip -> object oriented, modern C++ constructs
  • type safe -> again C++ templates
  • allow a classic C function, a lambda, a static class method or an object method as handler

example: Raspberry Pico blinky using this design

#include <new>
#include <stdio.h>
#include "pico/stdlib.h"

import callbackmanager;

const uint32_t delay_ms = 250;

callbackmanager::Callback<void> cb;

int main() {
    gpio_init(PICO_DEFAULT_LED_PIN);
    gpio_set_dir(PICO_DEFAULT_LED_PIN, GPIO_OUT);
    cb.set([]() {
        static bool state = false;
        gpio_put(PICO_DEFAULT_LED_PIN, state = !state);
    });   

    while (true) {
        cb();
        sleep_ms(delay_ms);
    }
}

project: 2133.pico_callback_blink.zip

Callback template class

The template callback class. This is in essence the whole mechanism. A generic class that allows you to register and call event handler functions, lambda's and methods.

#include <functional>

// concept guards what types of return values we can handle
template<typename R>
concept Callbackable = 
	std::is_void<R>::value ||
	std::is_arithmetic_v<R> ||
	std::is_class_v<R>;
	
template <Callbackable R, typename... Args>
class Callback {
	using callbackfunction_t = std::function<R(Args...)>;	
public:
	Callback() : callback_(nullptr), isSet(false){}

	inline void set(callbackfunction_t callback) {
	    callback_ = callback;
		isSet = true;
	}

	inline void unset() {
		callback_ = nullptr;
		isSet = false;
	}

	inline bool is_set() {
		return isSet;		
	}

	/*
	 * R can be an arithmetic type, an object, or void
	 */
	inline R operator()(Args... args) {
		if constexpr (std::is_void<R>::value) {  // void
			if (!is_callback_set) {
				return;
			} else {
				(callback_)(args...);
			}
		} else if constexpr (std::is_class<R>::value) { // object
			if (!is_callback_set) {
				return R();
			} else {
				return (callback_)(args...);
			}
		} else { // not void nor object
			if (!is_callback_set) {
				return 0; // R can only be a arithmetic type. 0 should work as default.
			} else {
				return (callback_)(args...);
			}
		}

	}
	
private:
	callbackfunction_t callback_;
	bool isSet;
};

This generic class allows for handlers that pass any amount of parameters. No assumption of the types.

When we use the class in our code, we 'll tell it what the parameters are, and their type. For this blog, I am going to pass it 2 integers. The return value is also an integer.

Callback<int, int, int> cb;

In the declaration above, the first int is the return value type, the 2 others are parameter 1 and 2. Once you write this code, the object cb will only accept handler methods that take two integers as parameter, and return an integer.

Example of class that will handle the callback

This could be a gio class (blinky a led when an interrupt occurred?), a GUIwidget, or a business object. Typical guidelines apply: a handler should be swift. In particular if it's an interrupt handler.

class MyClass {
public:
      int handler(int num1, int num2) {
          return num1 + num2;
      }
};

The example does not do a lot today. It just sums up the two integers passed. But as a POC this will do.

Actual code using the two

#include <cstdio>

int main()
{
    MyClass myClass;

    Callback<int, int, int> cb;
    // Use a lambda to capture myClass and call the member method
    cb.set([&myClass](int num1, int num2) -> int {
        return myClass.handler(num1, num2);
    });

    int a = 4;
    int b = 5;

    int o = cb(a, b);
    printf("Value: %i\n", o); // We might be on an embedded system, use printf() and not std::cout
}

Why use a lambda to pair the handler and Callback ?

In the code, I did not learn the MyClass how to register itself. And the Callback doesn't know anything about who or what it 'll call. These classes (and their objects) are unaware of each other. Loose coupling.

Callback<int, int, int> cb;

cb.set([&myClass](int num1, int num2) -> int {
  return myClass.handler(num1, num2);
})
;

In the application logic, I tie the two together. The lambda function code (the anonymous function, starting with the [, and ending with the } above), is used as the vehicle to hold the code that the Callback object will execute when needed.

The lambda function could as well be a straigtforward piece of code, not related to any object:

Callback<int, int, int> cb;

cb.set([](int num1, int num2) -> int {
  return num1 + num2;
});

Or we could pass completely different executable code. As long as the lambda matches the signature given when instantiating the Callback class.

In an embedded system,

  • myClass would be one of your application objects.
  • cb could be part of a driver, or the HAL layer
  • cb.set() would be called by you, to register the handler
  • cb.call() would be done by the driver, or HAL ISR, when it wants to notify you (call your callback handler)

In the case of this example, it will execute myClass.handler(). If you 'd have many MyClass objects, it would call the exact one that's registered in with set().

image
Example use of the callback class in an embedded application

Anything special?

This approach allows to write a reusable callback system. It is type safe. But it does not assume what the type is of the object it 'll call the handler off. (Or if it's actually an object).
It's a small amount of code, that performs a function that you regularly need in an embedded or event driven design.

What does type-safe mean in this context?

If your interrupt handler assumes a function that passes 2 integers, and you pass it a callback function that has different parameters,
you get a compile time error. Your code will not build, because the handler is not compatible.

And you get all of that, without having to specify the number of variables, and their types, in the Callback class code. We get a reusable class. Type safe. Without the need to foresee all possible combinations.

this library now also works for Arduino (tested with IDE2, and an Arduino MKT GSM 1400)

For Arduino, you can download callbackmanager.h to your computer, then use Sketch -> Add File ... to get the callbackmanager included to your project.
Add this line to your sketch:

#include "callbackmanager.h"

I added a sketch to test the callback manager to this gist: test_arduino.ino

image
Arduinos that use the gcc-avg toolchain are not supported (UNO, Mega, the original basic Nano)

shortcuts:

  • I assume fixed return value type. A richer implementation can use template for that too, and should allow void. edit: this works
  • I pass arguments by value. A better design would also allow pass by reference. And to pass const references. edit: this works
  • should I use a shared pointer, so that I can never call the handler of an object that no longer exists? (solved by alternative: provide an unset() method). edit: the class no longer uses pointers
  • it only allows to call one handler. Good for ISR use. But in an event driven design, you may want to register more handlers. I prefer just one handler. simple scope, simple responsibility.

Inspiration:

  • I started from this example by Geoffrey Hunter.
  • mbed's Callback class, although I didn't use any of the code
  • cplusplus' tutorial for std::function, to validate if it works for static class member, object member, classic C function and lambda function.

Code is available on github. Additional assets available on Gist.

CMakeLists.txt to build an example program:

cmake_minimum_required(VERSION 3.28)

project(callbackmanager C CXX ASM)

# GoogleTest requires at least C++14
set(CMAKE_CXX_STANDARD 26)
set(CMAKE_CXX_STANDARD_REQUIRED ON)
set(CMAKE_CXX_FLAGS "${CMAKE_CXX_FLAGS} -fmodules-ts -fcommon")

add_executable(${CMAKE_PROJECT_NAME})
target_sources(${CMAKE_PROJECT_NAME}
        PUBLIC
        ${CMAKE_CURRENT_SOURCE_DIR}/example/callback_examples.cpp
)
target_sources(${CMAKE_PROJECT_NAME}
        PUBLIC
        FILE_SET cxx_modules TYPE CXX_MODULES FILES
        ${CMAKE_CURRENT_SOURCE_DIR}/callbackmanager.cpp
)

target_link_libraries( ${CMAKE_PROJECT_NAME}
)

I test this code in  C++ callbacks and templates: make the Callback class call an object member, a static member, a C function and a pure lambda function 
edit 20250208: I converted it to a c++ module: modern C++ modules: convert existing example from .h to module 

  • Sign in to reply
  • Cancel

Top Replies

  • Jan Cumps
    Jan Cumps over 2 years ago +2
    The code is now available on Gist . I've put the template class in a header file. Also: tested on a Pico: I also attached a Pico SDK subproject archive, plug-and-play callback
  • shabaz
    shabaz over 2 years ago +1
    Hi Jan, Very interesting! By coincidence I too was looking for a way of doing callbacks, mine is nowhere near as clean though. I went with virtual functions, i.e.: class Bob_base { public: .. virtual…
  • Jan Cumps
    Jan Cumps over 2 years ago in reply to shabaz +1
    added advantage: you don't need inheritance. And nearly everything is resolved at compile time. Because this approach allows that you can call back methods of any class (or even functions that don't…
Parents
  • flyingbean
    flyingbean over 2 years ago

    Great tip. I could use the template  in my projects here.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 2 years ago in reply to flyingbean

    I've been testing it with toolchains. 

    Works with:

    • NXP MCUXpresso
    • Pico C/C++ SDK 1.5
    • Renesas e2 studio with gcc toolchain (everything, except the optional clause requires std::is_arithmetic<R>::value)
    • Eclipse with the arm linux cross-compiler (for Raspberry Pi, BB, ...)

    Does not work with:

    • Arduino IDE 2.0 avr-gcc: compiler version 7.3 is too low
    • Arduino IDE 2.0 arm-gcc: compiler version 7.2 is too low
    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Jan Cumps
    Jan Cumps over 2 years ago in reply to flyingbean

    I've been testing it with toolchains. 

    Works with:

    • NXP MCUXpresso
    • Pico C/C++ SDK 1.5
    • Renesas e2 studio with gcc toolchain (everything, except the optional clause requires std::is_arithmetic<R>::value)
    • Eclipse with the arm linux cross-compiler (for Raspberry Pi, BB, ...)

    Does not work with:

    • Arduino IDE 2.0 avr-gcc: compiler version 7.3 is too low
    • Arduino IDE 2.0 arm-gcc: compiler version 7.2 is too low
    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Children
  • flyingbean
    flyingbean over 2 years ago in reply to Jan Cumps

    I just got a new board from Renesas. Will try e2 studio after my vacation this Summer.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 2 years ago in reply to flyingbean

    comment out this requires line in the template definition.

    requires std::is_void<R>::value || std::is_arithmetic_v<R>

    It's code that doesn't execute anything but helps the developer to use supported attributes.
    The current GNU toolchain for Renesas is 1 version too low for this. 

    If you don't have this line, and use a non-supported return type for the callback, you 'll get a compile error anyway.
    But it 'll be a more cryptic one, at the first line where the code tries to do an operation that your type doesn't support.
    In my template, that will be at the return 0; line. That's the only line that doesn't work for any type of return value.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 2 years ago in reply to flyingbean

    latest version on github gist allows compilation with lower version GCC (including the Renesas and Arduino toolchains).

    There is no difference at runtime. You 'll only get a little more cryptic error if you use unsupported template types:
    an error when the compiler detects that the code can't handle your type, instead of an error right at the declaration where you define what parameter types you want to use.