Technical Library
  • Products & Partners
  • Dev Tools
  • Technical Library
  • More
  • Cancel
Technical Library
Files BBONE-GATEWAY-CAPE_README_11292016_v0 1.pdf
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Technical Library to participate - click to join for free!
Actions
  • Next
  • Previous
  • Share
  • More
  • Cancel
Related
Recommended

BBONE-GATEWAY-CAPE_README_11292016_v0 1.pdf

An important README on firmware compatibility, configuration and use of the Wireless Connectivity Cape for BeagleBone Black.

  • wireless connectivity cape
  • Reference Manual
  • BeagleBone Black
jcasiello
jcasiello
  • 29 Nov 2016
  • 16 Downloads
  • Share
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • chicagobob
    chicagobob over 7 years ago +3
    And I have the Element14 WIFI cape working with the latest Debian. It took a lot of poking around. But God smiled upon the struggle and I found BB-GATEWAY-WL1837-00A0.dtbo in the /lib/firmware directory…
  • bbbuser777
    bbbuser777 over 8 years ago +2
    Has anyone gotten this thing to work on a BBB Rev C? I suggest, that they update their documentation and/or show verifiable examples of getting this device to work or stop selling it. I will return this…
  • jack.dempsy47
    jack.dempsy47 over 9 years ago +1
    From other posts I've found that this wireless cape uses same pins as emmc, so you HAVE to boot from SD card.. the fun part is, in order to do this, you have to push a button inbetween the cape and BB…
  • phillipb0576
    phillipb0576 over 9 years ago

    A related question to the one I posted above- The instructions reference flashing a SD card with the image required to run the cape. Flashing the card will delete the image currently on the card which is the Debian version that is running the Beaglebone. The cape uses the same pins as the EMMC and so the board won't be able to boot properly if there is no image on the card. I would like to understand functionally how this works.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • phillipb0576
    phillipb0576 over 9 years ago in reply to cstiegman123

    I am having the same issue. I followed the instructions in the read me with no success. I am attempting to get the cape to function with a beaglebone black. I cant seem to find anyone who's completed this task successfully.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • cstiegman123
    cstiegman123 over 9 years ago

    ctday

    jack.dempsy47

     

    Jack, did you ever receive an answer or help with the issues you described in your last post?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jack.dempsy47
    jack.dempsy47 over 9 years ago

    From other posts I've found that this wireless cape uses same pins as emmc, so you HAVE to boot from SD card.. the fun part is, in order to do this, you have to push a button inbetween the cape and BB.

     

    Having followed the instructions, the OS still doesn't recognize the device. I'm seeing these messages from the capemgr:

    [    0.000000] Kernel command line: console=tty0 console=ttyO0,115200n8 bone_capemgr.enable_partno=BB-BONE-WL183 root=/dev/mmcblk0p1 rootfstype=ext4 rootwait coherent_pool=1M quiet net.ifnames=0 cape_universal=enable

    [    2.298679] bone_capemgr bone_capemgr: Baseboard: 'A335BNLT,00C0,2916BBBK1563'

    [    2.298712] bone_capemgr bone_capemgr: compatible-baseboard=ti,beaglebone-black - #slots=4

    [    2.337769] bone_capemgr bone_capemgr: slot #0: No cape found

    [    2.381769] bone_capemgr bone_capemgr: slot #1: No cape found

    [    2.425762] bone_capemgr bone_capemgr: slot #2: No cape found

    [    2.469762] bone_capemgr bone_capemgr: slot #3: No cape found

    [    2.475594] bone_capemgr bone_capemgr: enabled_partno PARTNO 'BB-BONE-WL183' VER 'N/A' PR '0'

    [    2.475607] bone_capemgr bone_capemgr: slot #4: override

    [    2.475622] bone_capemgr bone_capemgr: Using override eeprom data at slot 4

    [    2.475636] bone_capemgr bone_capemgr: slot #4: 'Override Board Name,00A0,Override Manuf,BB-BONE-WL183'

    [    2.475989] bone_capemgr bone_capemgr: initialized OK.

    [    3.486144] bone_capemgr bone_capemgr: loader: failed to load slot-4 BB-BONE-WL183:00A0 (prio 0)

     

    I see there's another dtb in the latest debian image named: am335x-boneblack-wl1835mod.dtb
    Should we be using that or the: am335x-boneblack-overlay.dtb   ?

     

    Also: Where can I find the documentation on the jumper pin-outs?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • cstiegman123
    cstiegman123 over 9 years ago in reply to ctday

    The instructions were intended to be used with a firmware image running off the inserted SD card.  It was not verified on the eMMC.  In fact I believe the inserted Cape may not function properly if running off of the eMMC.

     

    So, can you please try running the image from an SD card and report back the functionality?

     

    Thank you.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>