Technical Library
  • Products & Partners
  • Dev Tools
  • Technical Library
  • More
  • Cancel
Technical Library
Documents element14: Software examples and demos for the LPC4357-EVB
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Technical Library to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: vandana
  • Date Created: 15 Jan 2013 9:42 PM Date Created
  • Last Updated Last Updated: 8 Oct 2021 7:00 AM
  • Views 4290 views
  • Likes 0 likes
  • Comments 21 comments
Related
Recommended

element14: Software examples and demos for the LPC4357-EVB

This document lists the available software examples and demos for the LPC4357-EVB; Details on the examples and testing are provided in the User Manual.

 

Simply click on the links to download the code!

 

Examples 1 - Core & Drivers - (required for all examples)

Examples 2 - GPIO, SDRAM, I2C - Accelerometer, USB, LCD, Touch Screen

Examples 3 - I2S

Examples 4 - Dual-Core

Examples 5 - SD Card

 

Demo 1 - emWin Graphics

Demo 2 - Micrium uC/OS-III

  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • e14 Contributor
    e14 Contributor over 13 years ago +1
    Following the instructions on the enclosed 'Quick start guide' does not result in the driver for the VCOM installing. If this product is not compatible with Windows 8 or 64-bit Windows 7 then put that…
  • e14 Contributor
    e14 Contributor over 13 years ago

    Has anyone managed to successfully program the LPC4357-EVB board using the Keil ULINK2 with Keil MDK-ARM?

    I worked through the manual for this board following the example for the supplied Gpio_LEDBlinky in Examples 2 and continually get SWD Communication Failure whenever I try to Download, Debug or even just Erase the flash.

    This is despite the Settings screen in the uVision IDE showing that the ULINK2 debugger is detecting the Coresight debug unit on the target.

     

    I have verified my ULINK2 works on a board with a different ARM so can only think it is some configuration setting problem in this project or I have a dodgy board.

     

    Can anyone help?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
<