Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Chat (English) misaligned grid and test points
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 13 replies
  • Subscribers 188 subscribers
  • Views 1908 views
  • Users 0 members are here
Related

misaligned grid and test points

e14 Contributor
e14 Contributor over 15 years ago

I created a schematic with just a single Analog Devices ADIS16209 now I

need test points. I will be using Keystone miniature color coded thru-hole

type. .100 Dia.

http://www.keyelco.com/pdfs/M55p51.pdf

What is the equivalent in Eagle? I tried some of the built in test pads but

they don't show dimensions. I tried keeping a standard default 0.1 inch

grid. When I create the schematic everything aligns but when I create the

board they don't align with the grid why? This is my my very first board.

--

Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

 

  • Sign in to reply
  • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to e14 Contributor

    Thank you. I just wasn't right clicking on the origin cross. I was clicking

    on the border of the chip instead and only getting a "move" menu or another

    area and getting a ghosted out move menu.

     

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to e14 Contributor

     

    "Jay Beritz" wrote

    Adding the chip "ADIS16209" .................... Eagle won't let me smash

    the part to move it so

    I guess I'll have to copy and create my own version.

    You didn't say, do you know how close to the edge of the board I can have

    silkscreen or parts when using the Pentalogix board service.

     

    Hi Jay

     

    A few things

     

    1. The "ADIS16209" from the library  (v5.11)  does smash and I can move the

    name,  IC1 in your case. To be able to SMASH you must have the layer

    tOrigins turned on. i.e. the origin cross for the part is showing.

     

    2. ........do you know how close to the edge of the board I can have

    silkscreen or parts when using the Pentalogix board service.......Always ask

    your board service these questions. They will often have it available on

    their site, along with a whole heap of other stuff you have to know.  If not

    email them. No one else has the definitive answer.

     

    3.Tutorials. Watching video tutorials is a double edged sword. It's easy and

    they reveal features and techniques quickly but alas we don't learn well

    from them.   There are other tutorials that are "read and do" which will

    teach you better. Try the one that comes with Eagle in the Docs folder. Read

    the manual also in that folder. Then do others you find on the net like

    those at Sparkfun.com. Don't just read them, replicate what they are doing.

    As they say, you could  read a book on programming  but when you get to the

    end you won't be able to program.

     

    All the best

    Warren

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to e14 Contributor

    As I said in my first post this will be my first board. I have watched all

    of the tutorial video at:

    http://tangentsoft.net/elec/movies/

    and tried many things on my own. I didn't realize that my posts were random

    at all. They are all problems I am encountering with this circuit board. I

    don't see any reason to create another post hope someone answers them and

    take a long time to finish the board. I do appreciate your help. Eagle has

    a pretty step learning curve.

    Hiding the tNames and bNames only hides the "IC1" while I'm routing.

    According to the TangentSoft tutorial "TT #9"  When running the cam

    processor for gerber247x.cam on the tab marked "Silkscreen CMP" the tNames

    layer is highlighted by default. This shows up in the gerbers so if I

    didn't move the "IC1" it would be over the route in the gerber. I tried it

    and when viewing the .plc layer the "IC1" is on top of the route.

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to e14 Contributor

    On 1/10/2011 5:29 PM, Jay Beritz wrote:

    Adding the chip "ADIS16209" from the control panel or for the "add" button

    doesn't make a difference the silkscreen "IC1" still shows up and is in the

    way when I do the routing. Eagle won't let me smash the part to move it so

    I guess I'll have to copy and create my own version.

    You didn't say, do you know how close to the edge of the board I can have

    silkscreen or parts when using the Pentalogix board service.

    Just hide the tNames or bNames layer to not see the part names when you

    are routing. I have never heard of being unable to smash a part, perhaps

    you are doing it wrong? What is visible in the board editor is also not

    related to the silkscreen, that happens when you make gerber files and

    include drawing layers to your silkscreen file.

     

    From the randomness of your posts, it sounds like you don't know what

    you are doing. I would suggest that you do the eagle tutorial to

    familiarize yourself with the program before asking any more questions -

      you don't know enough about the program to be able to even explain

    things to you.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to e14 Contributor

    Adding the chip "ADIS16209" from the control panel or for the "add" button

    doesn't make a difference the silkscreen "IC1" still shows up and is in the

    way when I do the routing. Eagle won't let me smash the part to move it so

    I guess I'll have to copy and create my own version.

    You didn't say, do you know how close to the edge of the board I can have

    silkscreen or parts when using the Pentalogix board service.

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to e14 Contributor

    On 1/8/2011 5:16 PM, Jay Beritz wrote:

     

    I create a new schematic

    I select add

    I de-select Smd's in the search parameter and search for test pad

    I expand the search result "testpad"

    Under "TP" I select the fifth choice "TPPAD1-17"

     

    The three boxes to the right in the "add" dialog don't show me any drill

    sizes. If I go ahead and add it then right click and go to properties, I

    still see nothing that tells me the hole size.

    Where is this information?

     

    I add the test pads and wire them to the chip.

    File -> Switch to Board, "And let Eagle create the board from the

    schematic."

    I change the grid size to 0.01 inch

    I move the chip and pads into position.

    I route the chip's pads to the test pads.

     

    But no matter what I set the grid to, the center of the chip pads and the

    center of the test pads will not align to the grid. When I do a Errors

    check it it's says: Errors(0), Approved(0)

    Shouldn't it say Approved(1) or more?

    Also when I'm I have the board open I'm looking at the chip from the top

    down correct?

     

    >

    sorry my mistake, the through hole test pads are in solpad.lbr not

    testpad.lbr. The only reason I can think of that a single pad will not

    center on a grid point is that there is an error in the part, ie the

    origin of the part in the library is not in the pad center.

     

    The board grid does need to be a multiple of the chip pitch in order for

    the pad centers to be on grid points, but this is not required to route

    the board ( although it will look nicer if you do it ). Sometimes you

    have parts on the board which can not be routed on the same grid, then

    you need to switch grids when routing if you want it to look neat. But I

    don't recall that pad centers have to be on grid points.

     

    In eagle, when manually routing it is usually better to start /from the

    pads/. If you can't reach the other pad from because of a grid clash,

    then just stop in the middle; go to the other pad and route from there

    to the middle ( on grid) point. Neither end is required to be on the

    grid. The grid just sets how often you have an opportunity to turn a corner.

     

    I don't like to pick parts from the ADD dialog for the reasons you

    mentioned, I usually look through the libs in the control panel where I

    can see all the packages and ADD it from there, especially if I don't

    know what it is called. Remember eagle is translated to English and if

    you're american you have the added confusion of european terminology for

    the same component. it's hard to know what it is called elsewhere...so

    how do you know what to search for unless it's a part number? So, mostly

    I use the control panel.

     

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to e14 Contributor

    Well I couldn't find a test pad with the drill size I need but there's a

    Keystone library with the part I needed on the Cadsoft site so that saves

    me some trouble.

    ftp://ftp.cadsoft.de/eagle/userfiles/libraries/keystone.lbr

    Now for the board I'm having trouble with the "IC1" being in the way of the

    trace. Is there any way to move it without copying the whole part and

    creating a new version? Because I didn't create it I don't get the option

    to smash and reposition it.

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to e14 Contributor

    On 1/9/2011 3:04 PM, Jay Beritz wrote:

    Page 7 of the data sheet shows a pin pitch of 0.670 mm

    http://www.analog.com/static/imported-files/data_sheets/ADIS16209.pdf

     

    >

    Create schematic with default grid size of 0.1 inch "everything aligns"

    File -> Switch to Board "Let Eagle create the board from the schematic"

    Set grid size to twice as small as the pin pitch ( 0.670 / 2 = 0.335mm)

    Still nothing aligns to the grid. Also you didn't say, where is the drill

    size information for the test pads?

     

    If you use the library editor to open testpad.lbr you will find that

    most of the devices are Pads and are composed of an SMD so there is no

    associated hole.     There are a few devices which do have through-holes

    (eg P2-38-17.pac).   If you use library editor to open the package and

    use the info tool to select the hole you will see a display which gives

    the hole diamter (0.067 for the above referenced package).  For the

    TPPAD1-17 the P1-17 package is used and this part also is indicated as

    an 0.067 hole.

     

    I do not know why your cannot place your component so the pins are on

    grid.   Perhaps the origin of the package is not placed correctly

    relative to the pin locations so that when the origin is snapped to the

    grid the pin positions are still off?

     

    jiml

     

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to e14 Contributor

    Page 7 of the data sheet shows a pin pitch of 0.670 mm

    http://www.analog.com/static/imported-files/data_sheets/ADIS16209.pdf

     

     

    Create schematic with default grid size of 0.1 inch "everything aligns"

    File -> Switch to Board "Let Eagle create the board from the schematic"

    Set grid size to twice as small as the pin pitch ( 0.670 / 2 = 0.335mm)

    Still nothing aligns to the grid. Also you didn't say, where is the drill

    size information for the test pads?

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to e14 Contributor

    On 1/8/2011 8:16 PM, Jay Beritz wrote:

     

    I create a new schematic

    I select add

    I de-select Smd's in the search parameter and search for test pad

    I expand the search result "testpad"

    Under "TP" I select the fifth choice "TPPAD1-17"

     

    The three boxes to the right in the "add" dialog don't show me any drill

    sizes. If I go ahead and add it then right click and go to properties, I

    still see nothing that tells me the hole size.

    Where is this information?

     

    I add the test pads and wire them to the chip.

    File -> Switch to Board, "And let Eagle create the board from the

    schematic."

    I change the grid size to 0.01 inch

    I move the chip and pads into position.

    I route the chip's pads to the test pads.

     

    But no matter what I set the grid to, the center of the chip pads and the

    center of the test pads will not align to the grid. When I do a Errors

    check it it's says: Errors(0), Approved(0)

    Shouldn't it say Approved(1) or more?

    Also when I'm I have the board open I'm looking at the chip from the top

    down correct?

     

    >

     

    You are correct that the board view is showing you a view from layer 1

    down through to layer 16 (or whatever your bottom layer is).   The chip

    view will depend on whether you placed the part on the top or bottom of

    the board.   If its on the bottom then all the text (name,value) for the

    component will be mirrored.

     

    I think you need to make sure that your component pin pitch is an

    integer multiple of the board grid.   This should allow you to place the

    component on grid.

     

    The number and type of errors/warnings that you get from DRC will depend

    on the settings you used when you ran DRC.

     

    jiml

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
>