Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Chat (English) >$1000 for a simple 8"x8" PCB???
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 12 replies
  • Subscribers 192 subscribers
  • Views 1904 views
  • Users 0 members are here
  • eagle
  • pcb
Related

>$1000 for a simple 8"x8" PCB???

e14 Contributor
e14 Contributor over 12 years ago

I want to make a simple PCB, so I'm looking at Eagle as it seems to be what other hobbiests use.

The board is 8" x 8", and will have only a few LEDs and chip resistors on it. I don't need multiple layers, libraries, autorouting, or even drilled holes. I could make the PCB by hand with a utility knife, but I thought using a PCB program would be neater and cause less hand stress. BUT it seems the Eagle program is more than $1000 to do this! Do other hobbiests really spend this? (I was hoping for free...)

My question: Is there another program out there cheaper, Eagle just seems unreasonably priced.

  • Sign in to reply
  • Cancel
  • mcb1
    0 mcb1 over 12 years ago

    Steve

    You're correct that for a simple project the price is high.

     

    For your application there are several others available and PCB manufacturers accept output from these as well.

     

    Obviously Cad Soft Guest is a little biased but it doesn't translate in rudeness.

    Because it is a single board with a few parts on doesn't mean its trivial to the poster.

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 12 years ago

    On 05/05/14 22:27, Steve Ins wrote:

    I want to make a simple PCB, so I'm looking at Eagle as it seems to be

    what other hobbiests use.

    The board is 8" x 8", and will have only a few LEDs and chip resistors

    on it. I don't need multiple layers, libraries, autorouting, or even

    drilled holes. I could make the PCB by hand with a utility knife, but I

    thought using a PCB program would be neater and cause less hand stress.

    BUT it seems the Eagle program is more than $1000 to do this! Do other

    hobbiests really spend this? (I was hoping for free...)

    My question: Is there another program out there cheaper, Eagle just

    seems unreasonably priced.

     

     

    Eagle is free if you want to design simple and small. If you want to

    design something really complex that justifies 8"x8" then the $1000

    price tag is actually quite reasonable. If you're merely hell-bent on

    wasting PCB space...

     

    Yes there are cheaper programs. There are free ones, both as in beer and

    as in speech. Some of them are even tolerably usable apparently.

     

    Of course, if you had the cunning to work around things instead of

    whingeing about the price of something that's worth every penny, then

    there are ways to achieve what you need for your trivial case without

    needing any expensive options, but since this is an Eagle discussion

    group hosted by CadSoft / Element14 then I'm most certainly not going to

    give you any clues there.

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
<