EAGLE User Support (English) How to add 0R 1206 Resistor as Jumper t o Board Layout
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
  • Replies 15 replies
  • Subscribers 180 subscribers
  • Views 2685 views
  • Users 0 members are here
Related

How to add 0R 1206 Resistor as Jumper t o Board Layout

Former Member
Former Member over 15 years ago

Hi;

Most of the Cad editors allow to add a 0R Resistor to board as a jumper.

But I can't find how to do it without adding to schematic.

 

Thanks in advance..

--

Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

 

  • Sign in to reply
  • Cancel
  • Former Member
    Former Member over 15 years ago in reply to Former Member

    On 7/3/2010 12:44 PM, uMinded wrote:

     

    I have seen 0R SMT jumpers used on a few prototypes and they where used

    for this reason:

    The company has in house board manufacturing but only for 2-4layers and

    during development the board was too complex for a 4layer routing and

    they used SMT jumpers that looked like resistors but where just wire

    bridges in a standard SMT package. They where not on the schematic as

    the guy who routed the board just added them to get those last few

    airwires routed. This worked but if I saw a commercial product with that

    I would stay away as they where obviously cutting corners or cheap.

    >

    They are "obviously" cutting corners? I thought 2 layer boards are much

    more reliable than 4 layer boards. What is wrong with wanting to save

    their customers' money, is that being "cheap"? Once again, no logical

    objective reason that I can see...

     

    If an SMT resistor is reliable, why would an SMT jumper be less

    reliable? If you could somehow tell that there were a few extra

    resistors on a board, would you declare it to be cheap or cutting corners?

     

    I suspect the real reason this is not done more often is simply that CAD

    tools don't handle it gracefully. But if someone does have an answer to

    why it is a bad idea, I'd like to hear it...

     

    The second reason to use 0R jumpers is the acceptable reason. If you

    What makes them "acceptable" in this context but not in a jumper layer

    context?

     

    By the way, the disk drive in question was from the top rated

    manufacturer and was produced in the early 2000's. In my experience,

    volume commodity manufacturers favor double or single (yes!) layer

    boards wherever possible.

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 15 years ago in reply to Former Member

    On 2010-06-12 00:22:30 +0200, Gary Gofstein <nospam@use.forum.net> said:

     

    If it sounds like I'm preaching, I'm not; but I have asked this

    question many times and I have never gotten a satisfactory answer. Is

    there something wrong with using a jumper layer that I don't know

    about? Or is it just that it is too time consuming or impossible to

    make one on most EDA tools?

     

    There are several ways to handle jumpers, I use two of them. I etch the

    first edition of most boards myself.

     

     

    1) I route long jumpers on the top layer and use bare wires. Make the

    tracks going to the via as fat as possible, preferably the same

    diameter as the via, so the eyelet will stay on the board when you

    drill.

     

    2) short jumpers are done with 0R reistors, 1206 foorprint. Yes, these

    need to be in the BOM, so also in the schematic. See attach. Yes, I

    ignore the airwaire on the board.  These 1206 jumpers are used mostly

    for connecting GND planes, i.e. different parts of the same polygon.

     

    Soldering an 1206 0R resistor is a lot less work than drilling two

    holes and wiggling a wire through them. For boardhouse made boards, 2

    layers is enough for me.

     

    Yes, it would be nice if Eagle could see the jumper as part of the net,

    but this would involve different treatments of components that are part

    of the net and components that are not. A different layer would not

    solve that.

     

     

    --

    Eur van Andel  eur@fiwihex.nl

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 15 years ago in reply to Former Member

    Eur van Andel wrote on Mon, 12 July 2010 08:10

    short jumpers are done with 0R reistors, 1206 foorprint. Yes, these

    need to be in the BOM, so also in the schematic.

     

    SMD resistors used in this role should not be on the schematic, since they

    are a artifact of routing, and do not relate to the circuit itself.

     

    Currently there is no way to do this in Eagle, but that would be a nice

    idea.

     

    Quote:

    Yes, it would be nice if Eagle could see the jumper as part of the net,

     

    but this would involve different treatments of components that are part

     

    of the net and components that are not.

     

    I think if this were added it would have to be in the ROUTE command where

    it understands special packages you define as jumpers.  You should be able

    to place them anywhere in a route, just like vias.  There would need to be

    a list of allowable jumpers per net class so that the auto router knows

    what it can do.  Each type of jumper would also need its own cost in the

    auto router.

     

    Note that these jumpers must not show up in the schematic.  You must be

    free to add them or rip them up without having to edit the schematic.  They

    do need to be in the board data so that BOM tools can find them.

     

    While all this is nice, it sounds like it would be considerable effort to

    add to Eagle.  If I got to pick I'd rather CadSoft work on more flexible

    package definition so that you can suppress some DRC errors from deliberate

    overlaps within a package, and allow for multiple symbols per device (gate)

    with possibly different numbers of pins.

     

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 15 years ago in reply to Former Member

    On 7/12/2010 5:10 AM, Eur van Andel wrote:

    On 2010-06-12 00:22:30 +0200, Gary Gofstein <nospam@use.forum.net> said:

    >

    >> If it sounds like I'm preaching, I'm not; but I have asked this

    >> question many times and I have never gotten a satisfactory answer. Is

    >> there something wrong with using a jumper layer that I don't know

    >> about? Or is it just that it is too time consuming or impossible to

    >> make one on most EDA tools?

    >

    There are several ways to handle jumpers, I use two of them. I etch the

    first edition of most boards myself.

    >

    >

    1) I route long jumpers on the top layer and use bare wires. Make the

    tracks going to the via as fat as possible, preferably the same diameter

    as the via, so the eyelet will stay on the board when you drill.

    >

    2) short jumpers are done with 0R reistors, 1206 foorprint. Yes, these

    need to be in the BOM, so also in the schematic. See attach. Yes, I

    ignore the airwaire on the board. These 1206 jumpers are used mostly for

    connecting GND planes, i.e. different parts of the same polygon.

    >

    Soldering an 1206 0R resistor is a lot less work than drilling two holes

    and wiggling a wire through them. For boardhouse made boards, 2 layers

    is enough for me.

    >

    Yes, it would be nice if Eagle could see the jumper as part of the net,

    but this would involve different treatments of components that are part

    of the net and components that are not. A different layer would not

    solve that.

    >

    >

    I have heard that some CAD packages have a designated jumper layer that

    they can route on. The rules for this layer are derived from the type of

    jumper that are allowed to be generated ( fixed length wire, 0R thru

    hole resistor, 0R SMD resistors ). This allows the CAD software to keep

    track of the net connections ( through the special layer) and keep these

    jumpers off the schematic. It is not just another copper layer, EAGLE

    already has plenty of those. The special layer is not ever output, just

    used to contain the routes that belong to the jumper components.

     

    There are a lot of ways to make the software handle a "jumper layer"

    functionality...I was just pointing this out as an example.

     

    The reason for bringing up the topic in this thread is not related to

    how work around the problem in EAGLE, but rather to a poster's assertion

    that the jumpers /must/ appear in the schematic. I believe the original

    poster was talking about "jumper layer" jumpers rather than "option

    selecting" jumpers and that these kind of jumpers are not needed or

    desired in the schematic, only the BOM.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 15 years ago in reply to Former Member

    On 7/12/2010 6:15 AM, Olin Lathrop wrote:

    Eur van Andel wrote on Mon, 12 July 2010 08:10

    >> short jumpers are done with 0R reistors, 1206 foorprint. Yes, these

    >> need to be in the BOM, so also in the schematic.

    >

    SMD resistors used in this role should not be on the schematic, since they

    are a artifact of routing, and do not relate to the circuit itself.

    >

    Currently there is no way to do this in Eagle, but that would be a nice

    idea.

    >

    Quote:

    >> Yes, it would be nice if Eagle could see the jumper as part of the net,

    >>

    >> but this would involve different treatments of components that are part

    >>

    >> of the net and components that are not.

    >

    I think if this were added it would have to be in the ROUTE command where

    it understands special packages you define as jumpers. You should be able

    to place them anywhere in a route, just like vias. There would need to be

    a list of allowable jumpers per net class so that the auto router knows

    what it can do. Each type of jumper would also need its own cost in the

    auto router.

    >

    Note that these jumpers must not show up in the schematic. You must be

    free to add them or rip them up without having to edit the schematic. They

    do need to be in the board data so that BOM tools can find them.

    >

    While all this is nice, it sounds like it would be considerable effort to

    add to Eagle. If I got to pick I'd rather CadSoft work on more flexible

    package definition so that you can suppress some DRC errors from deliberate

    overlaps within a package, and allow for multiple symbols per device (gate)

    with possibly different numbers of pins.

    >

    This is also an excellent way to do it. The advantage of the dedicated

    layer approach is that it only requires relaxation of some of EAGLE's

    rules to implement the functionality, rather than new functionality.

     

    In this way it is analogous to the examples you've given where EAGLE's

    insistence on 1:1 correspondance and enforcing rules that are meant to

    keep newbies out of trouble are becoming a problem. A warning is more

    appropriate than a prohibition in these cases...

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
<