EAGLE User Support (English) Whats happening with EagleCad & Cadsoft?
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
  • Replies 46 replies
  • Subscribers 183 subscribers
  • Views 4090 views
  • Users 0 members are here
Related

Whats happening with EagleCad & Cadsoft?

Former Member
Former Member over 14 years ago

HI,

 

There have been plenty of user suggestions (including myself ) over the

years and many relating to the same old issues.

 

As a PAYING User, I have essentially invested my money ( but a lot of my

time) into using & Learning EagleCad.

 

So..

 

I would like to know ( from the horses mouth if possible) what is Cadsoft

Proposing/Planning for the next release(s) of Eagle Cad?

Is there an advantage to anyone ( especially users) if future features are

kept secret?

 

The following is what I can see as major changes in no particular order and

not inclusive..

 

Q1) Are there going to be any major changes to the LIBRARY?

 

Q2) Are we going to have a proper user definable /properly integrated BOM

window ?

 

Q3) Can CUT, COPY & PASTE ( and selection/group) work just like any other

application?

 

Q4) Can we open more than one PROJECT or LIBRARY part at the same time?

Will we be able to copy and paste ( Drag and drop) between these?

 

Q5) Can all the user settings and scr files ( or whatever setting files) be

kept in just ONE FILE , in one place and All accessible in ONE User

Preference (TABBED) window? (we can get rid of the Control panel if we do

this, and it means that updating Eaglecad will be less painful).

 

Q6) Are their any plans for some sort of SChematic/Layout hierarchy or

SUB-Circuits feature.

 

Q7) Any plans for a built in Gerber Viewer ( mac users have almost nothing

to work with here?)

 

Q8) Any plans for built in Circuit Simulation ( even basic stuff)?

 

Q9) Any plans for The Built in text editor to have its own Syntax

Highlighting etc?

 

Q10) Any plans for a built in Gerber Panalizer/Merger Tool?

 

Q11) Are there any plans for more control over pads/holes in the device

editor? i.e Odd/Complex shapes.

 

Q12) Can the design link feature work with other suppliers. ( should be

part of the BOM System anyhow)

 

Q13) Can we place less reliance on ULP's and command line entries as a

source of features/enhancements or usability, this should really be only

for specialised tasks. If you have a look at the ULP's over the years

theres a ton of them for Library Management and BOM'S  Is that telling you

something?

 

Q14) Can we have single keystroke functions for at lease basic items, Move,

Change Layer, etc ( user definable of course).

 

I just want to know whats happening, The Beta Test forum is VERY QUIET, The

last release only really had Farnell Shopping added/improved and a few bug

fix's, I am worried that development has either slowed down or stopped. OR

is their  something big in the pipeline. ( hoping!)

 

I am also worried that most suggestions are "Frowned" upon and this really

puts new users off !

 

So that I , ( and everyone else ) can stop wasting our time ( and your

time) with suggestions, can you please answer or give us something to look

forward to?

 

One reason I am asking all the above is that I am considering spending a

LOT OF TIME learning the scripting language so that I can program my own

features ( I have lots of big ideas) , Why, Because I don't know what is

the future for Eaglecad, And I am concerned that I may get to the stage of

writing very useful ULP's and then Cadsoft will release something in the

near future that replaces my work. Remember that all the time I spend

learning the scripting language TAKES ME AWAY From designing boards and

managing production, which is what brings in the money! and besides I

really pay cadsoft for the programming expertise.

 

At the end of the day I believe Eaglecad has a lot of potential, while I

can get boards designed ( its all there as far as capabilities are

concerned) I just think that there are too many frustrating / cumbersome

ways of doing things when I know there are easier /better ways.

 

The designing of a schematic or Layout or even designing a library part is

quite easy ( once you finally figure out the Eaglecad way) , and yes this

is the main parts of an application like this. The issues are with the way

it all comes together or integrates and is managed and how the user

interacts with it. As I have stated above  the key issues are Mainly

Project management, BOM Management, and especially Libray Management.

 

Thanks for listening .

 

Dave M

 

PS Please don't condemn me for asking.

--

Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

 

  • Sign in to reply
  • Cancel

Top Replies

  • michaelkellett
    michaelkellett over 8 years ago in reply to linhtf +1
    You have replied to a six year old thread about a product that doesn't really exist any more - Eagle belongs to Autodesk and they are the people you need to ask about this. Start a new thread if you want…
  • kcadsoft
    kcadsoft over 14 years ago

    On 07/28/11 18:51, Joerg wrote:

    Klaus Schmidinger wrote:

    >> On 07/23/11 09:54, davem wrote:

    >>> ...

     

     

    >>> Q6) Are their any plans for some sort of SChematic/Layout hierarchy or

    >>> SUB-Circuits feature.

    >>

    >> It will be possible to paste from a consistent board/schematic file pair

    >> into the current project by entering the file name in the PASTE command

    >> (i.e. "paste from file"). This will also be possible via drag&drop.

    >> That way you can easily and consistently fetch various pre-routed building

    >> blocks into your project.

    >>

    >

    Getting back to Dave's question, will there be a schmematic hierarchy in

    the next release? A while ago you guys said there would be. Is it still

    planned?

     

    I'm afraid we had to drop that idea. It's not possible to

    implement that within the time frame set for version 6.

     

    Klaus Schmidinger

    --

    _______________________________________________________________

     

    Klaus Schmidinger                       Phone: +49-8635-6989-10

    CadSoft Computer GmbH                   Fax:   +49-8635-6989-40

    Pleidolfweg 15                          Email:   kls@cadsoft.de

    D-84568 Pleiskirchen, Germany           URL:     www.cadsoft.de

    _______________________________________________________________

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • kcadsoft
    kcadsoft over 14 years ago

    On 07/28/11 17:40, Andreas Weidner wrote:

    Am 28.07.2011 16:13, schrieb Klaus Schmidinger:

    >> A wire in a package drawing will be considered electrically

    >> connected to a pad/smd if one of its end points coincides

    >> with the center of the pad/smd. These need to be the exact

    >> same coordinates.

     

    That sounds VERY useful, but just for safety let me point out a potential implementation problem (with a rather high probability, you already know that, but just in case...):

    - There might be several neighbouring pads in the same row that

    need to be connected with predefined routed wires.

    - Therefore, one would draw those pads and draw a wire from

    each of them to the next one.

    - Doing this NOW makes EAGLE automatically 'optimise' all of

    the drawn wires, so that they merge into ONE wire. In the new

    scheme, this would then mean that the 'inner' pads are not

    connected anymore.

    - Therefore, during the drawing of wires in libraries for

    version 6, the WIRE command should behave the same as the

    ROUTE command does now, and no automatic optimising should

    be done with connected pads.

     

    Good point - will do.

     

    Klaus Schmidinger

    --

    _______________________________________________________________

     

    Klaus Schmidinger                       Phone: +49-8635-6989-10

    CadSoft Computer GmbH                   Fax:   +49-8635-6989-40

    Pleidolfweg 15                          Email:   kls@cadsoft.de

    D-84568 Pleiskirchen, Germany           URL:     www.cadsoft.de

    _______________________________________________________________

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • kcadsoft
    kcadsoft over 14 years ago in reply to kcadsoft

    On 07/28/11 17:40, Andreas Weidner wrote:

    Am 28.07.2011 16:13, schrieb Klaus Schmidinger:

    >> A wire in a package drawing will be considered electrically

    >> connected to a pad/smd if one of its end points coincides

    >> with the center of the pad/smd. These need to be the exact

    >> same coordinates.

     

    That sounds VERY useful, but just for safety let me point out a potential implementation problem (with a rather high probability, you already know that, but just in case...):

    - There might be several neighbouring pads in the same row that

    need to be connected with predefined routed wires.

    - Therefore, one would draw those pads and draw a wire from

    each of them to the next one.

    - Doing this NOW makes EAGLE automatically 'optimise' all of

    the drawn wires, so that they merge into ONE wire. In the new

    scheme, this would then mean that the 'inner' pads are not

    connected anymore.

    - Therefore, during the drawing of wires in libraries for

    version 6, the WIRE command should behave the same as the

    ROUTE command does now, and no automatic optimising should

    be done with connected pads.

     

    Good point - will do.

     

    Klaus Schmidinger

    --

    _______________________________________________________________

     

    Klaus Schmidinger                       Phone: +49-8635-6989-10

    CadSoft Computer GmbH                   Fax:   +49-8635-6989-40

    Pleidolfweg 15                          Email:   kls@cadsoft.de

    D-84568 Pleiskirchen, Germany           URL:     www.cadsoft.de

    _______________________________________________________________

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 14 years ago

    Am 29.07.2011 13:10, schrieb Klaus Schmidinger:

    On 07/28/11 18:51, Joerg wrote:

    >> Klaus Schmidinger wrote:

    >>> On 07/23/11 09:54, davem wrote:

    >>>> ...

    >>

    >>

    >>

    >>>> Q6) Are their any plans for some sort of SChematic/Layout hierarchy or

    >>>> SUB-Circuits feature.

    >>>

    >>> It will be possible to paste from a consistent board/schematic file pair

    >>> into the current project by entering the file name in the PASTE command

    >>> (i.e. "paste from file"). This will also be possible via drag&drop.

    >>> That way you can easily and consistently fetch various pre-routed

    >>> building

    >>> blocks into your project.

    >>>

    >>

    >> Getting back to Dave's question, will there be a schmematic hierarchy in

    >> the next release? A while ago you guys said there would be. Is it still

    >> planned?

    >>

     

    I'm afraid we had to drop that idea. It's not possible to

    implement that within the time frame set for version 6.

     

    Klaus Schmidinger

     

    Lots of people would wait half a year longer if hierarchy is implemented

    I guess image

     

    --

    Mit freundlichen Grüßen / With best regards

     

    Joern Paschedag

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 14 years ago

    Joern Paschedag wrote:

    Am 29.07.2011 13:10, schrieb Klaus Schmidinger:

    >> On 07/28/11 18:51, Joerg wrote:

    >>> Klaus Schmidinger wrote:

    >>>> On 07/23/11 09:54, davem wrote:

    >>>>> ...

    >>>

    >>>

    >>>

    >>>>> Q6) Are their any plans for some sort of SChematic/Layout hierarchy or

    >>>>> SUB-Circuits feature.

    >>>>

    >>>> It will be possible to paste from a consistent board/schematic file

    >>>> pair

    >>>> into the current project by entering the file name in the PASTE command

    >>>> (i.e. "paste from file"). This will also be possible via drag&drop.

    >>>> That way you can easily and consistently fetch various pre-routed

    >>>> building

    >>>> blocks into your project.

    >>>>

    >>>

    >>> Getting back to Dave's question, will there be a schmematic hierarchy in

    >>> the next release? A while ago you guys said there would be. Is it still

    >>> planned?

    >>>

    >>

    >> I'm afraid we had to drop that idea. It's not possible to

    >> implement that within the time frame set for version 6.

    >>

    >> Klaus Schmidinger

     

    Thanks for the info, Klaus. This is very sad. I can only tell you from

    about 25 years of experience that not having a hierarchy is a major

    show-stopper in the sales process of a schematic editor. At many large

    companies a strict top down design flow is required, so they'll never

    buy Cadsoft tools. Yet that's where the big bucks would be for you guys,

    companies that buy licenses by the baker's dozen.

     

    A classic example that I see many times: Earlier this year I was tasked

    with the design review of a set of schematics that consisted of more

    than 50 pages. Repeating hierarchy blocks were only drawn once. If you

    had placed all the instances for those like you must in Eagle then the

    schematic would have probably been 150 pages long. It was done on Altium

    and it is pretty obvious that this design would be impossible on Eagle.

    This case is not "from far out there in the world", it was a company not

    too far from you guys.

     

     

    Lots of people would wait half a year longer if hierarchy is implemented

    I guess image

     

     

    Absolutamente!

     

    --

    Regards, Joerg

     

    http://www.analogconsultants.com/

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 14 years ago

    On 7/29/11 3:41 PM, Joerg wrote:

    Thanks for the info, Klaus. This is very sad. I can only tell you from

    about 25 years of experience that not having a hierarchy is a major

    show-stopper in the sales process of a schematic editor. At many large

    companies a strict top down design flow is required, so they'll never

    buy Cadsoft tools. Yet that's where the big bucks would be for you guys,

    companies that buy licenses by the baker's dozen.

     

    No company should attempt to be everything to everybody. Eagle is Eagle,

    Altium is Altium. I can live without hierarchy and would much rather

    CadSoft focused on improving Eagle for the purpose/market that it serves.

     

    Andrew.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 14 years ago

    Andrew Sterian wrote:

    On 7/29/11 3:41 PM, Joerg wrote:

    >> Thanks for the info, Klaus. This is very sad. I can only tell you from

    >> about 25 years of experience that not having a hierarchy is a major

    >> show-stopper in the sales process of a schematic editor. At many large

    >> companies a strict top down design flow is required, so they'll never

    >> buy Cadsoft tools. Yet that's where the big bucks would be for you guys,

    >> companies that buy licenses by the baker's dozen.

     

    No company should attempt to be everything to everybody. Eagle is Eagle,

    Altium is Altium. I can live without hierarchy and would much rather

    CadSoft focused on improving Eagle for the purpose/market that it serves.

     

     

    Yep, it's up to Cadsoft or maybe now Farnell which market they want to

    serve. I just wonder why Farnell offers 10-user packages if the product

    is geared towards small projects.

     

    For a CAD company it can be very tough to survive in the small business

    and hobby markets. All I wanted to say is that not having a hierarchy is

    like leaving a huge amount of money on the table.

     

    --

    Regards, Joerg

     

    http://www.analogconsultants.com/

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 14 years ago

    James Morrison wrote:

    Joerg wrote on Fri, 29 July 2011 16:06

    >> Andrew Sterian wrote:

    >>> On 7/29/11 3:41 PM, Joerg wrote:

    >>>> Thanks for the info, Klaus. This is very sad. I can only tell you

    >> from

    >>>> about 25 years of experience that not having a hierarchy is a major

    >>>> show-stopper in the sales process of a schematic editor. At many

    >> large

    >>>> companies a strict top down design flow is required, so they'll

    >> never

    >>>> buy Cadsoft tools. Yet that's where the big bucks would be for you

    >> guys,

    >>>> companies that buy licenses by the baker's dozen.

    >>> No company should attempt to be everything to everybody. Eagle is

    >>> Eagle,

    >>> Altium is Altium. I can live without hierarchy and would much

    >>> rather

    >>> CadSoft focused on improving Eagle for the purpose/market that it

    >>> serves.

    >>>

    >> Yep, it's up to Cadsoft or maybe now Farnell which market they want to

    >> serve. I just wonder why Farnell offers 10-user packages if the

    >> product

    >> is geared towards small projects.

    >>

    >> For a CAD company it can be very tough to survive in the small

    >> business

    >> and hobby markets. All I wanted to say is that not having a hierarchy

    >> is

    >> like leaving a huge amount of money on the table.

     

    I agree with you Joerg.  I see more and more requirements for hierarchy

    support.  Design reuse of layout is tightly-integrated with hierarchy as

    well, which is another requirement for professional design which I hope

    doesn't get dropped as well.

     

     

    Yes, re-use is the other reason. I have just completed one design where

    a circuit contains two sub-circuits that will even have their own ECOs.

    In a heavily regulated industry such as medical or aerospace you have to

    do it that way.

     

     

    Too bad that hierarchy isn't going to be supported.  I would think a wait

    of 2-3 months would be worth it to get this functionality.  Unfortunately,

    CadSoft is now publicly traded which means they can't just push things off

    for quality like they used to--there are now many other factors that enter

    the equation.

     

     

    It's sad. Now I'll probably sit out V6 as well.

     

    --

    Regards, Joerg

     

    http://www.analogconsultants.com/

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 14 years ago in reply to Former Member

     

    "James Morrison" <james@eaglecentral.ca> wrote in message

    news:j0v47r$1ga$1@cheetah.cadsoft.de...

    Joerg wrote on Fri, 29 July 2011 16:06

    >> Andrew Sterian wrote:

    I agree with you Joerg.  I see more and more requirements for hierarchy

    support.  Design reuse of layout is tightly-integrated with hierarchy as

    well, which is another requirement for professional design which I hope

    doesn't get dropped as well.

     

     

    If the "project's library" (that I have proposed a while ago) would have

    been implemented, this "hierarchy/reuse" problem would have been solved by

    default....

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 14 years ago in reply to Former Member

    James Morrison wrote:

    Joerg wrote on Fri, 29 July 2011 16:06

    >> Andrew Sterian wrote:

    >>> On 7/29/11 3:41 PM, Joerg wrote:

    >>>> Thanks for the info, Klaus. This is very sad. I can only tell you

    >> from

    >>>> about 25 years of experience that not having a hierarchy is a major

    >>>> show-stopper in the sales process of a schematic editor. At many

    >> large

    >>>> companies a strict top down design flow is required, so they'll

    >> never

    >>>> buy Cadsoft tools. Yet that's where the big bucks would be for you

    >> guys,

    >>>> companies that buy licenses by the baker's dozen.

    >>> No company should attempt to be everything to everybody. Eagle is

    >>> Eagle,

    >>> Altium is Altium. I can live without hierarchy and would much

    >>> rather

    >>> CadSoft focused on improving Eagle for the purpose/market that it

    >>> serves.

    >>>

    >> Yep, it's up to Cadsoft or maybe now Farnell which market they want to

    >> serve. I just wonder why Farnell offers 10-user packages if the

    >> product

    >> is geared towards small projects.

    >>

    >> For a CAD company it can be very tough to survive in the small

    >> business

    >> and hobby markets. All I wanted to say is that not having a hierarchy

    >> is

    >> like leaving a huge amount of money on the table.

     

    I agree with you Joerg.  I see more and more requirements for hierarchy

    support.  Design reuse of layout is tightly-integrated with hierarchy as

    well, which is another requirement for professional design which I hope

    doesn't get dropped as well.

     

     

    Yes, re-use is the other reason. I have just completed one design where

    a circuit contains two sub-circuits that will even have their own ECOs.

    In a heavily regulated industry such as medical or aerospace you have to

    do it that way.

     

     

    Too bad that hierarchy isn't going to be supported.  I would think a wait

    of 2-3 months would be worth it to get this functionality.  Unfortunately,

    CadSoft is now publicly traded which means they can't just push things off

    for quality like they used to--there are now many other factors that enter

    the equation.

     

     

    It's sad. Now I'll probably sit out V6 as well.

     

    --

    Regards, Joerg

     

    http://www.analogconsultants.com/

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
<>