Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) What is the right width of trace should I choose for 220VAC
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 15 replies
  • Answers 10 answers
  • Subscribers 190 subscribers
  • Views 5734 views
  • Users 0 members are here
  • high voltage
  • trace-width
  • pcb trace
  • eagle 9.0.0
Related

What is the right width of trace should I choose for 220VAC

anthonylauly
anthonylauly over 8 years ago

image

Hi, I want to design a pcb that convert AC (220VAC) to DC (10 V), so I would use a wider trace for the Neutral and Line. First I would like to know what is the measurement unit use in the radius and width toolbox, second what is the difference of the radius and width of the trace, because when I increase the radius, nothing is happen. Third, what is the right number of radius and width for 220 VAC, thank you.

  • Sign in to reply
  • Cancel
  • anthonylauly
    0 anthonylauly over 8 years ago in reply to rachaelp

    If I have this kind of circuit  :

    image

    That what is the trace width should I use from the N and L that is connected to the diode bridge ? Because I cannot measure the current flow. The output for the diode bridge is 2 Ampere. Then what is the trace width should I choose ?

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Jan Cumps
    0 Jan Cumps over 8 years ago in reply to anthonylauly

    Why?

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • anthonylauly
    0 anthonylauly over 8 years ago in reply to rachaelp

    Hi, can I talk about this personally, with message ?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • rachaelp
    0 rachaelp over 8 years ago

    Hi Anthony,

     

    I'm going to start by a very strong word of caution. Please be extremely careful when working with mains voltages. If you don't know you can do something safely or are unsure in any way then don't proceed.

     

    So, that said, you say 10V output but you don't state the current requirements. What are they? What is the power supply type? Is it linear? Is it switching? All these things will affect the current required on the mains input. It's the current requirement which drives the required trace width. On the other hand, the voltage drives the required separation which must be maintained between the live and neutral traces, and also to any other traces, not just the continuous mains voltage but any safety standards which require a particular level of isolation. See the following link for some further explanation: http://www.ni.com/white-paper/2827/en/

     

    For the clearances specified in IPC-2221 take a look at the following link: http://www.smpspowersupply.com/ipc2221pcbclearance.html

    To calculate the trace widths required take a look at the following link: http://circuitcalculator.com/wordpress/2006/01/31/pcb-trace-width-calculator/

     

    You don't need to worry about the radius setting in the route tool in EAGLE for now, that's for mitred corners. You can use that to smooth out 45 and 90 degree bends if you wish though.

     

    Best Regards,


    Rachael

    • Cancel
    • Vote Up +7 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 8 years ago

    On 6/21/2018 7:15 AM, Anthony Lauly wrote:

     

    Hi, I want to design a pcb that convert AC (220VAC) to DC (10 V), so I would use a wider trace for the Neutral and Line. First I would like to know what is the measurement unit use in the radius and width toolbox, second what is the difference of the radius and width of the trace, because when I increase the radius, nothing is happen. Third, what is the right number of radius and width for 220 VAC, thank you.

     

    --

    To view any images and attachments in this post, visit:

    https://www.element14.com/community/message/241262

     

     

    Trace width is determined by how much current is flowing and pcb copper

    weight as well as how warm you are willing to let the traces get. There

    are online trace width calculators but I usually find the cross

    sectional area of copper and use that to determine current carrying

    capacity.

    With higher voltage the clearance is important. Conformal coating

    reduces the spacing requirement. Most important - keep it safe for the

    user/tech.

     

    HTH

    Doug

     

    • Cancel
    • Vote Up +7 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
<