element14 Community
element14 Community
    Register Log In
  • Site
  • Search
  • Log In Register
  • About Us
  • Community Hub
    Community Hub
    • What's New on element14
    • Feedback and Support
    • Benefits of Membership
    • Personal Blogs
    • Members Area
    • Achievement Levels
  • Learn
    Learn
    • Ask an Expert
    • eBooks
    • element14 presents
    • Learning Center
    • Tech Spotlight
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
    • element14 presents Projects
    • Project14
    • Arduino Projects
    • Raspberry Pi Projects
    • Project Groups
  • Products
    Products
    • Arduino
    • Avnet Boards Community
    • Dev Tools
    • Manufacturers
    • Multicomp Pro
    • Product Groups
    • Raspberry Pi
    • RoadTests & Reviews
  • Store
    Store
    • Visit Your Store
    • Choose another store...
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
  • Settings
Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) "bridge' option for pad connected to the same pin
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 4 replies
  • Subscribers 174 subscribers
  • Views 297 views
  • Users 0 members are here
Related

"bridge' option for pad connected to the same pin

kikoun
kikoun over 10 years ago

Hi,

 

When we create a device, it's easy to connect several pads to the same pin,  ( for earlier Eagle version, to several pin with the same name (ex : GND@1, GND@2 ...). When we use a device with several pad to the same pin, Eagle consider that all the pad should be connected, so there is an airwire on each pad. That 's great because it's mostly what we need.

 

But in some cases, it's not quite what we need, and routing one of those pad is not mandatory. For example I have heat-sink, with 3 fixing pads, which are all connected to one pin (usually connected to GND but not necessary ). But on my board, I have one of them that can not reach the GND plane (it's 'lost' in a high voltage area). So the only 2 options I have are :

- I consider my board finished, even if I have ariwire left. I can leave with that, but when I send my .brd file to the PCB house they ask me why this ariwire is not routed....

 

- In the library I separate the third pad. But it's worse because of 2 problems.

The first, (but not the worse) is that I have to create different packages, depending on the board where I use it (It's not necessary the same pad that must be left unconnected on every board). Second problem is that the pad is not anymore connected to the signal of the 2 other pads, so the isolation with other signals around the pad is no longer respected, since there is no signal connected to this pad, no signal = default class.

 

There is also other components (such as battery clips), that can have this problem, and some time the component itself may be use as a bridge.

 

So my little suggestion would be : when we create a symbol, and connect several pad on one pin, we can add a 'bridge' option. So Eagle will know that at least one of these pad need to be connected, and the other connection are not mandatory. The optional ariwires could have a separate color (or layer so we can display or not). After a ratsnest, the result could look like  "ratsnest : 16 airwires, 1 optional airwires" or "Nothing to do but 1 optional airwire".

 

 

Guillaume.

  • Sign in to reply
  • Cancel
  • lbrer
    0 lbrer over 10 years ago

    Hallo Guillaume

     

    Very good suggestion not least for librarians.

    There is nothing to attach..

    You mean something like this ?..

    • Device
    • Connect
    • Append with FUTURE-Option

    image

    best regard.. to Cadsoft too

    Hans

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 10 years ago

    Hi,

     

    almoust the same function is realised by EAGLE. You find it under "multiple pads connections" under the option "all" or "any", described in the manual, chapter 8.4.

     

    Best regards...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • lbrer
    0 lbrer over 10 years ago in reply to Former Member

    hi

    i found it

    Thanks

    P.S. my nice Picture...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • kikoun
    0 kikoun over 10 years ago in reply to Former Member

    Hi,

    I didn't notice that Eagle already has this option...

     

    Anyway, there is room for improvement :

      - Not all the pad of a same group may have the same status, some connection may be mandatory, some not. (I may admit that it's not a big deal, because we can use 2 different symbol pins).

      - Optional airwires (on a different layer) are missing, and that is a problem, because as soon as one pad is connected, it's impossible to start a new route from one of the others pads (same appends for ending a route) ! it's almost impossible to create a route to reinforce the link between to pad ! By displaying the optional airwires layer it will be easy to :

                - start and finish a route even if one connection had been made: "external connection is not mandatory" doesn't mean that "don't do any external connection" !!!!!

                - it could be helpful to view  these links ( for following the current paths, or for placing purpose etc...)     

      - The ratsnest report should clearly display how many optional airwires have no external connection, this indication is really useful.

     

    Guillaume.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
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
An Avnet Company © 2025 Premier Farnell Limited. All Rights Reserved.