Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
Forum Special Promotion for EAGLE PCB Users
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 19 replies
  • Subscribers 191 subscribers
  • Views 3115 views
  • Users 0 members are here
  • frontpage
  • eagle pcb
  • altium circuitstudio
Related

Special Promotion for EAGLE PCB Users

circuitstudioadmin
circuitstudioadmin over 9 years ago

Hey, guys! We just wanted to let you know that we are running a special promotion exclusively for users of the Eagle PCB tool! We feel PCB designers should be able to buy a product and once they have paid that's that!!

 

Here's what we're offering: if you move over from Eagle's PCB design tool before the end of this month we are providing CircuitStudio for USD 495*. That's 50% off current our current USD 995 price! To take advantage of this great deal, visit our website!

 

Hit me up if you have any questions!

 

-Camaryn Bolton

 

*Prices quoted are for USA region.

  • Sign in to reply
  • Cancel
  • balearicdynamics
    balearicdynamics over 9 years ago in reply to rachaelp

    I have used Eagle on Windows for some years, it is not so blocking for me as I am working on Mac as well as you do, but I used too a number of VM on it. Managing with projects involving hardware and firmware development it is almost impossible. As far as I know, just to mention few, Rhino for 3D printing design, AVR Studio, Cypress PSoC programming, Mill Machine control etc. etc. needs windows. Last but not least as I develop on a multiplatform environment on both VisualStudio native applications and drivers and Qt I am almost used to work on Windows, Mac and Ubuntu at least together image

     

    Remain the fact that this is a minus point to the Altium circuit designer software. Anyway I deserve further considerations on ergonomy and usability after I have installed the trial version and used it for a while (hopefully before the end of this month to decide about their offer image )

     

    Enrico

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 9 years ago in reply to balearicdynamics

    Hi Enrico,

     

    You're absolutely right, there is no substitute for trying it out, I will do that sometime hopefully. I was just hoping that from the current user feedback I'd get warmer feet before trying it. The past DXP experience is now worth little since it was so long ago.

     

    rachaelp it is a good point that if subscription is a road they cannot steer away from then there is a huge leap between the two licenses that could be mitigated with a third option.

     

    The 'maker' option is something that many businesses have not executed well on. For 'makers' the old student license model doesn't work for them. And possibilities for them are more sophisticated nowadays and they don't want to be tied to severe restrictions like 2-layer. And they are more open to using free options like KiCAD.

     

    This is a different target customer, and an ultra-low cost like $10 per _year_ (not month) would instantly get tons of effectively beta-testers for early releases of EAGLE or CircuitStudio or otherwise, i.e. Autodesk or Altium could get these users to do their testing for them.

     

    Matlab *almost* had the right idea for 'makers' (in their case they called them home users), but their ultra-low cost was still slightly high to attract many 'makers' I suspect, and they had a broken model where you were locked out of spending more money with them for toolboxes, unless a support cost was paid.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • balearicdynamics
    balearicdynamics over 9 years ago in reply to shabaz

    Shabaz, I agree with your point, but - I try always to be pragmatic - I suggest you pass over your prejudice and try a new version. We all know very well your great capabilities in testing and reporting new products so your opinion on the behaviour of last version of this product swill be very appreciated.

     

    BTW, I confirm that one of the bigger lacks of Altium is just the single-platform support. The other non-trivial limitation is implicitly explained in the minimal requirements for the software installation:

     

    • Windows 7 or Windows 8 (32-bit or 64-bit)
    • IntelRegistered CoreTm i5 processor or equivalent
    • 8 GByte RAM
    • 3 GByte hard disk space (Install + User Files)
    • NVIDIARegistered GeForceRegistered GT 640 series or AMDRegistered RadeonRegistered HD 7770, 1024MB (or more) graphics card or better, supporting DirectX 9.0c and Shader model 3 (or later)
    • Dual monitors with at least 1680x1050 (widescreen) or 1600x1200 (4:3) screen resolution
    • USB2.0 port if connecting to 3D Mouse
    • 3D mouse for 3D PCB design, such as the Space Navigator

     

    (got from the Altium site). This means that with smaller machines this does not works fine? Or does not work at all? What do they mean for the 3D mouse availability? I regulalrly design 3D components with complex CAD applications (e.g. Rhino and more complex too) with just a mouse or a touch or a Wacom tablet with no difficult...

     

    Enrico

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • rachaelp
    rachaelp over 9 years ago in reply to balearicdynamics

    Enrico Miglino wrote:

     

    Last but not least, Eagle has both Mac and Windows versions, and Altium ?

    Altium is Windows only as far as I am aware. This alone makes it worthless to me.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • rachaelp
    rachaelp over 9 years ago in reply to shabaz

    I'm personally not jumping from EAGLE to Altium. I have a v7 Pro license so the logical jump "up" for me would be Altium Designer and not Circuit Studio but even with their 40% off promotion it is still WAY more money than EAGLE even before you factor in the cost of the subscription required to be able to access support and updates after the first year which is something people seem to forget. Add in that it's Windows only so I would need to boot into a Windows VM on my Mac to do design work and it's even less of an option.

     

    EAGLE does have some mitigation against not being able to continue once you let your subscription lapse. Designs are still fully readable and can be exported to manufacturing in the free version and you can always drop back to v7 if you need to edit something and your v8 subscription has lapsed.

     

    If you only need 6 layers for a small amount of time then you can upgrade your subscription to Premium for the duration of that project and then drop down to Standard or freeware when you don't need that capability.

     

    I do think they could staunch a lot of the bleeding of the existing user base by introducing two more licensing tiers:

     

    1) Low cost non-commercial license for Makers.

    2) Intermediate level license between Standard and Premium as currently the step between the two licenses is large.

     

    They clearly aren't going to reverse course on the subscription model. I do wish there was an option to pay a "full and final settlement" to allow the permanent use of the version you had on subscription once you let your subscription lapse but I don't know if they have the capability to implement such a thing into the subscription system or not. I don't see this happening any time soon if ever though, and being able to fall back to a v7 license mitigates a lot of the issues (for me at least) anyway.

     

    Best Regards,

     

    Rachael

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • balearicdynamics
    balearicdynamics over 9 years ago in reply to dougw

    I have other concerns but also concerns ... It's tempting but for now it is not the worth. There are some easy questions that I will see how can be answered and how easy it is to do.

     

    How to convert Eagle previous projects to Altium?

    How to reuse the custom libraries already designed?

    How is possible to generate a g-code for milling prototypes with Altium? This is my typical pre-prototyping PCB phase to avoid making many PCB circuits prototyping outside and this save an incredible amount of fime.

     

    These are just the most important concerns I have. I have just downloaded now the free trial to have time at least to make a test before consciously deciding what to do.

     

    Last but not least, Eagle has both Mac and Windows versions, and Altium ?

     

    A reply by the author of this post is also welcome.

    Enrico

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 9 years ago in reply to dougw

    I'm not averse to subscription but the significant cost increase for 6-layer with EAGLE means CircuitStudio will be lower cost over a couple of years, based on risk assessment that 6-layer may be used for a few months per year.

    However what's putting me off CircuitStudio is that when I tried their DXP product many years ago for a complete, reasonably complex project, it had far lower productivity than EAGLE. I could have done the job in half the time with EAGLE. I hope that has changed, but from the screenshots it doesn't seem to look much different. We give a lot of time learning how to use a CAD package, and the hope is it is in exchange for improving productivity.

    To compound that the second reason I get cold feet with putting effort into CircuitStudio is that there have been many comments from users about strange impacts due to CircuitStudio being a deliberately cut-down product. Just one example that was concerning to me was that polygon priority could not be controlled except by the order that polygons are created. To me this seems like trying to deliberately slow down the user. They may as well have nag screens to watch an advert in exchange to allow a user to type in a priority, it is that silly.

    So, for me I can't find an attractive package and I'm holding out until I hear that some of the deliberate cut-down functionality doesn't slow down productivity, and hearing more about ways that the work effort to create pads and parts and schematics and layout can be as fast compared to EAGLE, not just for CircuitStudio but for other packages too (for me I've ruled out DipTrace, I can't recall the reason but it was based on the information on their website).

    So like you, I'm also waiting out for this year and postponing the decision.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • dougw
    dougw over 9 years ago

    It is tempting.

    I have a full Eagle license and probably will be okay for about a year. The big question for me is which package will be the next highly popular package? The ability to share designs with a large user base is important.

    Eagle has a huge user base compared to other packages. What will happen to this user base?

    I expect their user base to erode substantially due to the new license scheme, but will they hang on to enough market share to make it a market leader in terms of seats?

    The door is open for others to take some of the user base, but are any other packages attractive enough to take a really significant share?

    I think it will still be a tough decision in a year when I will be considering choices as I am not keen on the subscription model.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • balearicdynamics
    balearicdynamics over 9 years ago

    Sounds interesting. I am just evaluating an Eagle alternative; I suppose the previous versions soon will not be available and - obviously - never will be updated. I am not sure I can stay inside your limited time offer (that is anyway a great opportunity).

     

    Enrico

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
<