3M
  • Products & Partners
  • Manufacturers
  • 3M
  • More
  • Cancel
3M
Forum Have a technical question, ask 3M's UHM expert Roland Nuiten
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join 3M to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 4 replies
  • Subscribers 7 subscribers
  • Views 1066 views
  • Users 0 members are here
  • connectors
  • interconnect
  • help
  • signal_integrity
  • expert
  • backplane
  • 3m
  • high_speed
  • roland_nuiten
Related

Have a technical question, ask 3M's UHM expert Roland Nuiten

tech6
tech6 over 16 years ago

 

This thread has been closed to new questions.

However, we welcome you to Post Your Question about Communications in the element14 Community Wireless Communications Technology group. You'll find many fellow members and experts who have just the answer you're looking to find! 

 

Thank You, Your Friends at element14 Community

 

 

rnuiten.jpg

 

Roland Nuiten

Roland has been working as an application development engineer for 3M High-Speed products for 7 years now and has been working as a E E in the connector industry for 15 years.

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 15 years ago

    Hi Roland I have a question. Not so long ago I decided to create a circuit with floating cores. Idea is that main single core can be split  into small ones (with shorter bit range)  and joined back into big. For example one 128 core splits into 8 16 bit cores or 2 64 bits. Idea is that program code which is usually much smaller than 32 bits can be processed better. It is a kind of optimization of used area and number gates involved in processing. (I heard about one company which created circuit with split cores in 2006 but later there were no any info on that project.)

    But now I got serious problem with instruction decoding. Each combination of cores requires special connection to the instruction set. So I got to many signal lines which create numerous time delays and circuit becomes very complicated for simulation. My question is - Is it possible to create high speed interconnect between instruction decoders and core units (arithmetic units, memory) so that each core will prefetch instruction independently and total time delay will be  enough small?(not like in reconfigurable systems).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 15 years ago

    Hi Roland I have a question. Not so long ago I decided to create a circuit with floating cores. Idea is that main single core can be split  into small ones (with shorter bit range)  and joined back into big. For example one 128 core splits into 8 16 bit cores or 2 64 bits. Idea is that program code which is usually much smaller than 32 bits can be processed better. It is a kind of optimization of used area and number gates involved in processing. (I heard about one company which created circuit with split cores in 2006 but later there were no any info on that project.)

    But now I got serious problem with instruction decoding. Each combination of cores requires special connection to the instruction set. So I got to many signal lines which create numerous time delays and circuit becomes very complicated for simulation. My question is - Is it possible to create high speed interconnect between instruction decoders and core units (arithmetic units, memory) so that each core will prefetch instruction independently and total time delay will be  enough small?(not like in reconfigurable systems).