Alpha Wire
  • Products & Partners
  • Manufacturers
  • Alpha Wire
  • More
  • Cancel
Alpha Wire
Forum Insulated versus not insulated copper wire
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Alpha Wire to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 14 replies
  • Subscribers 10 subscribers
  • Views 5476 views
  • Users 0 members are here
  • copper
  • wire
  • insulated
Related

Insulated versus not insulated copper wire

e14 Contributor
e14 Contributor over 11 years ago

I noticed someone used .0808 copper wire that is not insulated for a project, but I only have insulated, and the parts list does not make a distinction of which one to use...if I use the insulated wire, will that make a difference in the outcome of the project? Thank you!

  • Sign in to reply
  • Cancel

Top Replies

  • D_Hersey
    D_Hersey over 11 years ago +1
    Oh, John, I am fighting a bitter and fitful struggle against ignorance myself. Pardon my tone, I am distracted by extraneous events. Efficiency of your power supply, which you were brave to construct and…
  • D_Hersey
    D_Hersey over 11 years ago in reply to jw0752 +1
    Note that when you add windings to a core, you are increasing your B over an area, rather than a line. So if your twenty turns yields N quatloos of inductance, putting forty turns upon the same core yields…
  • D_Hersey
    D_Hersey over 11 years ago +1
    http://www.arrl.org/files/file/Technology/tis/info/pdf/8405015.pdf http://www.fair-rite.com/newfair/index.htm http://www.cwsbytemark.com/
Parents
  • jw0752
    0 jw0752 over 11 years ago

    Is it possible that what you see as uninsulated wire is really wire that has an enamel insulating coating? This type of wire is used on transformers and inductors and looks like bare wire but in fact is quite well insulated. Here is a coil that I wound using enameled wire that may look uninsulated but really is insulated.

    John

     

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • D_Hersey
    0 D_Hersey over 11 years ago in reply to jw0752

    What is the material in that transformer?  Is it 52 mix?  Is that a transductor or a transformer?  What size core?  How many turns?  What inductance?  What SRF? Why did you array the coils separately as you have, rather than wrap the core with a twisted pair?  What potentials are you operating at?  If that is used in some kinda saturation-based gadget oscillator, what frequency does it operate at?

     

    How you doin'?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jw0752
    0 jw0752 over 11 years ago in reply to D_Hersey

    Hi Don,

    It is a ferrite 0.5 inch core. The wire came out of a small transformer that I salvaged from an old computer switching supply. There are (2) 20 turn windings. If the windings are not arrayed properly the reason is ignorance. As far as winding it was very difficult with these old eyes. I was nearly permanently cross-eyed when I finally completed it. It is part of a Joule Thief circuit operating at 1.5 volts. I believe the frequency was about 45kHz.

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • D_Hersey
    0 D_Hersey over 11 years ago in reply to jw0752

    Note that when you add windings to a core, you are increasing your B over an area, rather than a line.  So if your twenty turns yields N quatloos of inductance, putting forty turns upon the same core yields 4*N quatloos of inductance.  Since you paid for a finite number of magnetic domains when you bought your core, saturation in the latter situation would come proportionately sooner.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • D_Hersey
    0 D_Hersey over 11 years ago in reply to jw0752

    Note that when you add windings to a core, you are increasing your B over an area, rather than a line.  So if your twenty turns yields N quatloos of inductance, putting forty turns upon the same core yields 4*N quatloos of inductance.  Since you paid for a finite number of magnetic domains when you bought your core, saturation in the latter situation would come proportionately sooner.