Altium CircuitStudio
  • Products
  • Manufacturers
  • Altium CircuitStudio
  • More
  • Cancel
Altium CircuitStudio
Blog CircuitStudio 1.5 Is Now Available
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Altium CircuitStudio to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: alexsander_altium
  • Date Created: 24 May 2018 11:23 PM Date Created
  • Views 5245 views
  • Likes 1 like
  • Comments 12 comments
  • circuitstudio
  • update
Related
Recommended

CircuitStudio 1.5 Is Now Available

alexsander_altium
alexsander_altium
24 May 2018

We’re happy to announce an update for CircuitStudio, CircuitStudio 1.5. Although this is not a major feature packed release -that's on its way- its still an important, and to be honest a much needed one. CircuitStudio is alive and still being developed. What this means is more regular updates, we even have planned another update to CircuitStudio by the end of this year.

 

I’m sure you guys want to know what’s new and what’s coming. So let me just jump into it. CircuitStudio 1.5 is currently out and ready for you to enjoy. In addition to general maintenance, there are three main features for this release of you should be aware of:

 

Selection Filter

Define what you want selected before you make a selection. This preselection filter enables you to accurately select everything you need, and nothing you don’t. This is a great filter when you want to pick out a certain type of object on a crowded board. For instance you can select a certain group of vias and then change the hole size for all the vias at once.

 

The selection filter can be accessed from the Home tab. To select a specific type of object click on the object type from the list. You may select one or multiple types of objects at once. To be able to select all object types select All Objects.

 

image

 

Layer sets

The Layer Sets Manager dialog allows designers to create, edit, and remove layer sets. Using layer sets allows designers to view only specific layers included in these sets. This is useful when only working on specific layers to help reduce clutter in the workspace.

 

To access the Layer Sets Manager right click on the layer tabs bar on the bottom of the workspace. Then click on Layer Sets > Board Layer Sets… Once the Layer Sets Manager is open you may create a new set or edit an existing one by checking the layers you want to include from the right.

 

image

 

3D PDF

Give you fabricators and project managers a much better understanding of your design intent by sharing with them a 3D PDF. Allow anyone on the team to view your PCB design with 3D PDFs as part of your output documentation. Interactively view board shape and components from any compatible PDF viewer.

 

A 3D PDF may be created as part of a batch output by using the Generate outputs button on the Project tab or by itself through the Printing button on the Outputs tab. Once the file is generated it will be ready to be sent or opened.

image

 

In addition to the good news above, we have even more good news for you. There is a roadmap for CircuitStudio and yes we will be releasing this. We want everyone to be up to date with CircuitStudio, no more wondering what’s going to happen. We’re excited to continue to improve CircuitStudio and empower the community with a powerful yet affordable design tool.

 

 

How To Install

 

You are able to update directly within CircuitStudio or have a clean installation by going to our download page. If you prefer to update your CircuitStudio installation:

 

  1. Select View>>Start to open the Home page
  2. While signed in, select Extensions and Updates from the My Account pull-down menu
  3. From the Extensions & Updates page, click the Updates tab
  4. Click the CircuitStudio 1.5.0 (Build 13) update link to start the update process
  5. Restart CircuitStudio (restart notification window will pop up)

 

 

New to CircuitStudio?

 

Why not download the free 30 day evaluation and give it a try, discover what you've been missing!

 

Expired Maintenance?

 

It's quick and easy to renew your maintenancerenew your maintenance to get access to this update. Don't worry if it your existing maintenance subscription has lapsed, you can purchase a new 12-month maintenance subscription and it will start from the date of purchase (no back dating, no surcharges, no fuss).

  • Sign in to reply

Top Comments

  • juhaszzs
    juhaszzs over 8 years ago +2
    I think the CircuitStudio users this wants... and not that what we got. Altium CircuitStudio Community Poll Q2) If you could improve something, or add a single feature to CircuitStudio, what would you…
  • voltsandjolts
    voltsandjolts over 8 years ago +1
    Layer Sets!!! Excellent, thank you.
  • astacvi
    astacvi over 8 years ago

    I cannot seem to get this update. Within CS, it says "platform up to date." When I try to run the installer manually, I get:

     

    Cannot find package in directory

    "C:\Users\*username*\Downloads\Altium Cache

    Please make sure installation files are available and retry to continue.

     

    How can I get this update? These features seem to be something I really want.

     

    BTW, I had the same problem trying to update to 1.14.1. It never worked until a support tech sent me a link to an offline installer. What can I do to resolve this issue?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • voltsandjolts
    voltsandjolts over 8 years ago

    Layer Sets!!! Excellent, thank you.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
<