Altium CircuitStudio
  • Products & Partners
  • Manufacturers
  • Altium CircuitStudio
  • More
  • Cancel
Altium CircuitStudio
Blog Multilayer PCB Design Tips
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Altium CircuitStudio to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: e14softwareuk
  • Date Created: 14 Nov 2017 2:37 PM Date Created
  • Views 1387 views
  • Likes 0 likes
  • Comments 0 comments
  • altium
  • altium circuit studio
  • circuitstudio
Related
Recommended

Multilayer PCB Design Tips

e14softwareuk
e14softwareuk
14 Nov 2017

Shy boy and girl on park bench

    

Doing something new for the first time can be difficult. Baby birds probably don’t appreciate being pushed out of the nest and teenagers are nervous before their first real date. I, personally, was scared to death on my first date. However, I’m glad that I took that first step because that milestone was a great moment in my life.

 

Now here you are with a different, although equally important, milestone of your own; you are about to design your first multilayer PCB layout. Are you consumed with questions and concerned about not making a mistake? If so, then don’t worry. You’re just like the rest of us and we’ve got some information here to help you. We’ll talk about some library issues to watch out for, as well as some general design guidelines to get you started.

 

Sometimes you have to take a step of faith that you will be able to accomplish what you are setting out to do and then do it. Designing your first multilayer board is one of those steps of faith for a PCB designer. Let’s jump in then, and help you to get going on this design.

MAKE SURE THAT YOUR LIBRARY IS SET UP FOR MULTILAYER DESIGNS

The first thing to look at when doing multilayer PCB designs is your CAD library. If you have only been designing single or double sided boards, your library may not be set up for multilayer configurations. Here are three areas to look at:

 

Negative plane layers: Negative image plane layers are often used to create power and ground planes on multilayer PCB layouts. Some CAD tools require clearances built into pad and footprint shapes for drilled holes in a negative plane layer. If you are using one of these tools, make sure that your pad and footprint shapes are set up with the correct negative plane clearances. If your shapes are not set up for these clearances, then you will create a short.

 

Pad shapes on inner signal layers: Some designs use different pad shapes on exterior layers than on inner layers. For instance, pin 1 pads often have a square shape for visual recognition instead of the round shape that it normally has on inner layers. If your libraries are not set up for multilayer configurations, you may not get the desired pad shapes on inner signal layers.

 

Drawing pieces: If you are creating your fabrication and assembly drawings from within your layout tools, you probably have different logos, tables, and views saved to your library. These will have to be modified for multilayer boards.

 

3D picture of a variety of PCB components

Make sure that your library parts are set up for multilayer PCB design

 

 

 

 

UNDERSTAND THE REQUIREMENTS OF THE FABRICATION SHOP

There are a lot of important benefits to a multilayer PCB design over single and double-sided boards. Not only will you be able to save space and increase design density, but you will have better control over signal integrity issues as well. The key is to work ahead with your fabrication shop so that you understand their requirements for manufacturing multilayer designs before you start.

 

Fabrication shops will have different requirements based on the level of board technology that they are able to build to. Some shops may not be set up to build boards above a certain layer count or with very small trace and spacing widths. If you exceed these limitations, it may increase your fabrication costs, or result in the board not being able to be manufactured.

 

Take via types for example. Fabrication shops typically handle regular thru-hole vias, but you should check with them first before using buried, blind or micro vias. And as we mentioned, you should also confer with them about trace width and spacing, and the amount and configuration of the board layers. All of these factors can have an impact on the manufacturability of the circuit board, and you should have a clear understanding of them before you start your design.

 

3D image of a multilayer PCB design

Multilayer PCB design

 

 

 

 

MULTILAYER PCB DESIGN TIPS

Now that your library is set up and you’ve checked ahead with the fabrication shop, you are ready to design your multilayer PCB design. Here are some design tips for multilayer boards that you may not be aware of:

 

  1. Route adjacent signal layers in opposite directions. If you have adjacent signal layers on layers 2 & 3, then route one horizontal and the other vertical. This will help to guard against broadside crosstalk problems.
  2. Use power and ground plane layers. Not only will this help distribute your power and ground evenly, but it will create amicrostrip structure that will help your signal integrity.
  3. Reduce the size of inner signal layer thru-hole pads. Check if the fabrication shop will allow smaller inner layer pads for thru-hole parts and vias. If so, the reduced pad sizes will open up more routing channels.

 

Taking your first steps into designing a multilayer PCB design can be overwhelming. It might not be as frightening as being pushed out of the nest or going on your first date, but it may be pretty close. Hopefully these tips will help lighten the burden on your shoulders and help you to fly.

 

Another thing that can help you with your next PCB layout is using high quality PCB design software, like Altium Designer and Altium’s CircuitStudio, for the job. CircuitStudio has the functionality to help you create library parts, manage your layer structures, and place and route a complex multilayer board designs at a very affordable price.

 

Would you like to find out more about how Element14 can help you with your next multilayer PCB design? Talk to us today.

 

Many thanks to Altium for permission to reproduce this post.