Altium CircuitStudio
  • Products & Partners
  • Manufacturers
  • Altium CircuitStudio
  • More
  • Cancel
Altium CircuitStudio
Blog PCB Design for Manufacturing: Avoiding Critical Design Mistakes
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Altium CircuitStudio to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: e14softwareuk
  • Date Created: 22 Nov 2017 1:48 PM Date Created
  • Views 1442 views
  • Likes 2 likes
  • Comments 0 comments
  • altium
  • circuitstudio
  • altium circuitstudio
Related
Recommended

PCB Design for Manufacturing: Avoiding Critical Design Mistakes

e14softwareuk
e14softwareuk
22 Nov 2017

cakes burning in oven

 

 

 

I swear I would have been on the journey to be the next MasterChef if I had not completed my engineering degree. Not because I’m terrifically good at cooking, but because I didn’t give up after a horrifying attempt to cook fried rice vermicelli. Failing to soak those long threads of noodles resulted in pasta with a hard wire texture that was beyond salvageable. This was a good example of what can happen to a dish when you don’t follow directions carefully.

 

Like in cooking, mistakes are bound to happen in electronics design, even for the most meticulous designers. But some mistakes are critical enough that you will have to scrap the entire printed circuit board (PCB) and start over. When you’re patiently waiting for a prototype PCB to test your circuits, this can spell costly delays in the product development cycle.

CRITICAL DESIGN MISTAKES IN PCB MANUFACTURING

We all hate to make mistakes. But in reality, it takes two or three tries to get the perfect design. As long as we fix mistakes in the early designs by simply cutting off tracks or jumper wires, the impact on the development process is minimal. The same can’t be said about some of the following mistakes that almost always ruin your PCBs.

 

1. Using the Wrong Footprint

While most passive components are available in both through-hole and surface-mounted form factors, integrated circuits (ICs), especially special function ICs, are produced in only a few package types. Confusing a Small Outline Integrated Circuit (SOIC) and a Shrink Small Outline Package (SSOP) may result in trying to fit a smaller IC on a larger footprint, or vice versa.

 

Remember to verify the package type of your components by thoroughly checking their datasheets. Don’t make assumptions and ensure that both the dimensions of the IC and its pitch size are correct. I learned my lesson when I mistakenly used the ‘narrow’ version of a SOIC since the ‘wide’ version had the same pitch size.

 

Electronic component on a PCB
Use the correct IC components to avoid design errors that will affect the design footprint.

 

 

 

2. Misaligning the Address Bus

During my early years as a designer, high-density memory requirements meant using parallel Flash memory or Static Random Access Memory (SRAM). I had to deal with up to 23 bits of address and 8 bits of data signals. A mistake in matching the address pins of the microcontroller to the memory components could result in an unusable prototype or spending a couple of days cutting off and rewiring the signals with jumper wires. To avoid this, I had to fully understand the addressing bus of the microprocessor and how each memory chip should be connected.

 

3. Bad Ground Plane Design

The effect of a proper ground plane design may not be obvious in simple digital circuits. But you may have a batch of populated, but unacceptable PCBs if you ignore the ground plane best practices for analog or mixed circuit designs. This can cause interference and cross-talk, making it necessary to quickly produce a better design.

 

While I’m lucky enough to have salvaged PCBs with bad ground connections, I now ensure that future designs adhere to proper ground plane designs. Remember to separate analog and digital grounds by a single point when it is appropriate and consider the current flow path.

 

4. Incorrect Mounting Holes

Mounting holes can be helpful for reducing electromagnetic interference (EMI). However, if your mounting hole coordinates are off then your well functioning board will not be secured to its casing. Make sure that your coordinates are exact, otherwise there might not be a clear path for to secure your screw.

 

For designs where the PCB is mounted to an enclosure, it is vital to start the PCB layout with the mounting holes placed on the right coordinate before populating other components.

 

Worker drilling a hole
Drilling won’t help when you get the hole position wrong in the first place.

 

 

5. Excessive Current Density On Thin Copper

What could go wrong when you’ve covered all your bases by performing power budget calculations at a subcircuit level? A common mistake is failing to consider the total current passing through the primary voltage signal track. Another common mistake is failing to provide adequate copper width. These mistakes can result in overheating or, in certain cases, for the conducting copper to totally break apart. The right power budget analysis should give you a clear indication of the required track width.

 

For users who want professional design software but aren’t in the market for Designer, Altium’s CircuitStudio is the perfect solution.

 

Many thanks for Altium for permission to reproduce this post