Altium CircuitStudio
  • Products & Partners
  • Manufacturers
  • Altium CircuitStudio
  • More
  • Cancel
Altium CircuitStudio
Altium CircuitStudio Forum Edit Board Shape
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Altium CircuitStudio to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Locked Locked
  • Replies 4 replies
  • Subscribers 91 subscribers
  • Views 2844 views
  • Users 0 members are here
Related
This discussion has been locked.
You can no longer post new replies to this discussion. If you have a question you can start a new discussion

Edit Board Shape

Squintz
Squintz over 6 years ago

I have a completed board and I noticed that when I view Board Information it says one of the sides is off by just a tiny bit. So, I went to click Edit Board Shape thinking I could click on the lines and have it snap into place or possibly even manually enter the coordinates. However, when I click on Edit Board Shape I can't click anything. In fact it seems that I get stuck in that command and the only way out of it is to close the file and re-open. Am I doing something wrong?

  • Cancel

Top Replies

  • adamwebber
    adamwebber over 6 years ago +1
    What you are doing sounds funny. Maybe an installation error or some kind of glitch. Something to contact the makers of the software but good luck with that. I find that one of the easiest ways to define…
  • tarribred61
    tarribred61 over 6 years ago +1
    Yes this does seem to be messed up. Mine behaves like you describe and it may be not unique to your install. To add to the prior response, I typically define the board shape on another mechanical layer…
  • jf_vt
    jf_vt over 5 years ago +1
    I have the very same issue as the original poster Is it a bug?
Parents
  • tarribred61
    tarribred61 over 6 years ago

    Yes this does seem to be messed up. Mine behaves like you describe and it may be not unique to your install.  To add to the prior response, I typically define the board shape on another mechanical layer (e.g. layer 20) and I can add in dimensions on a corresponding mechanical layer (e.g. layer 21).  Often these have been imported from a DXF file from a mechanical designer and then I modify them as needed to add pull-backs or edge cutouts and such.  Then I select the outline and copy it to the board outline layer and set the line width to be very thin.  Then I can define the board shape from the outline.

     

    After that I can edit the lines on the board outline layer as needed and redefine the board shape as needed.  The board outline then gets copied to the keepout layer and the lines made thicker to define the board copper pull-back from the edge.

    • Cancel
    • Vote Up +1 Vote Down
    • Cancel
Reply
  • tarribred61
    tarribred61 over 6 years ago

    Yes this does seem to be messed up. Mine behaves like you describe and it may be not unique to your install.  To add to the prior response, I typically define the board shape on another mechanical layer (e.g. layer 20) and I can add in dimensions on a corresponding mechanical layer (e.g. layer 21).  Often these have been imported from a DXF file from a mechanical designer and then I modify them as needed to add pull-backs or edge cutouts and such.  Then I select the outline and copy it to the board outline layer and set the line width to be very thin.  Then I can define the board shape from the outline.

     

    After that I can edit the lines on the board outline layer as needed and redefine the board shape as needed.  The board outline then gets copied to the keepout layer and the lines made thicker to define the board copper pull-back from the edge.