Altium CircuitStudio
  • Products & Partners
  • Manufacturers
  • Altium CircuitStudio
  • More
  • Cancel
Altium CircuitStudio
Altium CircuitStudio Forum POLYGON POUR - CLEARANCE
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Altium CircuitStudio to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Locked Locked
  • Replies 2 replies
  • Subscribers 88 subscribers
  • Views 1532 views
  • Users 0 members are here
Related
This discussion has been locked.
You can no longer post new replies to this discussion. If you have a question you can start a new discussion

POLYGON POUR - CLEARANCE

batista
batista over 6 years ago

Estive testando várias regras para funcionar com POLYGON POUR (CLEARANCE) não deu certo, aí tive a ideia de criar uma regra

com o mesmo nome POLYGON POUR, defini o cearense EX: 0.2, 0.3 funciona desde que o valor – (ARC APPROXIMATION)

Seja igual ao cearense definido na regra POLYGON POUR, não sei se é a forma certa para funcionar, mas deu certo conforme

a imagem abaixo.

 

I've been testing several rules to work with POLYGON POUR (CLEARANCE) it didn't work, so I had the idea to create a rule

with the same name POLYGON POUR, I defined the Ceará EX: 0.2, 0.3 works as long as the value - (ARC APPROXIMATION)

Be equal to the Ceará defined in the POLYGON POUR rule, I don't know if it's the right way to work, but it worked as

the image below.

 

 

image

  • Cancel
Parents
  • pizutti
    pizutti over 6 years ago

    Another option is to set a clearence for the Net of the Polygon, like this:

     

    image

     

    image

     

    so the polygon conected to that Net will be poured with the defined clearence for all other objects, you can even set the clearence between two Nets, by setting something in "Where the second object Matches".

     

    And If there are a lot of polygons with different Net's, you can create a class on the schematics and connect that class on the Nets that you want to have that clearence:

     

    image

     

    image

     

     

     

     

    thats a Polygon connect I have created without thermals for this class, the process is the same for clearence.image

     

     

     

     

    Att.

    Pablo B. Pizutti

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
Reply
  • pizutti
    pizutti over 6 years ago

    Another option is to set a clearence for the Net of the Polygon, like this:

     

    image

     

    image

     

    so the polygon conected to that Net will be poured with the defined clearence for all other objects, you can even set the clearence between two Nets, by setting something in "Where the second object Matches".

     

    And If there are a lot of polygons with different Net's, you can create a class on the schematics and connect that class on the Nets that you want to have that clearence:

     

    image

     

    image

     

     

     

     

    thats a Polygon connect I have created without thermals for this class, the process is the same for clearence.image

     

     

     

     

    Att.

    Pablo B. Pizutti