Altium CircuitStudio
  • Products & Partners
  • Manufacturers
  • Altium CircuitStudio
  • More
  • Cancel
Altium CircuitStudio
Altium CircuitStudio Forum Circuit Studio - Part created but then not found
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Altium CircuitStudio to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Locked Locked
  • Replies 5 replies
  • Subscribers 91 subscribers
  • Views 1872 views
  • Users 0 members are here
  • altium
  • part
  • circuitstudio
  • creation
  • stg
Related
This discussion has been locked.
You can no longer post new replies to this discussion. If you have a question you can start a new discussion

Circuit Studio - Part created but then not found

e14 Contributor
e14 Contributor over 10 years ago

Hi

Is anyone else finding that having created a part in CircuitStudio, complied the library with no errors reported that when one goes to place that component in a schematic that even though it is visible in the Library Circuit Studio reports ... "Failed to load <library path.schlib> STG <part name> could not be found"

 

If so any clues as to how to stop it doing this?

 

Thanks

 

Neil

  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    Hi Neil

     

    I am having this problem also.

     

    I am very new to this software having used Eagle for a number of years. I have followed the information in the help on creating parts but the links between the schematic and the footprints don't seem to work.

     

    I have a library for through hole capacitors that has 5 or so foot prints in it for various sizes of caps but the software wont included it for some reason.

     

    I notice the libraries that come supplied (not the vault) are in a compiled format. Don't know if that has something to do with it.

     

    As far as I know you make a new schematic library and place the pins and draw your shapes for the part.

     

    Next you make a PCB library that contains the footprint and a step file (optional I believe) for the part so it looks nice in the 3D view.

    I think the pads have the same number assigned as the pins. So pin 1 in the sch file is pin 1 in the PCB file. You then right click on the sch symbol and assign the PCB footprints.

     

    Sounds easy I think that's it but I am have a lot of problems making it work.

     

    Geoff.

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 9 years ago in reply to e14 Contributor

    Delete trailing space from the symbol reference.

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 9 years ago in reply to e14 Contributor

    Delete trailing space from the symbol reference.