Altium CircuitStudio
  • Products & Partners
  • Manufacturers
  • Altium CircuitStudio
  • More
  • Cancel
Altium CircuitStudio
Altium CircuitStudio Forum How to change the default settings for vias?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Altium CircuitStudio to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Locked Locked
  • Replies 8 replies
  • Answers 1 answer
  • Subscribers 90 subscribers
  • Views 4165 views
  • Users 0 members are here
  • default
  • vias
  • settings
  • circuit studio
Related
This discussion has been locked.
You can no longer post new replies to this discussion. If you have a question you can start a new discussion

How to change the default settings for vias?

batuu
batuu over 10 years ago

Following the online documentation there are two possibilities to place vias.

 

1.) Press * key or Shift+Ctrl+Mouse wheel in interactive routing mode. You can choose the favorite via size in the Favorite Interactive Via Sizes dialog pressing Shift+V while routing.

2.) Press V to place a via when not routing. As the documentation says, a default via will be placed.

 

How do I change the default via settings? When nailing vias into polygons and planes, I am not in interactive routing mode and I do not want to change the settings for every via pressing the TAB key. I also do not want to select all vias with a filter and change the settings afterwards.

 

Oliver

  • Cancel
Parents
  • _aw
    0 _aw over 7 years ago

    Just FYI, I find this annoying.  Along with the inability to turn off the soldermask using this method.  If I change the setting: SOLDERMASKEXPANSIONMODE=Rule to SOLDERMASKEXPANSIONMODE=None, CS just sets it right back to Rule.  There is no way to setup tenting by default.  If I try to copy and paste a via, it does not keep the Net that the copied via was attached to, and requires manually editing the net.

     

    So glad to see that "The development team at Altium is highly committed addressing problems like this as quickly as possible."  Here we are in 2019, v1.5.2, and this simple problem is not fixed?

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
Reply
  • _aw
    0 _aw over 7 years ago

    Just FYI, I find this annoying.  Along with the inability to turn off the soldermask using this method.  If I change the setting: SOLDERMASKEXPANSIONMODE=Rule to SOLDERMASKEXPANSIONMODE=None, CS just sets it right back to Rule.  There is no way to setup tenting by default.  If I try to copy and paste a via, it does not keep the Net that the copied via was attached to, and requires manually editing the net.

     

    So glad to see that "The development team at Altium is highly committed addressing problems like this as quickly as possible."  Here we are in 2019, v1.5.2, and this simple problem is not fixed?

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
Children
  • e14softwareuk
    0 e14softwareuk over 7 years ago in reply to _aw

    The tenting property does seem to persist. If the tick boxes for "Force complete tenting on top/bottom" are checked these parameters copy and paste. Also when placing a via hit TAB to check the property of these check boxes and then any subsequent vias should maintain the same selection. The net assignment is lost during copy/paste but the TAB property change does work - set the net for the first via and then subsequent ones placed will keep the same net. If you have vias without nets then you don't need to change the net on each one individually - use the object inspector to change all selected vias.

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • _aw
    0 _aw over 7 years ago in reply to e14softwareuk

    That IS helpful Peter.  Thank you.  Hitting TAB before placing vias allows me to set it just the way I need it for all subsequently placed vias.  I just wish the user interface let you know about these secrets before you get frustrated trying to find solutions.  I guess if I would have read the F1 help page carefully, I might have realized that I could do this.