Altium CircuitStudio
  • Products & Partners
  • Manufacturers
  • Altium CircuitStudio
  • More
  • Cancel
Altium CircuitStudio
Altium CircuitStudio Forum Via to pad clearance design rule
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Altium CircuitStudio to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Locked Locked
  • Replies 6 replies
  • Subscribers 91 subscribers
  • Views 6803 views
  • Users 0 members are here
Related
This discussion has been locked.
You can no longer post new replies to this discussion. If you have a question you can start a new discussion

Via to pad clearance design rule

jallard
jallard over 9 years ago

Placing a via over the top of a SMT pad with the same net does not create a design rule error. Is there a way to add a rule prohibiting this?

 

I tried creating a clearance rule for "same net only" with all the clearance matrix values set to zero except Via-to-SMD Pad and Via-to-TH Pad. Unfortunately, this generates a Via-to-track clearance violation on all vias. I'm assuming zero is not sufficient to disable the matrix connection (e.g., setting Via-to-Track == 0, doesn't disable this clearance check).

 

Seems like there should be a way to prevent vias over the top of SMD pads. Am I missing something?

  • Cancel

Top Replies

  • adamwebber
    adamwebber over 9 years ago +2 verified
    So I've never had an issue with this but suddenly I am questioning all of my previous work. I have used Altium extensively and it is so easy to create simple rules to avoid placing vias on pads. CircuitStudio…
  • jallard
    jallard over 9 years ago in reply to adamwebber +1
    Wonderful! Thank you. -1 in the Minimum clearance. Seems like something that should be documented. :-) This works great, which leads to another issue. Some pads and fills require vias in the middle of…
  • songshome
    songshome over 9 years ago in reply to jallard +1
    Firstly, thank you James Clark for -1. To Jim, you can try this: make rule for netclass, then export it and change netclass to padclass with text editor and then import rule. I did not try it, but it should…
Parents
  • adamwebber
    0 adamwebber over 9 years ago

    Here's an update.  I closed CS and reopened the program.  It no longer shows the visible error of the via on the pad.  It does show the error in the DRC, though.  Always make sure to run the Design Rule Check.

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • jallard
    0 jallard over 9 years ago in reply to adamwebber

    Yes, I found the same thing. It does show the visible error once the DRC is run.

     

    Another way to get it to show without running the DRC is make a small change in the Design rules (e.g., change a comment in one of the rules) and hit "Apply." This is faster than running to whole DRC process.

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
Reply
  • jallard
    0 jallard over 9 years ago in reply to adamwebber

    Yes, I found the same thing. It does show the visible error once the DRC is run.

     

    Another way to get it to show without running the DRC is make a small change in the Design rules (e.g., change a comment in one of the rules) and hit "Apply." This is faster than running to whole DRC process.