Altium CircuitStudio
  • Products & Partners
  • Manufacturers
  • Altium CircuitStudio
  • More
  • Cancel
Altium CircuitStudio
Altium CircuitStudio Forum CS doesn't start anymore
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Altium CircuitStudio to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Locked Locked
  • Replies 3 replies
  • Subscribers 88 subscribers
  • Views 711 views
  • Users 0 members are here
Related
This discussion has been locked.
You can no longer post new replies to this discussion. If you have a question you can start a new discussion

CS doesn't start anymore

medvedev
medvedev over 9 years ago

Hello,

since yesterday CircuitStudio doesn't start anymore.

The day before yesterday everything was fine. I didn't change anything in the settings of CS nor in the settings of my Win10 x64.

Now I have updated it to the current version 1.4 (was 1.3 before) and it didn't change anything.

When I start CS nothing happen; the Task Manager shows that the dxp.exe is running with 15% of CPU usage and constant 100MB RAM usage.

What else  can I do?

 

Thanks!

  • Cancel
  • e14softwareuk
    0 e14softwareuk over 9 years ago

    Hi Sergej, I'm not clear if you are saying when you updated to 1.4 it suddenly stopped working or it stopped working with 1.3 and updating to 1.4 still didn't work?

     

    Windows 10 has a habit of applying software updated whenever it feels like so that may be cause of the issue. Can you roll back the last updates the Win 10 installed to see if that helps.

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • medvedev
    0 medvedev over 9 years ago in reply to e14softwareuk

    The problem existed before and after update. I have now uninstalled CS and installed it again. Now it works but my last Project is corrupted! Completly gone! I have 10y of EDA experience and have never seen that before!

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • e14softwareuk
    0 e14softwareuk over 9 years ago in reply to medvedev

    Thanks for the update and sorry to hear your project was corrupted, it may be possible to recover. Is the folder that contained your project still present? If so then you may be able to run CS and use the local history to recover a prior version of you design. To manually get at the previous versions open the folder in file explorer and look for the History sub-folder. This should contain many *.Zip files that represent older versions of design documents which you should be able to use to recover your design from.