Altium CircuitStudio
  • Products & Partners
  • Manufacturers
  • Altium CircuitStudio
  • More
  • Cancel
Altium CircuitStudio
Altium CircuitStudio Forum Several issues to help with
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Altium CircuitStudio to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Locked Locked
  • Replies 0 replies
  • Subscribers 88 subscribers
  • Views 314 views
  • Users 0 members are here
  • library concept
  • output configuration save
Related
This discussion has been locked.
You can no longer post new replies to this discussion. If you have a question you can start a new discussion

Several issues to help with

lupal
lupal over 9 years ago

Hi all,

I've started using CircuitStudio several months ago and still struggle with some details:

 

  1. I didn't like the concept of libraries in Eagle where you have to have a whole component with all details for everything I would personally prefer placing for example NPN transistor to the schematic and assign it a package(TO92 when I need to If needed I can assign the name BC546 or even  BC546ATABC546ATA But not in the beginning That's what I expected I am just wandering what is the advantage of choosing the exact component in the beginning If I should use this approach I expect complete libraries For example there are only some tantalum capacitors values
  2. Continuation from question 1. Let's consider placing a resistor. I do not know the value in the beginning and I expect the resistors to be the same but their value. So I created a library with resistors and kept the Value field modifiable. I set the value in schematic. This looks to do the job but BOM does not work the expected way. The components are expected the same, so they are in the same line etc. I solved this by copying the value to comment automatically. The only problem now is that if I make a modification of the component in the library and update the schematic. The Value is changed to its default and I loose a lot of time changing it over again. Is there a better way to deal with this?
  3. One reason for creating the own components was EU resistor symbol. I didn't find any such resistor in the vault. So it seams like thousands of resistors are useless. Is there any way how to use the components with a symbol according to other standard? Or modify the library in a batch?
  4. I run the DRC check and open the verification report. There are many errors. I click one of them. The PCB centers somehow but there is no specific pointing to the problem so I can't identify it from what I see. I have to go back to the report, find the coordinates and point the cursor to these coordinates on PCB so I see where the problem occured. This consumes a lot of time. How can I deal with it?
  5. I spent some time modifying the Print preview and Generate output file configuration. It is saved automatically in system. Can I store it somehow in a file so I can use it in a different installation again etc.?

 

Please advice if you have an answer or opinion.

Thank you very much.

 

Lukas