Altium CircuitStudio
  • Products & Partners
  • Manufacturers
  • Altium CircuitStudio
  • More
  • Cancel
Altium CircuitStudio
Altium CircuitStudio Forum Schematic design workflow hints please?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Altium CircuitStudio to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Locked Locked
  • Replies 6 replies
  • Answers 3 answers
  • Subscribers 91 subscribers
  • Views 1502 views
  • Users 0 members are here
  • variants
  • schematics
  • footprints
Related
This discussion has been locked.
You can no longer post new replies to this discussion. If you have a question you can start a new discussion

Schematic design workflow hints please?

gwideman
gwideman over 8 years ago

Hi folks. I'm looking for some hints on how to use CircuitStudio to develop schematics without having to commit to very specific components prematurely.

 

I often want to design the approximate schematic first, for example including resistors and capacitors whose values I haven't calculated yet, and certainly haven't decided on a package/footprint, let alone a supplier.  All the tutorials I've seen so far place very specific components immediately, which is not what I want.

 

So I guess this amounts to the following questions about a workflow for this iterative process:

 

1. How do I place a generic component, be it a passive whose value I don't yet know, or an IC whose package I haven't decided.

2. How do I later set the value of the generic component.

3. How do I later still set the package, and then specific part number?

4. Even later, how do I change any of the above?

 

Thanks. Graham

  • Cancel

Top Replies

  • e14softwareuk
    e14softwareuk over 8 years ago +2 suggested
    I'll chip in with a suggestion, please feel free to join in this discussion as it's an excellent topic. Taking a resister as an example. It is possible to just place on a schematic and use the same symbol…
  • e14softwareuk
    e14softwareuk over 8 years ago in reply to gwideman +2 suggested
    There are no generic components with lots of footprints attached as standard, you would need to build your own library. However you don't need to start from scratch as you can make use of existing symbols…
  • batuu
    batuu over 8 years ago in reply to gwideman +2 suggested
    Hi Graham, you said that you do not prefer to use dummy components and replace them with the real ones later, but I highly recommand this approach. When I delete a component, the wires stay in schematic…
Parents
  • e14softwareuk
    0 e14softwareuk over 8 years ago

    I'll chip in with a suggestion, please feel free to join in this discussion as it's an excellent topic.

     

    Taking a resister as an example. It is possible to just place on a schematic and use the same symbol for every resistor instance. Later on you can assign values to each instance. The library part may contain multiple footprints and you can tailor each resistor on your design once you have decided on the package type required. The ECO process will keep the PCB up to date with the footprint changes. Symbols support extra parameters (name value pairs) so you can make use of these if you wish to specify manufacturer, supplier, part codes etc.

     

    Another option would be to place generic components and then later in the design process delete and replace with the specific one required. There is a lot of flexibility, once you understand the possibilities you should be able to design your own workflow that works for you.

    • Cancel
    • Vote Up +2 Vote Down
    • Cancel
  • gwideman
    0 gwideman over 8 years ago in reply to e14softwareuk

    Hi Peter, thanks again for your answers -- I seem to be keeping you busy this past day or so :-).

     

    I do not like at all the idea of having to delete and replace components. That requires breaking the connections and rewiring, which strikes me as very error prone.

     

    However, the generic resistor (capacitor, LED, etc) whose value can be set as a parameter, and which has multiple footprints from which to later choose -- that sounds good. Where do I find such components?

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • e14softwareuk
    0 e14softwareuk over 8 years ago in reply to gwideman

    There are no generic components with lots of footprints attached as standard, you would need to build your own library. However you don't need to start from scratch as you can make use of existing symbols and footprints (beware of attempting to copy symbols from the Online Vault as they tend to default back to their original state if copied and edited locally).

    • Cancel
    • Vote Up +2 Vote Down
    • Cancel
Reply
  • e14softwareuk
    0 e14softwareuk over 8 years ago in reply to gwideman

    There are no generic components with lots of footprints attached as standard, you would need to build your own library. However you don't need to start from scratch as you can make use of existing symbols and footprints (beware of attempting to copy symbols from the Online Vault as they tend to default back to their original state if copied and edited locally).