Altium CircuitStudio
  • Products & Partners
  • Manufacturers
  • Altium CircuitStudio
  • More
  • Cancel
Altium CircuitStudio
Altium CircuitStudio Forum Arcs As Traces = Consistent Crashes in Layout, STEP Output...
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Altium CircuitStudio to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Locked Locked
  • Replies 3 replies
  • Subscribers 89 subscribers
  • Views 1060 views
  • Users 0 members are here
Related
This discussion has been locked.
You can no longer post new replies to this discussion. If you have a question you can start a new discussion

Arcs As Traces = Consistent Crashes in Layout, STEP Output...

erix
erix over 8 years ago

I design a lot of round boards and the CS routing tool does not make for attractive or functional layouts with only straight traces in one of eight directions (0, 45, 90, 135, 180, 225, 270, 315 degrees). I have had success drawing arcs on the copper layers and using them for traces but MANY times the software will crash when I try to connect a trace drawn with the route tool to one of these arcs. I've gotten to the point that I have to save the file after every new trace is added so I don't lose too much work. It's a pain but it works. I have had the same issue in AD 14 and 15 as well.

 

When the software crashes it throws up an exception (or access violation) in the ADVPCB.DLL, generates a report, does a screen cap, and then sends it off to Altium to go into the pile.

 

Today I learned another way arcs-as-traces crash the software - STEP export. I never had this trouble with this particular function in AD and I'm wondering if the design file is somehow corrupt as it used to export before I added the arcs-as-traces.

 

SO! Has anyone else experienced this behavior? Want to try to reproduce it?

  • Cancel
Parents
  • bugrobotics
    0 bugrobotics over 8 years ago

    Ill try and reproduce

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
Reply
  • bugrobotics
    0 bugrobotics over 8 years ago

    Ill try and reproduce