Altium CircuitStudio
  • Products & Partners
  • Manufacturers
  • Altium CircuitStudio
  • More
  • Cancel
Altium CircuitStudio
Altium CircuitStudio Forum Arcs As Traces = Consistent Crashes in Layout, STEP Output...
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Altium CircuitStudio to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Locked Locked
  • Replies 3 replies
  • Subscribers 89 subscribers
  • Views 1059 views
  • Users 0 members are here
Related
This discussion has been locked.
You can no longer post new replies to this discussion. If you have a question you can start a new discussion

Arcs As Traces = Consistent Crashes in Layout, STEP Output...

erix
erix over 8 years ago

I design a lot of round boards and the CS routing tool does not make for attractive or functional layouts with only straight traces in one of eight directions (0, 45, 90, 135, 180, 225, 270, 315 degrees). I have had success drawing arcs on the copper layers and using them for traces but MANY times the software will crash when I try to connect a trace drawn with the route tool to one of these arcs. I've gotten to the point that I have to save the file after every new trace is added so I don't lose too much work. It's a pain but it works. I have had the same issue in AD 14 and 15 as well.

 

When the software crashes it throws up an exception (or access violation) in the ADVPCB.DLL, generates a report, does a screen cap, and then sends it off to Altium to go into the pile.

 

Today I learned another way arcs-as-traces crash the software - STEP export. I never had this trouble with this particular function in AD and I'm wondering if the design file is somehow corrupt as it used to export before I added the arcs-as-traces.

 

SO! Has anyone else experienced this behavior? Want to try to reproduce it?

  • Cancel
Parents
  • e14softwareuk
    0 e14softwareuk over 8 years ago

    You should be able to add in arcs to any trace you are routing by using SHIFT+SPACE to toggle corner styles until you get to arc drawing, also hit SHIFT+F1 during routing to see the other shortcuts you can use (e.g. adjusting arc radius).

     

    Regarding STEP export crashing, I have come across this and one solution seemed to be make sure the ends of the arc actually tie up with the other line segments correctly. Try zooming right in, moving the arc a little and adding a line that snaps to end of arc and other nearby line segment.

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • erix
    0 erix over 8 years ago in reply to e14softwareuk

    Thanks Peter! I had never seen that SHIFT+F1 menu before!

     

    I did as you suggested and drew a radius with the trace tool. When I double click the radius the dialog box that comes up is the same one as you get when you draw an arc - which leads me to believe it is the same type of entity? I'll give it a go on my next board and see if it stops the crashing.

     

    I changed all my outlines to 1 mil width and found a few disconnects. I connected them and the STEP output went without flaw. THANKS!

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
Reply
  • erix
    0 erix over 8 years ago in reply to e14softwareuk

    Thanks Peter! I had never seen that SHIFT+F1 menu before!

     

    I did as you suggested and drew a radius with the trace tool. When I double click the radius the dialog box that comes up is the same one as you get when you draw an arc - which leads me to believe it is the same type of entity? I'll give it a go on my next board and see if it stops the crashing.

     

    I changed all my outlines to 1 mil width and found a few disconnects. I connected them and the STEP output went without flaw. THANKS!