Altium CircuitStudio
  • Products & Partners
  • Manufacturers
  • Altium CircuitStudio
  • More
  • Cancel
Altium CircuitStudio
Altium CircuitStudio Forum Best way to duplicate / clone a project?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Altium CircuitStudio to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Locked Locked
  • Replies 1 reply
  • Answers 1 answer
  • Subscribers 88 subscribers
  • Views 7165 views
  • Users 0 members are here
  • clone
  • duplicate project
Related
This discussion has been locked.
You can no longer post new replies to this discussion. If you have a question you can start a new discussion

Best way to duplicate / clone a project?

lamabrew
lamabrew over 8 years ago

Project Save As...  seems to only make a copy of the .PrPcb file and it still points back to the original schematic and layout files. I would like to make a full copy of all files in the project, change all of the file names with a suffix to match the new project's name, and then treat that as a project not related to thing it was copied from.

 

I've tried a couple of variations, but so far this seems like the simplest way:

 

  1. copy the directory in windows
  2. from windows rename the .PrPcb , topmost schematic sheet, and layout files.
  3. open the project and do Add Existing to project... for the renamed files
  4. Use Rename Child Sheet on each sheet symbol for the remaining schematic files
  5. (Hit project compile each time a rename is done to get things in the hierarchy)

 

When you create a New Project there's an option to select a Project Template but I didn't find an explanation about how to create them and/or if the template can actually be a complete project vs. a collection of schematic and layout templates.

 

Is there a better way to do this?

 

------

Added after original post:

I do not copy the History, Previews, Logs, or Output directories.

I'm not sure about the .Harness files yet. It seems to automatically generate new ones but I have not experimented to see if it needs to have the old ones to do that. (In general the workings of Harnesses are still a mystery to me so don't take anything I say about it as useful).

 

Despite the above seemingly working I now do have a case where it seems like PCB is confused about component classes. I will open a separate thread on that once I understand it.

  • Cancel
  • e14softwareuk
    0 e14softwareuk over 8 years ago

    I think you are most likely doing it the best way by copying the directory in Windows, you are correct in Save As only renames the project file and doesn't create a full copy. The *.outjob file may be an issue, even though you can rename it the content may not adjust correctly so keep and eye on this.