Altium CircuitStudio
  • Products & Partners
  • Manufacturers
  • Altium CircuitStudio
  • More
  • Cancel
Altium CircuitStudio
Altium CircuitStudio Forum Second source/"Solution 1" for components in circuitstudio without using supplier links
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Altium CircuitStudio to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Locked Locked
  • Replies 3 replies
  • Subscribers 89 subscribers
  • Views 753 views
  • Users 0 members are here
  • circuitstudio
Related
This discussion has been locked.
You can no longer post new replies to this discussion. If you have a question you can start a new discussion

Second source/"Solution 1" for components in circuitstudio without using supplier links

doov123
doov123 over 8 years ago

I have been using the supplier links for several components in a circuitstudio design.  One nice aspect of doing this is that when I export my BOM several pieces of critical information are filled in if I enable the "solution 1" checkbox as seen in the attachment (e.g. MPN)

 

I have other components and or second sources for components that are not available through the select distributors that CircuitStudio has partnered with.


How do I import the same data structure for these components?  E.g. how do I manually add "solution 1" to a component without using supplier links and or how do I add "solution 2" to a component also without using supplier links?

One interesting thing to note is that when I edit the component properties in the schematic library editor I do not see all the subfields (e.g. MPN) shown in the "solution 1" fields.

Attachments:
image
  • Cancel
  • e14softwareuk
    0 e14softwareuk over 8 years ago

    You can manually add any number of parameters with names of your choosing to components and optionally have them display on the schematic. The BOM configuration dialog allows you to display any parameter in the report.

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • doov123
    0 doov123 over 8 years ago in reply to e14softwareuk

    Right, but that's not quite the same thing (so far as I can tell) -- I'd like to create the equivalent data structure such that these those parameters are subcategories of solution 1.  Is there a way to manually add sub parameters?

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • e14softwareuk
    0 e14softwareuk over 8 years ago in reply to doov123

    Sorry but I don't know of any way to add sub-parameters to solution 1.