Altium CircuitStudio
  • Products & Partners
  • Manufacturers
  • Altium CircuitStudio
  • More
  • Cancel
Altium CircuitStudio
Altium CircuitStudio Forum Why can't I add this pin or pad to this net?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Altium CircuitStudio to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Locked Locked
  • Replies 2 replies
  • Subscribers 89 subscribers
  • Views 1629 views
  • Users 0 members are here
  • troubleshooting
  • pad
  • pin
  • net
  • circuitstudio
Related
This discussion has been locked.
You can no longer post new replies to this discussion. If you have a question you can start a new discussion

Why can't I add this pin or pad to this net?

jaza_tom
jaza_tom over 8 years ago

I have a component:  an ATmega328PB microcontroller.  It has 32 pins, plus a back pad (33rd pin).  My footprint has 33 pads (extra pad for back pad (thermal)).  My schematic symbol also has 33 pins, mapped to the corresponding pads (1 thru 33).

 

For some reason, if I connect pin 33 to a net in the schematic, that connection does not get translated to the PCB.  If I select the pad in the PCB editor and open it's properties dialogue, I can manually assign a net to that pad, which is a workaround I suppose.  If I subsequently connect a different net to this pad, the same behaviour persists (i.e. if I manually set that pad to be connected to GND and then in the schematic I connect +5V to pin 33, if I go to import that change into the PCB file, CircuitStudio says that there are no changes to import.  image

 

See video to see what I mean (below).

 

e14softwareuk  -->  what could be the cause of such strange behaviour?

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

  • Cancel
  • voltsandjolts
    0 voltsandjolts over 8 years ago

    If you can't share your design files, could you create a minimal CS Project with this part and issue for us to have a poke at?

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • e14softwareuk
    0 e14softwareuk over 8 years ago

    Hi Tom. Thanks for the video - a little fuzzy but looks like you are doing the right thing. It would help if you could send through the design or create a sample design with just the one component and some power/ground that exhibits this same issue.