Altium CircuitStudio
  • Products & Partners
  • Manufacturers
  • Altium CircuitStudio
  • More
  • Cancel
Altium CircuitStudio
Altium CircuitStudio Forum Can't subscribe for library destroy notify
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Altium CircuitStudio to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Locked Locked
  • Replies 3 replies
  • Subscribers 90 subscribers
  • Views 824 views
  • Users 0 members are here
Related
This discussion has been locked.
You can no longer post new replies to this discussion. If you have a question you can start a new discussion

Can't subscribe for library destroy notify

jgerber
jgerber over 7 years ago

While working in CircuitStudio, I frequently get this error when trying to place a part from a schematic library - when this happens, the library appears as blank, until i open another and then switch back. Has anyone else had this problem? I know it's one of very many bugs in CS, but it's getting to be one of the more annoying ones:

 

"Can't subscribe for library destroy notify because allready subscribed" (sp)

Attachments:
image
image
  • Cancel
  • e14softwareuk
    0 e14softwareuk over 7 years ago

    We have had this error reported before but extremely rare so we don't have a definitive solution to offer. To help narrow down does this occur with just one library or across all libraries; for one project or across all projects. Is there a known way to trigger the error so help others reproduce. I use CS 1.5.1 on Win 7 and do not see this. Maybe there is some unwanted interactions from a anti-virus package or similar that is causing issues.

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • jgerber
    0 jgerber over 7 years ago in reply to e14softwareuk

    It isn't predictable, but occurs frequently. I have 23 different schematic libraries installed - I first tried them as Project libraries but that doesn't work well, so have put them as Installed. It's worth noting that I have used Altium recently on a different machine and find that Circuitstudio appears a lot slower, especially when loading, with very variable startup delays, so perhaps there is something going on.

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • frog
    0 frog over 7 years ago

    I've seen this from time to time, will keep an eye out in case I can quantify the conditions under which is happens.