Altium CircuitStudio
  • Products & Partners
  • Manufacturers
  • Altium CircuitStudio
  • More
  • Cancel
Altium CircuitStudio
Altium CircuitStudio Forum Courtyard vs Outline for DRC and let's finally decide what should be Courtyard?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Altium CircuitStudio to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Locked Locked
  • Replies 0 replies
  • Subscribers 88 subscribers
  • Views 695 views
  • Users 0 members are here
  • pads editing
  • pads
  • footprint
  • pcb library
  • outline
  • courtyard
Related
This discussion has been locked.
You can no longer post new replies to this discussion. If you have a question you can start a new discussion

Courtyard vs Outline for DRC and let's finally decide what should be Courtyard?

olemi
olemi over 7 years ago

1) OK, say we follow IPC-7351 and use 0.40mm maximum for spacing between components.

 

First, spacing between bodies+pins or bodies+pads? We know it's for pick&place on PCBA, so the core of the rule is to allow spacing between components. The component consist of body and legs (if have).

 

Example 1. Say we place two QFN in front of each other. No problems, 0.4mm is obviously between bodies.

 

Example 2: We have two sop8 or any other with legs. Why standard libs of CS offer courtyard around body+pins+pads+space instead of just body+pins? See attached.

 

2) Courtyard vs Outline

 

In previous CADs I had only Outline and used it as seems Courtyard suppose to be used here. Does it really make sense to have Outline if Courtyard is used? Will they work the same on DRC?

 

3) About DRC and Courtyard

 

Above we agreed on  0.4mm between components. So, should I draw 0.2mm for a single footprint to pass DRC or CS is smart enough to recognize that if I use 0.4mm for a single component and place them on 0.5mm distance (which obviously cause crossing of courtyards) I don't violate the rule and will pass DRC?

Attachments: