Altium CircuitStudio
  • Products & Partners
  • Manufacturers
  • Altium CircuitStudio
  • More
  • Cancel
Altium CircuitStudio
Altium CircuitStudio Forum Clicking on a component in PCB layout able to focus schematic to that component?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Altium CircuitStudio to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Locked Locked
  • Replies 10 replies
  • Subscribers 90 subscribers
  • Views 3955 views
  • Users 0 members are here
Related
This discussion has been locked.
You can no longer post new replies to this discussion. If you have a question you can start a new discussion

Clicking on a component in PCB layout able to focus schematic to that component?

_aw
_aw over 7 years ago

I would like to click on a component in the PCB layout and have it focus the schematic document to that component.  Can CircuitStudio be setup to do this?  I am in multi-window mode with my PCB in one window, and my schematic sheets in the other window.

  • Cancel
  • _aw
    0 _aw over 7 years ago

    I realized that I should clarify...  Cross-Probe under the Tools menu does what I want, but I was hoping for more of a "Live" option that would do the focusing as I am selecting and moving components in the PCB.

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • e14softwareuk
    0 e14softwareuk over 7 years ago in reply to _aw

    If you already have the schematics open it should highlight the schematic symbol as you click on the PCB component. Unlike full cross probing new sheets will not be opened so you do need them to be visible first. Don't forget that CS supports multiple monitors and split views so many schematic sheets can be viewed at once.

     

    To get the above working you may need to change the Cross Select Zoom Option from File > System Preferences.

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • _aw
    0 _aw over 7 years ago in reply to e14softwareuk

    Thanks for the reply... mine does not seem to do what you are proposing.  Does it have to be in the same window?  I have my PCB in a window on my left screen, and my schematic sheets in a separate window on my right screen.  I have four sheets, so I have split my right screen so I can see all four sheets.  In normal operation, clicking in the PCB is not affecting anything in the schematics.

     

    The preferences for "Zoom Precision" say it is for when you "use the zoom navigation method".  I don't know if it is in that method normally, or if I have to do something to put it in that method?

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • e14softwareuk
    0 e14softwareuk over 7 years ago in reply to _aw

    Sounds very similar to how I tested - the schematics needed to be opened and visible because they would not be automatically opened. Try a cross probe first from the PCB and then cancel and go to selecting a PCB component - I saw CS highlight (surround with a selection box) the schematic symbol.

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • _aw
    0 _aw over 7 years ago in reply to e14softwareuk

    It works the opposite direction.  If I click in the schematic, it zooms and highlights in the PCB.  Cross-probe works both directions.  Seems like I must be missing a setting somewhere.

     

    Just FYI, I restarted CS and it did not change how it is working.

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • e14softwareuk
    0 e14softwareuk over 7 years ago in reply to _aw

    Not sure what setting would be needed. One thing to try is compiling the schematic after opening.

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • _aw
    0 _aw over 7 years ago in reply to e14softwareuk

    I have tried that to no avail.  Thanks for your replies.  It would be nice to know the difference between my setup and yours...  I have the latest CS version.

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • e14softwareuk
    0 e14softwareuk over 7 years ago in reply to _aw

    I'm using latest version and do have a dual monitor setup but works with just a split window display on one monitor. I've had a look through but cannot see any other setting that might be relevant other than the one already mentioned (zoom navigation).

     

    Interestingly mine only works from PCB to Schematic whereas you said it worked both directions. If I use the cross probe command it will do both but only PCB to Schematic otherwise.

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • _aw
    0 _aw over 7 years ago in reply to e14softwareuk

    Thanks again for your effort.  I can move on for now and live without it.  Seems like a bug though, that yours works only one direction (PCB -> Schematic) and mine only works the opposite direction (Schematic -> PCB).

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • Squintz
    0 Squintz over 4 years ago

    https://documentation.circuitstudio.com/display/CSTU/PCB_Cmd-CrossProbeChoose_Composite((Cross-Probe+&+Cross-Select+Tools))_CS

    See the Cross Selection section of that help doc. It says that you need to enable Cross Select mode from Home->Select->Cross Select Mode in BOTH documents for it to work.

    Also, it seems to only work when the component are on the board. If they are off to the side of the board it doesn't seem to work for me sometimes. It's super finicky. I once had it working where I would click on the PCB and no matter what page the part was on it would zoom to it. Now I must have the page the part is on active for it to find it on that page with is a lot less useful.