Altium CircuitStudio
  • Products & Partners
  • Manufacturers
  • Altium CircuitStudio
  • More
  • Cancel
Altium CircuitStudio
Altium CircuitStudio Forum Keep-Out and Mechanical 4 handling for fabrication
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Altium CircuitStudio to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Locked Locked
  • Replies 3 replies
  • Subscribers 90 subscribers
  • Views 1586 views
  • Users 0 members are here
Related
This discussion has been locked.
You can no longer post new replies to this discussion. If you have a question you can start a new discussion

Keep-Out and Mechanical 4 handling for fabrication

tyro01
tyro01 over 7 years ago

Hi,

 

I designed 2 Layer PCB and am using a Keep-Out Layer for mask from both-side copper pour. Of course, PCB outline is determined on CircuitStudio.

FusionPCB recommend to output GKO as PCB outline. Another factories recommend to output GM4.

 

However when I checked at gerber viewer, GKO includes mask shape without PCB outline.

Should I add line manually along to PCB outline at Keep-Out(or Mechanical 4)? Or, CircuitStudio generates PCB outline data automatically to other file?

 

tyro

  • Cancel
Parents
  • tchristie
    0 tchristie over 7 years ago

    @e14softwareuk

    Just one additional note: While using Create Primitives From Board Shape, the "Outline" layer is not one of the choices in the dropdown. It is called "Mechanical 1". This is rather confusing until you realize from Gerber Files Configure...  that "Outline" is the file extension and not the name of the layer. But on the bottom of PCB editor, "Outline" is the layer name.  So this is just another example of simple GUI mistake. Personally I would like it called "Outline" layer and file extension everywhere.

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
Reply
  • tchristie
    0 tchristie over 7 years ago

    @e14softwareuk

    Just one additional note: While using Create Primitives From Board Shape, the "Outline" layer is not one of the choices in the dropdown. It is called "Mechanical 1". This is rather confusing until you realize from Gerber Files Configure...  that "Outline" is the file extension and not the name of the layer. But on the bottom of PCB editor, "Outline" is the layer name.  So this is just another example of simple GUI mistake. Personally I would like it called "Outline" layer and file extension everywhere.