Altium CircuitStudio
  • Products & Partners
  • Manufacturers
  • Altium CircuitStudio
  • More
  • Cancel
Altium CircuitStudio
Altium CircuitStudio Forum "Object reference not set...." in vault explorer
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Altium CircuitStudio to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Locked Locked
  • Replies 71 replies
  • Answers 16 answers
  • Subscribers 97 subscribers
  • Views 14910 views
  • Users 0 members are here
Related
This discussion has been locked.
You can no longer post new replies to this discussion. If you have a question you can start a new discussion

"Object reference not set...." in vault explorer

mjschurman
mjschurman over 7 years ago

When searching for parts in the vault explorer I am receiving the following result:

 

"Object reference not set to an instance of an object"

 

I am using Circuit Studio 1.5.2

  • Cancel

Top Replies

  • e14softwareuk
    e14softwareuk over 7 years ago in reply to alienjack +1 suggested
    Just to confirm a request is open with Altium to investigate.
  • dmcfatter
    dmcfatter over 7 years ago in reply to e14softwareuk +1 suggested
    I was able to get it work in the search tab only after setting the view to "Search Results View". To get this menu to show up I had manually pull up a part out of a folder on the other tab.
  • sshaferdlm
    sshaferdlm over 7 years ago in reply to e14softwareuk +1
    Hi Peter, "Are we there yet?" Any information would be helpful. Best Regards, Steve
Parents
  • markvanber
    0 markvanber over 4 years ago

    An Object is an instance of a Class , it is stored some where in memory. A reference is what is used to describe the pointer to the memory location where the Object resides. The message "object reference not set to an instance of an object" means that you are referring to an object the does not exist or was deleted or cleaned up. It's usually better to avoid a NullReferenceException than to handle it after it occurs. To prevent the error, objects that could be null should be tested before being used.

    if (mClass != null)
    {
    // Go ahead and use mClass
    mClass.property = ...
    }
    else
    {
    // Attempting to use mClass here will result in NullReferenceException
    }
    
    

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • shabaz
    0 shabaz over 4 years ago in reply to markvanber

    That type of error can have a million and one root causes, without knowing the code detail any further : (
    For instance it's very commonly seen in occasions where either the local system, or remote system, is either bottlenecked, or behaving in a bursty manner, or messages are unexpectedly not being received or sent, or the software is running much faster or much slower than usual.

    In these cases, objects may be deleted at the wrong time, or accessed when it's no longer appropriate, due to multiple state machines (say local and remote, or ingress and egress or anything else) being in unexpected combination of states with respect to each other. For sure it should be coded better to continue operations or handle reattempts or better error handling and reporting, but the reason these errors are often seen is simply because race conditions are unexpected, and often some development teams won't test that as well as they could, since it often entails deliberately introducing delays or load just to simulate possible conditions users may experience with (say) slower or faster computers, or slower or faster communication paths, or broken network connections, missing or moved URLs and so on.

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
Reply
  • shabaz
    0 shabaz over 4 years ago in reply to markvanber

    That type of error can have a million and one root causes, without knowing the code detail any further : (
    For instance it's very commonly seen in occasions where either the local system, or remote system, is either bottlenecked, or behaving in a bursty manner, or messages are unexpectedly not being received or sent, or the software is running much faster or much slower than usual.

    In these cases, objects may be deleted at the wrong time, or accessed when it's no longer appropriate, due to multiple state machines (say local and remote, or ingress and egress or anything else) being in unexpected combination of states with respect to each other. For sure it should be coded better to continue operations or handle reattempts or better error handling and reporting, but the reason these errors are often seen is simply because race conditions are unexpected, and often some development teams won't test that as well as they could, since it often entails deliberately introducing delays or load just to simulate possible conditions users may experience with (say) slower or faster computers, or slower or faster communication paths, or broken network connections, missing or moved URLs and so on.