Altium CircuitStudio
  • Products & Partners
  • Manufacturers
  • Altium CircuitStudio
  • More
  • Cancel
Altium CircuitStudio
Altium CircuitStudio Forum CS Crashes on Library Access
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Altium CircuitStudio to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Locked Locked
  • Replies 13 replies
  • Subscribers 92 subscribers
  • Views 2523 views
  • Users 0 members are here
Related
This discussion has been locked.
You can no longer post new replies to this discussion. If you have a question you can start a new discussion

CS Crashes on Library Access

larry_137
larry_137 over 6 years ago

I cannot get CS to work. If I access a library, it crashes. If I view a 3D image of my circuit card, it crashes. If I try to do a 3D edit a footprint, it crashes. If I run a rules check and try to save the PCB file, it crashes. I just paid my "subscription" fee, but the program is useless.

 

Note that I completely designed a PCB (it is now in production) using the same libraries and CS worked flawlessly (well, good enough). At one point several months later, I went to check something in the design files, and the 3D view no longer worked and the Libraries window showed only a line outline with a clear center section. OK? When I tried to exit CS, all I could do was press the kill switch in Task Manager to get out. Task Manager said that DXP.exe was "unresponsive". No kidding.

 

The PCB was designed under Win7 (and as I said all worked fine) and this lock up happened under the same Win7 (who knows what Microsoft updates do). OK. I tried reloading the program. Crash. Because Win7 expired, I had to update to Win10. Before doing so, I uninstalled CS using Wise Program Uninstall. This kills everything in the program including Registry Keys. I then installed the new operating system (wasn't THAT fun!). With Window 10 on board, most everything seemed OK with minor exceptions. I then loaded CS using all of the defaults, just as the installer wants.  Started CS, and navigated the license activation routine. Great! Good to go. Started CS, and the home page came up. Blank Project Directory on the left, home page in the middle, and thin Library to the right. I checked that the two default integrated libraries were installed. Yes. On the task bar I pressed View and then Libraries. Crash! Could only kill CS using Task Manager. None of my files (which I checked by downloading a 3D viewer and they all looked good) were in use. As an experiment, I loaded CS on my laptop (also Win 10) and did the same sequence. The two integrated libraries came right up, and the footprints showed 3D views on all of the parts.

 

I have tried asking the forum with no results. Anybody have an idea of a way forward?

  • Cancel
Parents
  • larry_137
    0 larry_137 over 6 years ago

    Hi folks, thanks for the response. My gut feel is that it may be the graphics. However, it used to work with the graphics card I have under Windows 7. It stopped working on Windows 7 and I could not get it going. Due to Microsoft, I then updated to Windows 10. Still did not work. I loaded the latest drivers from Nvidia. Still does not work. So yes, a pretty clean installation but with everything up to date. The Video card is Nvidia Quadro K2220 with the latest drivers from Nvidia.

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • spegs21
    0 spegs21 over 6 years ago in reply to larry_137

    I had basically the same problem:

     

    Application Locks Up on PCB Open, Missing Library?

     

    It was resolved with an update to 442.50 Game Ready Driver (RTX 2080). Looks like latest Quadro drivers are the same version.

     

    Do you have integrated graphics you could try to see if it works?

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
Reply
  • spegs21
    0 spegs21 over 6 years ago in reply to larry_137

    I had basically the same problem:

     

    Application Locks Up on PCB Open, Missing Library?

     

    It was resolved with an update to 442.50 Game Ready Driver (RTX 2080). Looks like latest Quadro drivers are the same version.

     

    Do you have integrated graphics you could try to see if it works?