Altium CircuitStudio
  • Products & Partners
  • Manufacturers
  • Altium CircuitStudio
  • More
  • Cancel
Altium CircuitStudio
Altium CircuitStudio Forum Multiple Attributes(?) To Drive BOM Content
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Altium CircuitStudio to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Locked Locked
  • Replies 1 reply
  • Subscribers 88 subscribers
  • Views 458 views
  • Users 0 members are here
Related
This discussion has been locked.
You can no longer post new replies to this discussion. If you have a question you can start a new discussion

Multiple Attributes(?) To Drive BOM Content

crimsonaudio
crimsonaudio over 6 years ago

Is there a way for a single part to drive multiple line items in a BOM? For instance, an SMD with a light pipe would have BOM information in it;s attributes for both the LED and the light pipe. I am currently using a separate schematic symbol for the mechanical part (light pipe) that populates it's line item in the BOM, but I was hoping there might be a way for one part to drive the two line items.

 

Thanks!

Dan

  • Cancel
  • tarribred61
    0 tarribred61 over 6 years ago

    I don't think there is a way to have a single instance generate multiple line items in a BOM.  To do this, I have a single generic schematic library part that has a symbol that is just a text note.

    Here is an example.  I do this for various parts such as the bare PCB itself, adhesives, assy procedures, silpads, heat sinks, fasteners, etc.

    image

     

    The schematic symbol looks like the following:

    image

    This is just a text frame with a note and then the "Apply to...." text is a parameter that I can change.  It would appear on the schematic as a note but it generates a BOM item.  Also, if I include the parameter in the BOM then the text appears there.  The parameter I use for the notes I call "Component Note1" and I put special notes or extra value information there that I want to appear on the BOM.

     

    You will see that I made the Type dropbox be the mechanical type.  Here is a shot of the library part that puts the bare PCB p/n into the BOM.

    image

     

    These end up appearing on the schematic something like this.....

     

    image

    I didn't make the Default Designator visible but if you did you could make ordered numbered notes.  I typically just bunch up the various mechanical only parts like this on a top sheet or with the fiducials or mounting holes or something.