Altium CircuitStudio
  • Products & Partners
  • Manufacturers
  • Altium CircuitStudio
  • More
  • Cancel
Altium CircuitStudio
Altium CircuitStudio Forum How to make a component keepout that allows tracks?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Altium CircuitStudio to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Locked Locked
  • Replies 6 replies
  • Subscribers 90 subscribers
  • Views 2836 views
  • Users 0 members are here
  • clearance rule
Related
This discussion has been locked.
You can no longer post new replies to this discussion. If you have a question you can start a new discussion

How to make a component keepout that allows tracks?

bigbaldjohn
bigbaldjohn over 6 years ago

Hi,

I'm using CS 1.5.2.

I'm designing a PCB for a housing that has support pillars placed all over the PCB and need to be sure I don't place components in these areas. Tracks are OK.

If I put the contact areas onto the keep-out layer I can't put tracks there, which is not what I want.

I've tried putting a Fill onto Mechanical 15 layer (Courtyard Top), which is OK for eyeballing but I don't get a clearance violation in DRC.

I've added the following Clearance rule but it didn't help:

SELECTION=FALSE|LAYER=TOP|LOCKED=FALSE|POLYGONOUTLINE=FALSE|USERROUTED=TRUE|UNIONINDEX=0|UNIQUEID=RIRCENJA|

RULEKIND=ComponentClearance|NETSCOPE=AnyNet|LAYERKIND=SameLayer|

SCOPE1EXPRESSION=(OnLayer('Mechanical 15') OR OnLayer('Courtyard Top'))|

SCOPE2EXPRESSION=All|

NAME=ComponentClearance_Courtyard|

ENABLED=TRUE|PRIORITY=2|COMMENT= |DEFINEDBYLOGICALDOCUMENT=FALSE|

GAP=0mil|

COLLISIONCHECKMODE=3|VERTICALGAP=0mil|SHOWDISTANCES=FALSE¶

(all one line in the .RUL file)

 

What am I doing wrong please?

 

Cheers

John

  • Cancel

Top Replies

  • tarribred61
    tarribred61 over 6 years ago in reply to frog +1
    Yes, that is what I was trying to say but perhaps unclearly. What I was suggesting further is that the pillar component could be put into a newly added component class and then a separate clearance rule…
Parents
  • frog
    0 frog over 6 years ago

    An alternative approach, which I've used to good effect, is to create a step file representing the pillars and use it to create a component that can then be placed on the PCB.  I don't know whether that will do exactly what you want, but it will give a design rule error if any components collide with the pillars.  This has the potential advantage that it works in 3D rather than assuming that obstacles are projections of 2D shapes.

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
Reply
  • frog
    0 frog over 6 years ago

    An alternative approach, which I've used to good effect, is to create a step file representing the pillars and use it to create a component that can then be placed on the PCB.  I don't know whether that will do exactly what you want, but it will give a design rule error if any components collide with the pillars.  This has the potential advantage that it works in 3D rather than assuming that obstacles are projections of 2D shapes.

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
Children
  • tarribred61
    0 tarribred61 over 6 years ago in reply to frog

    Yes, that is what I was trying to say but perhaps unclearly.  What I was suggesting further is that the pillar component could be put into a newly added component class and then a separate clearance rule can be based on the pillar's component class.  This would allow some expanded clearance to account for mechanical alignments.  Another way would be to make the shape of the step model slightly larger than the actual pillar diameter so as to account for the extra space that might be needed when fitting the PCB to the pillars.  The amount of extra room needed might perhaps depend on whether there is fastening screw, expansion/contraction, mechanical tolerance on the parts, etc. 

    • Cancel
    • Vote Up +1 Vote Down
    • Cancel
  • frog
    0 frog over 6 years ago in reply to tarribred61

    Or perhaps entirely clearly - it was late last night and I may not have given your response the attentiveness that it deserves :-)