Altium CircuitStudio
  • Products & Partners
  • Manufacturers
  • Altium CircuitStudio
  • More
  • Cancel
Altium CircuitStudio
Altium CircuitStudio Forum Wie kann ich den PDF-Output Files verschiedene Namen geben (automatisch generiert)
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Altium CircuitStudio to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Locked Locked
  • Replies 2 replies
  • Subscribers 89 subscribers
  • Views 563 views
  • Users 0 members are here
  • output file
Related
This discussion has been locked.
You can no longer post new replies to this discussion. If you have a question you can start a new discussion

Wie kann ich den PDF-Output Files verschiedene Namen geben (automatisch generiert)

lroth
lroth over 6 years ago

Hallo community,

 

wenn ich die PDF-Output Files generiere (Schema, Layout, Assembly) werden alle unter dem gleichen Namen abgelegt.

Egal welcher Typ Output, es wird immer der gleiche Parameter im File "*.OutJob " verwendet: Parameter "OutputFileName2".

 

Ich habe verschiedenes versucht, letztendlich wird immer der Parameter "OutputFileName2" verwendet.

Auch für die BOM wird der gleiche Parameter verwendet: =OutputName14 + '-' + OutputFileName2.

 

Vielen Dank schon im voraus für eine schnelle Antwort.

  • Cancel

Top Replies

  • tarribred61
    tarribred61 over 6 years ago +1
    You wrote: " Hello community, When I generate the PDF output files (schema, layout, assembly) they are all saved under the same name. Regardless of the output type, the same parameter is always used in…
Parents
  • tarribred61
    0 tarribred61 over 6 years ago

    You wrote:

    " Hello community,
    When I generate the PDF output files (schema, layout, assembly) they are all saved under the same name.  Regardless of the output type, the same parameter is always used in the "* .OutJob" file: "OutputFileName2" parameter.

    I've tried various things, but in the end the parameter "OutputFileName2" is always used. The same parameter is also used for the BOM: = OutputName14 + '-' + OutputFileName2.
    Thank you in advance for a quick answer."

     

    Yes, the output generation and file naming is a bit of a "dog's breakfast" (that is, great big mess) in CircuitStudio.

     

    You can edit the outjob file in a text editor and change names somewhat but there is no guidance on how best to do this.  I have gotten used to it and I generate the outputs one-at-a-time and then rename the PDF files to what I want them to be.

     

    There is room for improvement and maybe we will get some in the next version that is currently in beta testing.  I believe that Altium Designer does have the ability to control output file names for all the generated outputs.

     

    • Cancel
    • Vote Up +1 Vote Down
    • Cancel
Reply
  • tarribred61
    0 tarribred61 over 6 years ago

    You wrote:

    " Hello community,
    When I generate the PDF output files (schema, layout, assembly) they are all saved under the same name.  Regardless of the output type, the same parameter is always used in the "* .OutJob" file: "OutputFileName2" parameter.

    I've tried various things, but in the end the parameter "OutputFileName2" is always used. The same parameter is also used for the BOM: = OutputName14 + '-' + OutputFileName2.
    Thank you in advance for a quick answer."

     

    Yes, the output generation and file naming is a bit of a "dog's breakfast" (that is, great big mess) in CircuitStudio.

     

    You can edit the outjob file in a text editor and change names somewhat but there is no guidance on how best to do this.  I have gotten used to it and I generate the outputs one-at-a-time and then rename the PDF files to what I want them to be.

     

    There is room for improvement and maybe we will get some in the next version that is currently in beta testing.  I believe that Altium Designer does have the ability to control output file names for all the generated outputs.

     

    • Cancel
    • Vote Up +1 Vote Down
    • Cancel
Children
  • lroth
    0 lroth over 6 years ago in reply to tarribred61

    Hi Thomas,

     

    thank you for your answer.

    I do exactly the same work around like you. I also hope Altium will release next version of CS, else it will looks bad for CS.

    I just heard from Farnell technic support that the communication with Altium is very bad and a lot of customers also waiting for answers..