Altium CircuitStudio
  • Products & Partners
  • Manufacturers
  • Altium CircuitStudio
  • More
  • Cancel
Altium CircuitStudio
Altium CircuitStudio Forum CircuitStudio Libraries
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Altium CircuitStudio to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Locked Locked
  • Replies 7 replies
  • Subscribers 91 subscribers
  • Views 2745 views
  • Users 0 members are here
Related
This discussion has been locked.
You can no longer post new replies to this discussion. If you have a question you can start a new discussion

CircuitStudio Libraries

geostel
geostel over 5 years ago

I'm new to CircuitStudio. I've been using Protel for years. I see some similarities. However I'm struggling to create a new component. First Question. There seems to be two standard component libraries. MiscellaneousDevices and MiscellaneousConnectors.

  • Cancel
Parents
  • geostel
    0 geostel over 5 years ago

    Huh, I see half of my message is missing. Questions are.. Can I edit a component in the standard libraries, and can I add a new component to the standard libraries.

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • mf_ibfeew
    0 mf_ibfeew over 5 years ago in reply to geostel

    The answer is on principle yes, but ...

    1) At first: the two original delivered libraries are only a collection of unsorted devices without visible order. I have rejected this two libraries after some hours of work.

    2) this two libraries are from the "integrated library" type, file extension intlib. This is an extension of the old pcblib/schlib concept and integrates both libs into one integrated library-file. So no more looking: have I the according foorptint-library for my schlib available?

    But the disadvantage: you can not directly edit the intlib-library, instead you first have to break the intlib into a separate schlib/pcblib, than edit what you want (add sch-parts or new footprints), than build both again together into the intlib-format. For me this makes constant ongoing work on parts in an integrated library not easy, personally I use mostly the old schlib/pcblib concept (I'm also not lucky with this, it's not easy to get some good ordering concept).

    A description of the integrated library:

    Component Management in CircuitStudio | Online Documentation for Altium Products

    3) A good collection for libraries to start with: the original Altiumlibraries. They are also integrated libraries, but sorted with manufacturer and type. Much better starting point to modify some of this libraries.

    https://techdocs.altium.com/display/ADOH/Download+Libraries

     

    4) If you want to edit/modify such an integrated library:

    File --> Open library --> select the intlib you want

    You will get a question:

    extract sources --> yes, if you want to edit/change something or look in the underlying pcb/schlib or copy some parts

    install library  --> installs the intlib for use in your project, no modification

    For the rebuilding process of the intlib: you have to search through the documentation on element14 or someone else may help.

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
Reply
  • mf_ibfeew
    0 mf_ibfeew over 5 years ago in reply to geostel

    The answer is on principle yes, but ...

    1) At first: the two original delivered libraries are only a collection of unsorted devices without visible order. I have rejected this two libraries after some hours of work.

    2) this two libraries are from the "integrated library" type, file extension intlib. This is an extension of the old pcblib/schlib concept and integrates both libs into one integrated library-file. So no more looking: have I the according foorptint-library for my schlib available?

    But the disadvantage: you can not directly edit the intlib-library, instead you first have to break the intlib into a separate schlib/pcblib, than edit what you want (add sch-parts or new footprints), than build both again together into the intlib-format. For me this makes constant ongoing work on parts in an integrated library not easy, personally I use mostly the old schlib/pcblib concept (I'm also not lucky with this, it's not easy to get some good ordering concept).

    A description of the integrated library:

    Component Management in CircuitStudio | Online Documentation for Altium Products

    3) A good collection for libraries to start with: the original Altiumlibraries. They are also integrated libraries, but sorted with manufacturer and type. Much better starting point to modify some of this libraries.

    https://techdocs.altium.com/display/ADOH/Download+Libraries

     

    4) If you want to edit/modify such an integrated library:

    File --> Open library --> select the intlib you want

    You will get a question:

    extract sources --> yes, if you want to edit/change something or look in the underlying pcb/schlib or copy some parts

    install library  --> installs the intlib for use in your project, no modification

    For the rebuilding process of the intlib: you have to search through the documentation on element14 or someone else may help.